<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: math.h pow() not working</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/math-h-pow-not-working/m-p/1650454#M10157</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;can you please specify what's is not working on pow() function? There is wrong value or why you think that it is not working?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Anyway - the pow() function is returning double by default. Also using pow() for left bit shifting is kind of odd. But seems that EWL STD C library can handle it and uses simple bit shifting.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 15 May 2023 16:10:57 GMT</pubDate>
    <dc:creator>jiri_kral</dc:creator>
    <dc:date>2023-05-15T16:10:57Z</dc:date>
    <item>
      <title>math.h pow() not working</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/math-h-pow-not-working/m-p/1541183#M9274</link>
      <description>&lt;P&gt;im working on MPC mcu im using an example project, i tried to include math.h and use pow(), its not showing errors but its not working, it should be highlighted in an other collor and also i should see where its declared when i press on it but it doesnt show it , the library is shown also at the includes of the project can you please help me&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="turkmani_11_0-1666271363971.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/197517i0BFF779A61614AE7/image-size/medium?v=v2&amp;amp;px=400" role="button" title="turkmani_11_0-1666271363971.png" alt="turkmani_11_0-1666271363971.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 20 Oct 2022 13:09:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/math-h-pow-not-working/m-p/1541183#M9274</guid>
      <dc:creator>turkmani_11</dc:creator>
      <dc:date>2022-10-20T13:09:39Z</dc:date>
    </item>
    <item>
      <title>Re: math.h pow() not working</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/math-h-pow-not-working/m-p/1650411#M10156</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206444"&gt;@turkmani_11&lt;/a&gt;&amp;nbsp;,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Is the problem fixed?&lt;/P&gt;
&lt;P&gt;If not please can you provide more information to help with.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you. Best regards.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;- Mehul&lt;/P&gt;</description>
      <pubDate>Mon, 15 May 2023 14:57:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/math-h-pow-not-working/m-p/1650411#M10156</guid>
      <dc:creator>Mehul_Patel_NXP</dc:creator>
      <dc:date>2023-05-15T14:57:24Z</dc:date>
    </item>
    <item>
      <title>Re: math.h pow() not working</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/math-h-pow-not-working/m-p/1650454#M10157</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;can you please specify what's is not working on pow() function? There is wrong value or why you think that it is not working?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Anyway - the pow() function is returning double by default. Also using pow() for left bit shifting is kind of odd. But seems that EWL STD C library can handle it and uses simple bit shifting.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 15 May 2023 16:10:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/math-h-pow-not-working/m-p/1650454#M10157</guid>
      <dc:creator>jiri_kral</dc:creator>
      <dc:date>2023-05-15T16:10:57Z</dc:date>
    </item>
  </channel>
</rss>