<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>S32 Design StudioのトピックRe: S32G2 intCtrlConfig undeclared</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/S32G2-intCtrlConfig-undeclared/m-p/1650371#M10155</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Are you using Can_Llce_DS_Can2Can_S32G274A_M7&amp;nbsp; example project ?&lt;/P&gt;&lt;P&gt;Yes.&lt;/P&gt;&lt;P&gt;can you tell us which gpio and uart you added ?&lt;/P&gt;&lt;P&gt;UART1 port&amp;nbsp; -RXD- PB_00 ,TXD- PA_13&lt;/P&gt;&lt;P&gt;and also tells which vertion of RTD and S32DS you are using?&lt;/P&gt;&lt;P&gt;RTD-4.4.3.0.2.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Viswanath K&lt;/P&gt;</description>
    <pubDate>Mon, 15 May 2023 13:58:20 GMT</pubDate>
    <dc:creator>viswa_kondapall</dc:creator>
    <dc:date>2023-05-15T13:58:20Z</dc:date>
    <item>
      <title>S32G2 intCtrlConfig undeclared</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32G2-intCtrlConfig-undeclared/m-p/1649411#M10146</link>
      <description>&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;We are using NXP CAN2CAN project. initially it is working fine but once we added few GPIO's and UART and Intrctrl module then this error is occured.&lt;/P&gt;&lt;P&gt;//-------------------------&lt;/P&gt;&lt;P&gt;Building file: ../generate/IntCtrl_Ip/IntCtrl_Ip_Cfg.c&lt;BR /&gt;../generate/src/Platform_Ipw_Cfg.c:101:6: error: 'intCtrlConfig' undeclared here (not in a function); did you mean 'IntCtrlConfig_0'?&lt;BR /&gt;101 | &amp;amp;intCtrlConfig,&lt;BR /&gt;| ^~~~~~~~~~~~~&lt;BR /&gt;| IntCtrlConfig_0&lt;BR /&gt;Building file: ../board/Siul2_Port_Ip_Cfg.c&lt;/P&gt;&lt;P&gt;//---------------------------------------------&lt;/P&gt;&lt;P&gt;Once replaced&amp;nbsp;intCtrlConfig with IntCtrlConfig_0 then it is working. Why is this error is coming.&amp;nbsp;&lt;/P&gt;&lt;P&gt;With this GPIO's and Uart1 is not working&amp;nbsp; We enabled in GPIO in intrctrl for interrupt and uart1 irq handled also given in the list. but not working. for this error occurred then GPIO are not working and UART also not working.&amp;nbsp; These are software changes after this array difference nothing working.&lt;/P&gt;&lt;P&gt;Regads,&lt;/P&gt;&lt;P&gt;Viswa&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 12 May 2023 12:15:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32G2-intCtrlConfig-undeclared/m-p/1649411#M10146</guid>
      <dc:creator>viswa_kondapall</dc:creator>
      <dc:date>2023-05-12T12:15:26Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2 intCtrlConfig undeclared</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32G2-intCtrlConfig-undeclared/m-p/1650327#M10154</link>
      <description>&lt;P&gt;Hi Viswanath&lt;/P&gt;
&lt;P&gt;hope you are doing well.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Are you using Can_Llce_DS_Can2Can_S32G274A_M7&amp;nbsp; example project ?&lt;/P&gt;
&lt;P&gt;can you tell us which gpio and uart you added ?&lt;/P&gt;
&lt;P&gt;and also tells which vertion of RTD and S32DS you are using?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards&lt;/P&gt;
&lt;P&gt;Tushar&lt;/P&gt;</description>
      <pubDate>Mon, 15 May 2023 12:47:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32G2-intCtrlConfig-undeclared/m-p/1650327#M10154</guid>
      <dc:creator>nxf92355</dc:creator>
      <dc:date>2023-05-15T12:47:54Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2 intCtrlConfig undeclared</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32G2-intCtrlConfig-undeclared/m-p/1650371#M10155</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Are you using Can_Llce_DS_Can2Can_S32G274A_M7&amp;nbsp; example project ?&lt;/P&gt;&lt;P&gt;Yes.&lt;/P&gt;&lt;P&gt;can you tell us which gpio and uart you added ?&lt;/P&gt;&lt;P&gt;UART1 port&amp;nbsp; -RXD- PB_00 ,TXD- PA_13&lt;/P&gt;&lt;P&gt;and also tells which vertion of RTD and S32DS you are using?&lt;/P&gt;&lt;P&gt;RTD-4.4.3.0.2.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Viswanath K&lt;/P&gt;</description>
      <pubDate>Mon, 15 May 2023 13:58:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32G2-intCtrlConfig-undeclared/m-p/1650371#M10155</guid>
      <dc:creator>viswa_kondapall</dc:creator>
      <dc:date>2023-05-15T13:58:20Z</dc:date>
    </item>
    <item>
      <title>Re: S32G2 intCtrlConfig undeclared</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/S32G2-intCtrlConfig-undeclared/m-p/1652839#M10174</link>
      <description>&lt;P&gt;Hi Viswanath&lt;/P&gt;&lt;P&gt;I have added Intrctrl component in same example and compiled to regenerate issue. i am not getting such error. can you please tell steps or way you used to add modules in example. so that i can reproduce the issue.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards ,&lt;/P&gt;&lt;P&gt;Tushar&lt;/P&gt;</description>
      <pubDate>Thu, 18 May 2023 06:45:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/S32G2-intCtrlConfig-undeclared/m-p/1652839#M10174</guid>
      <dc:creator>nxf92355</dc:creator>
      <dc:date>2023-05-18T06:45:54Z</dc:date>
    </item>
  </channel>
</rss>