<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to add MCAL / Drivers / OS / Middleware components in S32 Design Studio in S32 Design Studio</title>
    <link>https://community.nxp.com/t5/S32-Design-Studio/How-to-add-MCAL-Drivers-OS-Middleware-components-in-S32-Design/m-p/1645407#M10094</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are CAN2CAN example project from LLCE example list. In this we like to add&amp;nbsp;MCAL / Drivers / OS / Middleware components in S32 Design Studio.&lt;/P&gt;&lt;P&gt;ETH_43 plugins is required but ETH-GMAC only available.&lt;/P&gt;&lt;P&gt;We like to add Uart1 but Linflexuart is not available to addd in the same project.&lt;/P&gt;&lt;P&gt;Power component we like to add to the project but we are not able to add to the project.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So could anyone please help.&amp;nbsp;How to add MCAL / Drivers / OS / Middleware components in S32 Design Studio&amp;nbsp; - 3.4/3.5 - procedure is same i think in the both versions.&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Viswanath K&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 05 May 2023 10:05:13 GMT</pubDate>
    <dc:creator>viswa_kondapall</dc:creator>
    <dc:date>2023-05-05T10:05:13Z</dc:date>
    <item>
      <title>How to add MCAL / Drivers / OS / Middleware components in S32 Design Studio</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/How-to-add-MCAL-Drivers-OS-Middleware-components-in-S32-Design/m-p/1645407#M10094</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are CAN2CAN example project from LLCE example list. In this we like to add&amp;nbsp;MCAL / Drivers / OS / Middleware components in S32 Design Studio.&lt;/P&gt;&lt;P&gt;ETH_43 plugins is required but ETH-GMAC only available.&lt;/P&gt;&lt;P&gt;We like to add Uart1 but Linflexuart is not available to addd in the same project.&lt;/P&gt;&lt;P&gt;Power component we like to add to the project but we are not able to add to the project.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So could anyone please help.&amp;nbsp;How to add MCAL / Drivers / OS / Middleware components in S32 Design Studio&amp;nbsp; - 3.4/3.5 - procedure is same i think in the both versions.&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Viswanath K&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 05 May 2023 10:05:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/How-to-add-MCAL-Drivers-OS-Middleware-components-in-S32-Design/m-p/1645407#M10094</guid>
      <dc:creator>viswa_kondapall</dc:creator>
      <dc:date>2023-05-05T10:05:13Z</dc:date>
    </item>
    <item>
      <title>Re: How to add MCAL / Drivers / OS / Middleware components in S32 Design Studio</title>
      <link>https://community.nxp.com/t5/S32-Design-Studio/How-to-add-MCAL-Drivers-OS-Middleware-components-in-S32-Design/m-p/1645702#M10097</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;To add different peripherals inside S32DS, Config Tools is used. The following links provide a simple blink example from scratch, which should provide the general idea of adding more features into your project:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-a-Blinking-LED-application-project-for-S32G-using/ta-p/1562381" target="_blank"&gt;HOWTO: Create a Blinking LED application project f... - NXP Community&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-a-Blinking-LED-application-project-for-S32G-using/ta-p/1563066" target="_blank"&gt;HOWTO: Create a Blinking LED application project f... - NXP Community&lt;/A&gt;&lt;/P&gt;&lt;P&gt;One is without Autosar (first link) and the other is with Autosar (second link).&lt;/P&gt;&lt;P&gt;As for additional features not available under LLCE and RTD, they need to be installed prior to be usable (i.e. PFE).&lt;/P&gt;&lt;P&gt;More HOWTO's are provided under the following link that may provide to be useful:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/S32DS-list-of-HOWTOs/ta-p/1113475" target="_blank"&gt;S32DS - list of HOWTOs - NXP Community&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Fri, 05 May 2023 18:59:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/S32-Design-Studio/How-to-add-MCAL-Drivers-OS-Middleware-components-in-S32-Design/m-p/1645702#M10097</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-05-05T18:59:56Z</dc:date>
    </item>
  </channel>
</rss>