<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Robotic HardwareのトピックRe: LED driver PCA9635 and PCA9685BS,118</title>
    <link>https://community.nxp.com/t5/Robotic-Hardware/LED-driver-PCA9635-and-PCA9685BS-118/m-p/1216916#M8</link>
    <description>&lt;P&gt;From the datasheet: "The Software Reset (SWRST) Call allows the master to perform a reset of the PCA9635&lt;BR /&gt;through the I2C-bus, identical to the Power-On Reset (POR) that initializes the registers to&lt;BR /&gt;their default state &lt;FONT color="#FF00FF"&gt;&lt;STRONG&gt;causing the outputs to be set HIGH (LED off)&lt;/STRONG&gt;&lt;/FONT&gt;. This allows an easy and&lt;BR /&gt;quick way to reconfigure all device registers to the same condition."&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;The Power-On Reset (POR) default state of LEDn output pins is &lt;STRONG&gt;&lt;FONT color="#FF00FF"&gt;LOW in the case of PCA9685&lt;/FONT&gt;&lt;/STRONG&gt;. It is HIGH for PCA9635&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;So if you are suggesting you will use one for the LEDs that need to be on after reset and the other for LEDs that need to be off, it appears that would work.&lt;/P&gt;</description>
    <pubDate>Tue, 19 Jan 2021 13:38:24 GMT</pubDate>
    <dc:creator>iaingalloway</dc:creator>
    <dc:date>2021-01-19T13:38:24Z</dc:date>
    <item>
      <title>LED driver PCA9635 and PCA9685BS,118</title>
      <link>https://community.nxp.com/t5/Robotic-Hardware/LED-driver-PCA9635-and-PCA9685BS-118/m-p/1065569#M1</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;we have application to turn ON the LEDs during power ON stage and same for some other LEDs to turn OFF.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For that we have selected PCA9635 and PCA9685.&amp;nbsp; After power on processor will take control but we need the state during power on / default condition some ON/OFF.&lt;/P&gt;&lt;P&gt;Please suggest if selected device work with the application.&lt;/P&gt;&lt;P&gt;I have also attached schematics for your review.&lt;/P&gt;&lt;P&gt;-&lt;/P&gt;&lt;P&gt;Mahesh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jul 2020 08:42:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Robotic-Hardware/LED-driver-PCA9635-and-PCA9685BS-118/m-p/1065569#M1</guid>
      <dc:creator>mahesh_gohil</dc:creator>
      <dc:date>2020-07-20T08:42:07Z</dc:date>
    </item>
    <item>
      <title>Re: LED driver PCA9635 and PCA9685BS,118</title>
      <link>https://community.nxp.com/t5/Robotic-Hardware/LED-driver-PCA9635-and-PCA9685BS-118/m-p/1216916#M8</link>
      <description>&lt;P&gt;From the datasheet: "The Software Reset (SWRST) Call allows the master to perform a reset of the PCA9635&lt;BR /&gt;through the I2C-bus, identical to the Power-On Reset (POR) that initializes the registers to&lt;BR /&gt;their default state &lt;FONT color="#FF00FF"&gt;&lt;STRONG&gt;causing the outputs to be set HIGH (LED off)&lt;/STRONG&gt;&lt;/FONT&gt;. This allows an easy and&lt;BR /&gt;quick way to reconfigure all device registers to the same condition."&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;The Power-On Reset (POR) default state of LEDn output pins is &lt;STRONG&gt;&lt;FONT color="#FF00FF"&gt;LOW in the case of PCA9685&lt;/FONT&gt;&lt;/STRONG&gt;. It is HIGH for PCA9635&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;So if you are suggesting you will use one for the LEDs that need to be on after reset and the other for LEDs that need to be off, it appears that would work.&lt;/P&gt;</description>
      <pubDate>Tue, 19 Jan 2021 13:38:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Robotic-Hardware/LED-driver-PCA9635-and-PCA9685BS-118/m-p/1216916#M8</guid>
      <dc:creator>iaingalloway</dc:creator>
      <dc:date>2021-01-19T13:38:24Z</dc:date>
    </item>
  </channel>
</rss>