<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: NXP Rapid IoT: unable to authenticate device's hardware credentials in Rapid IoT</title>
    <link>https://community.nxp.com/t5/Rapid-IoT/NXP-Rapid-IoT-unable-to-authenticate-device-s-hardware/m-p/880022#M482</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am probably having a related issue but slightly different.&amp;nbsp; I am able to operate my device using the Out-of-Box Demo and the Weather Station application that are provided in the Rapid IoT Studio examples.&amp;nbsp; When I try to use other sample applications that I've found on the forum, I run into a host of problems that are related to the Bluetooth connection.&amp;nbsp; One thing that I've noticed is that is consistent is that if I use the provided binary files that the Rapid IoT app on the phone cannot see the device when it is searching even though the phone can see the device in its Bluetooth setup.&amp;nbsp; If I recompile the various demos then some of the them will be seen and will provision but don't completely work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is what I have tried:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Remote Motion Detector&lt;/P&gt;&lt;P&gt;1) Using provided binary - device cannot be found&lt;/P&gt;&lt;P&gt;2) Using recompiled binary - device can be provisioned and phone app can enable but not disable the detector, i.e. on/off does not toggle (this is with an iPhone, with an Android tablet it provisions but does not function).&amp;nbsp; Motion detection feature does work on the iPhone although I can't disable it once it's enabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Smart Locker&lt;/P&gt;&lt;P&gt;1) Using provided binary - device cannot be found&lt;/P&gt;&lt;P&gt;2) Using recompiled binary - device can be provisioned and phone app&amp;nbsp;doesn't work&amp;nbsp;lock state does not toggle (I can toggle it on the device, but change is not detected on the phone and phone cannot change state of the device)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Smart Air Conditioner v0.2&lt;/P&gt;&lt;P&gt;1) Using provided binary - device cannot be found&lt;/P&gt;&lt;P&gt;2) Using recompiled binary - device cannot be provisioned -&amp;nbsp;unable to authenticate device's hardware credentials&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So. it feels like I've got some sort of firmware/software incompatibility.&lt;/P&gt;&lt;P&gt;I've tried recovering the K64F and KW41Z firmware using the documented boot modes.&lt;/P&gt;&lt;P&gt;Is there updated firmware that I should be using?&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do I determine the version of the loaded firmware?&lt;/P&gt;&lt;P&gt;Is there a document that describes the Bluetooth detection and provisioning process?&amp;nbsp; What determines if the A1006 key is used or not?&amp;nbsp; I haven't detected differences in the Atmosphere code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It appears that other have been having these same problems for a while :&amp;nbsp;&lt;A href="https://community.nxp.com/thread/482534"&gt;https://community.nxp.com/thread/482534&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm kind of stuck if I can't get this fixed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ralph&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="IMG_1791.JPG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63629i1013DBC6B7B77D58/image-size/large?v=v2&amp;amp;px=999" role="button" title="IMG_1791.JPG" alt="IMG_1791.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 18 Jan 2019 00:29:23 GMT</pubDate>
    <dc:creator>ralphjy</dc:creator>
    <dc:date>2019-01-18T00:29:23Z</dc:date>
    <item>
      <title>NXP Rapid IoT: unable to authenticate device's hardware credentials</title>
      <link>https://community.nxp.com/t5/Rapid-IoT/NXP-Rapid-IoT-unable-to-authenticate-device-s-hardware/m-p/880019#M479</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am not able to provision my NXP Rapid IoT prototyping kit. The device is listed but when I click "Provision" all I get is "unable to authenticate device's hardware credentials" message. Same results with the Out of the box application as well as with my first application prepared based on the tutorial. Both NXP as well as my android mobile (Xiaomi Redmi Note 3) restarted several times - still the same results.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Screenshot_2019-01-16-19-54-26-315_com.nxp.iot.rapidiot.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/62893i4AC278EA70D210CC/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot_2019-01-16-19-54-26-315_com.nxp.iot.rapidiot.png" alt="Screenshot_2019-01-16-19-54-26-315_com.nxp.iot.rapidiot.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2019 19:17:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Rapid-IoT/NXP-Rapid-IoT-unable-to-authenticate-device-s-hardware/m-p/880019#M479</guid>
      <dc:creator>vilem</dc:creator>
      <dc:date>2019-01-16T19:17:25Z</dc:date>
    </item>
    <item>
      <title>Re: NXP Rapid IoT: unable to authenticate device's hardware credentials</title>
      <link>https://community.nxp.com/t5/Rapid-IoT/NXP-Rapid-IoT-unable-to-authenticate-device-s-hardware/m-p/880020#M480</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm not sure what do you mean by restarting the Rapid IoT, I imagine you refer to the procedure mentioned in this post&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/481369"&gt;https://community.nxp.com/thread/481369&lt;/A&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have not tried it, could you please do it?&amp;nbsp;Also, do you have another device registered for the Rapid IoT? if you do, could you please try to erase it and try to provision again?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If those do not help, could you please try flashing the Out Of The Box example again in the Rapid IoT.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2019 22:13:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Rapid-IoT/NXP-Rapid-IoT-unable-to-authenticate-device-s-hardware/m-p/880020#M480</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2019-01-16T22:13:49Z</dc:date>
    </item>
    <item>
      <title>Re: NXP Rapid IoT: unable to authenticate device's hardware credentials</title>
      <link>https://community.nxp.com/t5/Rapid-IoT/NXP-Rapid-IoT-unable-to-authenticate-device-s-hardware/m-p/880021#M481</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Vilém,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What you described&amp;nbsp;is quite surprising.&lt;/P&gt;&lt;P&gt;Normaly during the provisioning process, the kit is authentified by the server using a key stored in the A1006 component included in the kit. From what you describe it appears that your kit was not authentified for an unclear reason.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This means that, for now and via the Rapid IoT studio, you will not be able to provision the kit on our servers.&amp;nbsp;The provisioning&amp;nbsp;process breaks and you cannot connect the kit to the&amp;nbsp;phone (application)&amp;nbsp;over BLE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In our stand alone weather station example:&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-342336"&gt;https://community.nxp.com/docs/DOC-342336&lt;/A&gt;&lt;/P&gt;&lt;P&gt;The authentication is not enabled via A1006 certificate and with this one you will be able to connect the kit to your phone over BLE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Could you provide me with the serial number of your kit (to be found at the back)&lt;/STRONG&gt; ? This will help me retrieving the test log of your kit. Rapid IoT are all tested ok before shipping but I will take a deep look in the log to check if I can detect something weird.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Jan 2019 12:49:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Rapid-IoT/NXP-Rapid-IoT-unable-to-authenticate-device-s-hardware/m-p/880021#M481</guid>
      <dc:creator>frq05186</dc:creator>
      <dc:date>2019-01-17T12:49:27Z</dc:date>
    </item>
    <item>
      <title>Re: NXP Rapid IoT: unable to authenticate device's hardware credentials</title>
      <link>https://community.nxp.com/t5/Rapid-IoT/NXP-Rapid-IoT-unable-to-authenticate-device-s-hardware/m-p/880022#M482</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am probably having a related issue but slightly different.&amp;nbsp; I am able to operate my device using the Out-of-Box Demo and the Weather Station application that are provided in the Rapid IoT Studio examples.&amp;nbsp; When I try to use other sample applications that I've found on the forum, I run into a host of problems that are related to the Bluetooth connection.&amp;nbsp; One thing that I've noticed is that is consistent is that if I use the provided binary files that the Rapid IoT app on the phone cannot see the device when it is searching even though the phone can see the device in its Bluetooth setup.&amp;nbsp; If I recompile the various demos then some of the them will be seen and will provision but don't completely work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is what I have tried:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Remote Motion Detector&lt;/P&gt;&lt;P&gt;1) Using provided binary - device cannot be found&lt;/P&gt;&lt;P&gt;2) Using recompiled binary - device can be provisioned and phone app can enable but not disable the detector, i.e. on/off does not toggle (this is with an iPhone, with an Android tablet it provisions but does not function).&amp;nbsp; Motion detection feature does work on the iPhone although I can't disable it once it's enabled.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Smart Locker&lt;/P&gt;&lt;P&gt;1) Using provided binary - device cannot be found&lt;/P&gt;&lt;P&gt;2) Using recompiled binary - device can be provisioned and phone app&amp;nbsp;doesn't work&amp;nbsp;lock state does not toggle (I can toggle it on the device, but change is not detected on the phone and phone cannot change state of the device)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Smart Air Conditioner v0.2&lt;/P&gt;&lt;P&gt;1) Using provided binary - device cannot be found&lt;/P&gt;&lt;P&gt;2) Using recompiled binary - device cannot be provisioned -&amp;nbsp;unable to authenticate device's hardware credentials&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So. it feels like I've got some sort of firmware/software incompatibility.&lt;/P&gt;&lt;P&gt;I've tried recovering the K64F and KW41Z firmware using the documented boot modes.&lt;/P&gt;&lt;P&gt;Is there updated firmware that I should be using?&amp;nbsp;&lt;/P&gt;&lt;P&gt;How do I determine the version of the loaded firmware?&lt;/P&gt;&lt;P&gt;Is there a document that describes the Bluetooth detection and provisioning process?&amp;nbsp; What determines if the A1006 key is used or not?&amp;nbsp; I haven't detected differences in the Atmosphere code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It appears that other have been having these same problems for a while :&amp;nbsp;&lt;A href="https://community.nxp.com/thread/482534"&gt;https://community.nxp.com/thread/482534&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm kind of stuck if I can't get this fixed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ralph&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="IMG_1791.JPG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63629i1013DBC6B7B77D58/image-size/large?v=v2&amp;amp;px=999" role="button" title="IMG_1791.JPG" alt="IMG_1791.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Jan 2019 00:29:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Rapid-IoT/NXP-Rapid-IoT-unable-to-authenticate-device-s-hardware/m-p/880022#M482</guid>
      <dc:creator>ralphjy</dc:creator>
      <dc:date>2019-01-18T00:29:23Z</dc:date>
    </item>
    <item>
      <title>Re: NXP Rapid IoT: unable to authenticate device's hardware credentials</title>
      <link>https://community.nxp.com/t5/Rapid-IoT/NXP-Rapid-IoT-unable-to-authenticate-device-s-hardware/m-p/880023#M483</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Reset did not help, flashing&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Out Of The Box example did not help. The behaviour is still the same.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Jan 2019 07:39:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Rapid-IoT/NXP-Rapid-IoT-unable-to-authenticate-device-s-hardware/m-p/880023#M483</guid>
      <dc:creator>vilem</dc:creator>
      <dc:date>2019-01-18T07:39:19Z</dc:date>
    </item>
    <item>
      <title>Re: NXP Rapid IoT: unable to authenticate device's hardware credentials</title>
      <link>https://community.nxp.com/t5/Rapid-IoT/NXP-Rapid-IoT-unable-to-authenticate-device-s-hardware/m-p/880024#M484</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric,&lt;/P&gt;&lt;P&gt;I followed the hint from&amp;nbsp;Estephania (Reset &amp;amp; Reflashing the Out of the box application) without any success - it behaves still the same way.&lt;/P&gt;&lt;P&gt;Hereunder is the ID and Mac of my unit:&amp;nbsp;&lt;/P&gt;&lt;P&gt;ID 410379789406069B, M 00603700000AAED9&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="NXPback.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63731iE9FF21F67788611D/image-size/large?v=v2&amp;amp;px=999" role="button" title="NXPback.jpg" alt="NXPback.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I will try the weather station example over the weekend and let you know.&lt;/P&gt;&lt;P&gt;Thank you for your support.&lt;/P&gt;&lt;P&gt;Vilém&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Jan 2019 07:45:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Rapid-IoT/NXP-Rapid-IoT-unable-to-authenticate-device-s-hardware/m-p/880024#M484</guid>
      <dc:creator>vilem</dc:creator>
      <dc:date>2019-01-18T07:45:16Z</dc:date>
    </item>
    <item>
      <title>Re: NXP Rapid IoT: unable to authenticate device's hardware credentials</title>
      <link>https://community.nxp.com/t5/Rapid-IoT/NXP-Rapid-IoT-unable-to-authenticate-device-s-hardware/m-p/880025#M485</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #ff0000;"&gt;&lt;STRONG&gt;PROBLEM SOLVED&lt;/STRONG&gt;&lt;/SPAN&gt; - Mea Culpa!&lt;/P&gt;&lt;P&gt;The issue is my mobile - I tried a different one and it worked.&amp;nbsp;Then I realized I have my mobile paired with another BLE device - Xiaomi mi band 2. It started to work once I canceled this pairing.&lt;/P&gt;&lt;P&gt;Vilem&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 19 Jan 2019 18:05:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Rapid-IoT/NXP-Rapid-IoT-unable-to-authenticate-device-s-hardware/m-p/880025#M485</guid>
      <dc:creator>vilem</dc:creator>
      <dc:date>2019-01-19T18:05:35Z</dc:date>
    </item>
    <item>
      <title>Re: NXP Rapid IoT: unable to authenticate device's hardware credentials</title>
      <link>https://community.nxp.com/t5/Rapid-IoT/NXP-Rapid-IoT-unable-to-authenticate-device-s-hardware/m-p/880026#M486</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Small update: Once provisioned the device can be operated from my mobile (Xiaomi Redmi Note 3). But I am not able to provision my device from that mobile under any cimcumstances. Have to take my daughter's mobile (Xiaomi Redmi 6) to provision.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Jan 2019 18:25:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Rapid-IoT/NXP-Rapid-IoT-unable-to-authenticate-device-s-hardware/m-p/880026#M486</guid>
      <dc:creator>vilem</dc:creator>
      <dc:date>2019-01-21T18:25:30Z</dc:date>
    </item>
    <item>
      <title>Re: NXP Rapid IoT: unable to authenticate device's hardware credentials</title>
      <link>https://community.nxp.com/t5/Rapid-IoT/NXP-Rapid-IoT-unable-to-authenticate-device-s-hardware/m-p/1152403#M774</link>
      <description>&lt;P&gt;I had same problem, frustrated with devise.complete waste of money and time.good concept of product but implemented badly&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sat, 12 Sep 2020 15:24:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Rapid-IoT/NXP-Rapid-IoT-unable-to-authenticate-device-s-hardware/m-p/1152403#M774</guid>
      <dc:creator>Suryarasp</dc:creator>
      <dc:date>2020-09-12T15:24:01Z</dc:date>
    </item>
  </channel>
</rss>