<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS1026A - PCI Express RC inbound issue in QorIQ</title>
    <link>https://community.nxp.com/t5/QorIQ/LS1026A-PCI-Express-RC-inbound-issue/m-p/1179752#M9923</link>
    <description>&lt;P&gt;Please check with the OS vendor whether SMMU is properly configured for the defined inbound region.&lt;/P&gt;
&lt;P&gt;Also ensure that the region is outside of the base and limit ranges defined for the port in the Type 1 configuration header.&lt;/P&gt;</description>
    <pubDate>Mon, 09 Nov 2020 01:36:55 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2020-11-09T01:36:55Z</dc:date>
    <item>
      <title>LS1026A - PCI Express RC inbound issue</title>
      <link>https://community.nxp.com/t5/QorIQ/LS1026A-PCI-Express-RC-inbound-issue/m-p/1179739#M9922</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;In our system we are using an LS1026A connected to a device by PCIe. The LS1026A is acting as RC, and the device as EP. We are running vxWorks RTOS.&lt;/P&gt;&lt;P&gt;Accesses from CPU to the device is working correctly. But when the device is trying to access the CPU RAM it looks like it doesn't work properly.&lt;/P&gt;&lt;P&gt;We configured an Inbound memory window at 0x88000000-0x8803FFFFF (4MB space) -&amp;nbsp; the physical address space of the shared memory. We also configured the EP to this address space.&lt;/P&gt;&lt;P&gt;0x900 = 0x80000004 = INBOUND | &lt;STRONG&gt;REGION #4&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;0x904 = 0x00000000&amp;nbsp; =MEM&lt;/P&gt;&lt;P&gt;0x908 = 0x80000000 = ENABLED ADDRESS MATCH MODE&lt;/P&gt;&lt;P&gt;0x910-0x90C = 0x00000000_88000000 = REGION BASE ADDRESS&lt;/P&gt;&lt;P&gt;0x914 = 0x883FFFFF = LIMIT&lt;/P&gt;&lt;P&gt;0x91C-0x918 = 0x00000000_88000000 = TARGET BASE ADDRESS&lt;/P&gt;&lt;P&gt;Is there any other configuration we need to do to get it to work?&lt;BR /&gt;Is there any way to monitor the read attempts from the EP? to validate there are such an attempts&lt;/P&gt;&lt;P&gt;Do you have any suggestions?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Sun, 08 Nov 2020 11:04:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/LS1026A-PCI-Express-RC-inbound-issue/m-p/1179739#M9922</guid>
      <dc:creator>PL_Haim</dc:creator>
      <dc:date>2020-11-08T11:04:50Z</dc:date>
    </item>
    <item>
      <title>Re: LS1026A - PCI Express RC inbound issue</title>
      <link>https://community.nxp.com/t5/QorIQ/LS1026A-PCI-Express-RC-inbound-issue/m-p/1179752#M9923</link>
      <description>&lt;P&gt;Please check with the OS vendor whether SMMU is properly configured for the defined inbound region.&lt;/P&gt;
&lt;P&gt;Also ensure that the region is outside of the base and limit ranges defined for the port in the Type 1 configuration header.&lt;/P&gt;</description>
      <pubDate>Mon, 09 Nov 2020 01:36:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/LS1026A-PCI-Express-RC-inbound-issue/m-p/1179752#M9923</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2020-11-09T01:36:55Z</dc:date>
    </item>
  </channel>
</rss>