<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can I disable secure boot in P1010 forever? in QorIQ</title>
    <link>https://community.nxp.com/t5/QorIQ/Can-I-disable-secure-boot-in-P1010-forever/m-p/904718#M8006</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please look P1010 Reference Manual, Section 4.5.3.16 "Secure boot configuration"&lt;/P&gt;&lt;P&gt;If "Intent to secure" fuse is not blown, you can pull-up HRESET_REQ_B during reset to disable secure boot.&lt;/P&gt;&lt;P&gt;This pin has internal weak pull-up, however if you have anything connected to this pin (I'm quite sure you do have), than this internal weak pull-up may be not adequate and external pull-up or active driver is required. Please see device datasheet, Table 1, Note 3 below the table.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Both mentioned documents are available for download from P1010 Product Page, "Documentation" tab:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/power-architecture-processors/qoriq-platforms/p-series/qoriq-p1010-and-p1014-low-power-communications-processors-with-trust-architecture:P1010?tab=Documentation_Tab"&gt;https://www.nxp.com/products/processors-and-microcontrollers/power-architecture-processors/qoriq-platforms/p-series/qoriq-p1010-and-p1014-low-power-communications-processors-with-trust-architecture:P1010?tab=Documentation_Tab&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Apr 2019 19:51:05 GMT</pubDate>
    <dc:creator>alexander_yakov</dc:creator>
    <dc:date>2019-04-23T19:51:05Z</dc:date>
    <item>
      <title>Can I disable secure boot in P1010 forever?</title>
      <link>https://community.nxp.com/t5/QorIQ/Can-I-disable-secure-boot-in-P1010-forever/m-p/904717#M8005</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Now, I am use P1010 cpu in the system. I use normal uboot&amp;amp;linux image booting from nor flash, not secure boot and never touch sfp fuse in P1010.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sometimes I find that the cpu cannot boot uboot and no uboot print info in the uart console. When I power off and power on it again, it is the same. Then I use codewarrior usb tape to connnet the cpu, but the codewarrior software ask for a 64bit response word, and I also do not known the word.&amp;nbsp;&lt;/P&gt;&lt;P&gt;This problem is cased by hardware or software and maybe where? Can I skip this problem by disble secure boot completely and how?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Apr 2019 10:00:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/Can-I-disable-secure-boot-in-P1010-forever/m-p/904717#M8005</guid>
      <dc:creator>cq_wangwei_me</dc:creator>
      <dc:date>2019-04-23T10:00:49Z</dc:date>
    </item>
    <item>
      <title>Re: Can I disable secure boot in P1010 forever?</title>
      <link>https://community.nxp.com/t5/QorIQ/Can-I-disable-secure-boot-in-P1010-forever/m-p/904718#M8006</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please look P1010 Reference Manual, Section 4.5.3.16 "Secure boot configuration"&lt;/P&gt;&lt;P&gt;If "Intent to secure" fuse is not blown, you can pull-up HRESET_REQ_B during reset to disable secure boot.&lt;/P&gt;&lt;P&gt;This pin has internal weak pull-up, however if you have anything connected to this pin (I'm quite sure you do have), than this internal weak pull-up may be not adequate and external pull-up or active driver is required. Please see device datasheet, Table 1, Note 3 below the table.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Both mentioned documents are available for download from P1010 Product Page, "Documentation" tab:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/power-architecture-processors/qoriq-platforms/p-series/qoriq-p1010-and-p1014-low-power-communications-processors-with-trust-architecture:P1010?tab=Documentation_Tab"&gt;https://www.nxp.com/products/processors-and-microcontrollers/power-architecture-processors/qoriq-platforms/p-series/qoriq-p1010-and-p1014-low-power-communications-processors-with-trust-architecture:P1010?tab=Documentation_Tab&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Apr 2019 19:51:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/Can-I-disable-secure-boot-in-P1010-forever/m-p/904718#M8006</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2019-04-23T19:51:05Z</dc:date>
    </item>
    <item>
      <title>Re: Can I disable secure boot in P1010 forever?</title>
      <link>https://community.nxp.com/t5/QorIQ/Can-I-disable-secure-boot-in-P1010-forever/m-p/904719#M8007</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your suggestion.&lt;/P&gt;&lt;P&gt;If the cfg_sb_dis is not external pull-up suitably, P1010 may enter secure boot mode. Does the cpu&amp;nbsp; not never enter non-secure boot mode by power up again if pull-up resister is ok? It seams that the cpu is locked by it self and I must replace the cpu. Now i use a 4.7k pull-up resister to 3.3v.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Apr 2019 02:25:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/Can-I-disable-secure-boot-in-P1010-forever/m-p/904719#M8007</guid>
      <dc:creator>cq_wangwei_me</dc:creator>
      <dc:date>2019-04-24T02:25:55Z</dc:date>
    </item>
    <item>
      <title>Re: Can I disable secure boot in P1010 forever?</title>
      <link>https://community.nxp.com/t5/QorIQ/Can-I-disable-secure-boot-in-P1010-forever/m-p/904720#M8008</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If pull-up is ignored, than this means "Intent to secure" fuse is blown. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Apr 2019 19:58:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/Can-I-disable-secure-boot-in-P1010-forever/m-p/904720#M8008</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2019-04-24T19:58:00Z</dc:date>
    </item>
  </channel>
</rss>