<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Does the Layerscape QorIQ LS1043A Support PTP (1588, precision timing protocol) over 10GBE? in QorIQ</title>
    <link>https://community.nxp.com/t5/QorIQ/Does-the-Layerscape-QorIQ-LS1043A-Support-PTP-1588-precision/m-p/867963#M7555</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see the LS1043A supports Ethernet 1588 which is precision timing protocol. I also see it has 5 available 1GBE Ethernet interfaces, and a single XFI interface which operates at 10G. I would like to know if the 10G interface from the XFI supports 1588/PTP as it seems the other 1GBE interfaces do.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is not clear to me from the datasheet, but if this is specified somewhere please do point me there.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 28 Jan 2019 15:50:50 GMT</pubDate>
    <dc:creator>steveX9</dc:creator>
    <dc:date>2019-01-28T15:50:50Z</dc:date>
    <item>
      <title>Does the Layerscape QorIQ LS1043A Support PTP (1588, precision timing protocol) over 10GBE?</title>
      <link>https://community.nxp.com/t5/QorIQ/Does-the-Layerscape-QorIQ-LS1043A-Support-PTP-1588-precision/m-p/867963#M7555</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see the LS1043A supports Ethernet 1588 which is precision timing protocol. I also see it has 5 available 1GBE Ethernet interfaces, and a single XFI interface which operates at 10G. I would like to know if the 10G interface from the XFI supports 1588/PTP as it seems the other 1GBE interfaces do.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is not clear to me from the datasheet, but if this is specified somewhere please do point me there.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Jan 2019 15:50:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/Does-the-Layerscape-QorIQ-LS1043A-Support-PTP-1588-precision/m-p/867963#M7555</guid>
      <dc:creator>steveX9</dc:creator>
      <dc:date>2019-01-28T15:50:50Z</dc:date>
    </item>
    <item>
      <title>Re: Does the Layerscape QorIQ LS1043A Support PTP (1588, precision timing protocol) over 10GBE?</title>
      <link>https://community.nxp.com/t5/QorIQ/Does-the-Layerscape-QorIQ-LS1043A-Support-PTP-1588-precision/m-p/867964#M7556</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I think you can find that in the QorIQ LS1043A Data Path Acceleration Architecture (DPAA) Reference Manual. It says: "The 1588 timer module interfaces to up to an unlimited number of 10/100/1000 MB or 10G Ethernet&amp;nbsp;MAC". mEMAC Features Summary also says that it has 1588 timestamping. The mEMAC supports&amp;nbsp;&lt;SPAN&gt;10/100/1000 MB&amp;nbsp;and 10G.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Feb 2019 03:38:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/Does-the-Layerscape-QorIQ-LS1043A-Support-PTP-1588-precision/m-p/867964#M7556</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2019-02-01T03:38:45Z</dc:date>
    </item>
    <item>
      <title>Re: Does the Layerscape QorIQ LS1043A Support PTP (1588, precision timing protocol) over 10GBE?</title>
      <link>https://community.nxp.com/t5/QorIQ/Does-the-Layerscape-QorIQ-LS1043A-Support-PTP-1588-precision/m-p/867965#M7557</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for pointing me to that reference manual. Yes, I see the quote you copied in section 7.1 of that manual. I think this does answer my question in that PTP is supported over any of the ethernet interfaces.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 03 Feb 2019 06:23:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/Does-the-Layerscape-QorIQ-LS1043A-Support-PTP-1588-precision/m-p/867965#M7557</guid>
      <dc:creator>steveX9</dc:creator>
      <dc:date>2019-02-03T06:23:34Z</dc:date>
    </item>
  </channel>
</rss>