<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PCIe Master Abort in QorIQ</title>
    <link>https://community.nxp.com/t5/QorIQ/PCIe-Master-Abort/m-p/735825#M5942</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a P4080 configured as RC connected to a P1022 through a switch. During a test the P4080 read data from P1022 and P1022 was reseted.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When this happened the P4080 crashed. I attached a Lauterbach debugging probe and saw that the Received_master_abort bit in Status_Register was set. I wasn't able to do any configuration accesses to any bus but the internal (bus 0). Only a hot reset resolved this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After consulting the datasheet I thought that the master abort was caused by&amp;nbsp;a unsupported request completion. I&amp;nbsp;disabled the unsupported request error reporting in the switch but that didn't solve anything.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Am I on the right track? Is the error caused by some error forwarded to the P4080 because it's RC? I have disabled every error bit I can find without any progress.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Emil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Jan 2018 16:58:20 GMT</pubDate>
    <dc:creator>emilviding</dc:creator>
    <dc:date>2018-01-18T16:58:20Z</dc:date>
    <item>
      <title>PCIe Master Abort</title>
      <link>https://community.nxp.com/t5/QorIQ/PCIe-Master-Abort/m-p/735825#M5942</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a P4080 configured as RC connected to a P1022 through a switch. During a test the P4080 read data from P1022 and P1022 was reseted.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When this happened the P4080 crashed. I attached a Lauterbach debugging probe and saw that the Received_master_abort bit in Status_Register was set. I wasn't able to do any configuration accesses to any bus but the internal (bus 0). Only a hot reset resolved this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After consulting the datasheet I thought that the master abort was caused by&amp;nbsp;a unsupported request completion. I&amp;nbsp;disabled the unsupported request error reporting in the switch but that didn't solve anything.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Am I on the right track? Is the error caused by some error forwarded to the P4080 because it's RC? I have disabled every error bit I can find without any progress.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Emil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jan 2018 16:58:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/PCIe-Master-Abort/m-p/735825#M5942</guid>
      <dc:creator>emilviding</dc:creator>
      <dc:date>2018-01-18T16:58:20Z</dc:date>
    </item>
    <item>
      <title>Re: PCIe Master Abort</title>
      <link>https://community.nxp.com/t5/QorIQ/PCIe-Master-Abort/m-p/735826#M5943</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The problem seems to be PCIe Ack time-out (PEX_ERR_DR[PAT]). When that bit is set it's not possible to access any external PCIe bus. In some cases it's possible to regain access by clearing the bit but not always. Disabling the bit does nothing to solve the problem, it just masks the error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to be able to access other endpoints even when the P1022 is in reset. It that possible?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/Emil&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 20 Jan 2018 15:59:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/PCIe-Master-Abort/m-p/735826#M5943</guid>
      <dc:creator>emilviding</dc:creator>
      <dc:date>2018-01-20T15:59:37Z</dc:date>
    </item>
  </channel>
</rss>