<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>QorIQのトピックWindows 10 + Codewarrior ssh + LA1575?</title>
    <link>https://community.nxp.com/t5/QorIQ/Windows-10-Codewarrior-ssh-LA1575/m-p/730590#M5877</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Trying to run programs via codewarrior using ssh to LA1575.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm getting this error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="win10-CW-ssh-error.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/4587iF9707136E119D466/image-size/large?v=v2&amp;amp;px=999" role="button" title="win10-CW-ssh-error.png" alt="win10-CW-ssh-error.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas what could be wrong? Seems to build fine, I can use CW tap and connect to the target and reflash, etc. Also - I can ssh from putty on the same PC to the target.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Version: 11.3.0&lt;BR /&gt;Build Id: 180126&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Randy Krakora&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Feb 2018 00:24:53 GMT</pubDate>
    <dc:creator>RandyKrakora</dc:creator>
    <dc:date>2018-02-09T00:24:53Z</dc:date>
    <item>
      <title>Windows 10 + Codewarrior ssh + LA1575?</title>
      <link>https://community.nxp.com/t5/QorIQ/Windows-10-Codewarrior-ssh-LA1575/m-p/730590#M5877</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Trying to run programs via codewarrior using ssh to LA1575.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm getting this error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="win10-CW-ssh-error.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/4587iF9707136E119D466/image-size/large?v=v2&amp;amp;px=999" role="button" title="win10-CW-ssh-error.png" alt="win10-CW-ssh-error.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas what could be wrong? Seems to build fine, I can use CW tap and connect to the target and reflash, etc. Also - I can ssh from putty on the same PC to the target.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Version: 11.3.0&lt;BR /&gt;Build Id: 180126&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Randy Krakora&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Feb 2018 00:24:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/Windows-10-Codewarrior-ssh-LA1575/m-p/730590#M5877</guid>
      <dc:creator>RandyKrakora</dc:creator>
      <dc:date>2018-02-09T00:24:53Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 10 + Codewarrior ssh + LA1575?</title>
      <link>https://community.nxp.com/t5/QorIQ/Windows-10-Codewarrior-ssh-LA1575/m-p/730591#M5878</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Randy Krakora,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you debugging Linux application project?&lt;/P&gt;&lt;P&gt;If yes, please refer to the section "8.2.2.2 Updating remote connection" in C:\Freescale\CW4NET_v2018.01\CW_ARMv8\ARMv8\Help\PDF\ARMv8_Targeting_Manual.pdf to configure the debug connection property.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Apr 2018 03:13:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/Windows-10-Codewarrior-ssh-LA1575/m-p/730591#M5878</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2018-04-13T03:13:49Z</dc:date>
    </item>
  </channel>
</rss>