<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>QorIQのトピックLS1012a standby mode</title>
    <link>https://community.nxp.com/t5/QorIQ/LS1012a-standby-mode/m-p/710177#M5670</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working with the custom ls1012a board. Trying to send device to sleep and wake it up. For now stuck after the first step, it doesn't wake up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Running yocto&amp;nbsp;bsp is based on the RDB board.&amp;nbsp;I have configured needed pin (gpio0 27) as gpio&amp;nbsp;in the RCW and tested it's&amp;nbsp;in/out functions. All is ok. Then I have it registered as gpio-key and as a possible wakeup source within dts:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;gpio-keys {&lt;BR /&gt;&amp;nbsp; &amp;nbsp; compatible = "gpio-keys";&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; up {&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; label = "gpio-wake";&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; gpios = &amp;lt;&amp;amp;gpio0 27 GPIO_ACTIVE_HIGH&amp;gt;;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; linux,code = &amp;lt;29&amp;gt;;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; gpio-key,wakeup;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; };&lt;BR /&gt; };&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;But still, when I send board into "mem" sleep (tried "freeze" as well, same thing) I can't wake it up with gpio. As a matter of fact, I can't wake it up with anything else as well. I have tried enabling uart as a wakeup source, same thing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What am I doing wrong? Should this work in the current implementation of the BSP? Would be grateful for any pointers where I can look to debug it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Oct 2017 15:03:16 GMT</pubDate>
    <dc:creator>haff</dc:creator>
    <dc:date>2017-10-18T15:03:16Z</dc:date>
    <item>
      <title>LS1012a standby mode</title>
      <link>https://community.nxp.com/t5/QorIQ/LS1012a-standby-mode/m-p/710177#M5670</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working with the custom ls1012a board. Trying to send device to sleep and wake it up. For now stuck after the first step, it doesn't wake up.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Running yocto&amp;nbsp;bsp is based on the RDB board.&amp;nbsp;I have configured needed pin (gpio0 27) as gpio&amp;nbsp;in the RCW and tested it's&amp;nbsp;in/out functions. All is ok. Then I have it registered as gpio-key and as a possible wakeup source within dts:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;gpio-keys {&lt;BR /&gt;&amp;nbsp; &amp;nbsp; compatible = "gpio-keys";&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; up {&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; label = "gpio-wake";&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; gpios = &amp;lt;&amp;amp;gpio0 27 GPIO_ACTIVE_HIGH&amp;gt;;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; linux,code = &amp;lt;29&amp;gt;;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; gpio-key,wakeup;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; };&lt;BR /&gt; };&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;But still, when I send board into "mem" sleep (tried "freeze" as well, same thing) I can't wake it up with gpio. As a matter of fact, I can't wake it up with anything else as well. I have tried enabling uart as a wakeup source, same thing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What am I doing wrong? Should this work in the current implementation of the BSP? Would be grateful for any pointers where I can look to debug it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Oct 2017 15:03:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/LS1012a-standby-mode/m-p/710177#M5670</guid>
      <dc:creator>haff</dc:creator>
      <dc:date>2017-10-18T15:03:16Z</dc:date>
    </item>
    <item>
      <title>Re: LS1012a standby mode</title>
      <link>https://community.nxp.com/t5/QorIQ/LS1012a-standby-mode/m-p/710178#M5671</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Found what I have missed.&lt;/P&gt;&lt;P&gt;Needed to stop RCPM from powering down GPIO during LPM20. To do it I have added&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;fsl,rcpm-wakeup = &amp;lt;&amp;amp;rcpm 0x00000040&amp;gt;;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;into the&amp;nbsp;gpio-keys node in dts. Now can wake up the device using this GPIO.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Oct 2017 10:18:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/LS1012a-standby-mode/m-p/710178#M5671</guid>
      <dc:creator>haff</dc:creator>
      <dc:date>2017-10-19T10:18:49Z</dc:date>
    </item>
  </channel>
</rss>