<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>QorIQのトピックu-boot configuration changes using ls1021A QORIQ SDK</title>
    <link>https://community.nxp.com/t5/QorIQ/u-boot-configuration-changes-using-ls1021A-QORIQ-SDK/m-p/685350#M5331</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the document QorIQ SDK v2.0-1703 Documentation: Section 3.3.1 Customize U-Boot : The document says u-boot &amp;lt;machine&amp;gt;.conf UBOOT_CONFIG variables are to be modified as needed and then u-boot source code is modified.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our custom board will boot from QSPI FLASH. It will have a larger FLASH than the ls1021Atwr.&lt;/P&gt;&lt;P&gt;When analyzing the &amp;lt;machine&amp;gt;.conf file, there are a variety of "defaults" configured. I see that several u-boot versions are built, one of which is QSPI boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, my questions are:&lt;/P&gt;&lt;P&gt;1) Are the required modifications to u-boot source/configs already taken care of by the SDK?&lt;/P&gt;&lt;P&gt;2) If not, which ones require mods for a given boot device? I read in other places that the boot source when building with yacto is determined in the local.conf file, but I don't see that said in the SDK document. ... So, this is confusing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you mind clarifying what needs to be done to build a QSPI boot from Nor for a ls1021a? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Jul 2017 20:53:51 GMT</pubDate>
    <dc:creator>scottywimberley</dc:creator>
    <dc:date>2017-07-26T20:53:51Z</dc:date>
    <item>
      <title>u-boot configuration changes using ls1021A QORIQ SDK</title>
      <link>https://community.nxp.com/t5/QorIQ/u-boot-configuration-changes-using-ls1021A-QORIQ-SDK/m-p/685350#M5331</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the document QorIQ SDK v2.0-1703 Documentation: Section 3.3.1 Customize U-Boot : The document says u-boot &amp;lt;machine&amp;gt;.conf UBOOT_CONFIG variables are to be modified as needed and then u-boot source code is modified.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our custom board will boot from QSPI FLASH. It will have a larger FLASH than the ls1021Atwr.&lt;/P&gt;&lt;P&gt;When analyzing the &amp;lt;machine&amp;gt;.conf file, there are a variety of "defaults" configured. I see that several u-boot versions are built, one of which is QSPI boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, my questions are:&lt;/P&gt;&lt;P&gt;1) Are the required modifications to u-boot source/configs already taken care of by the SDK?&lt;/P&gt;&lt;P&gt;2) If not, which ones require mods for a given boot device? I read in other places that the boot source when building with yacto is determined in the local.conf file, but I don't see that said in the SDK document. ... So, this is confusing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you mind clarifying what needs to be done to build a QSPI boot from Nor for a ls1021a? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jul 2017 20:53:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/u-boot-configuration-changes-using-ls1021A-QORIQ-SDK/m-p/685350#M5331</guid>
      <dc:creator>scottywimberley</dc:creator>
      <dc:date>2017-07-26T20:53:51Z</dc:date>
    </item>
    <item>
      <title>Re: u-boot configuration changes using ls1021A QORIQ SDK</title>
      <link>https://community.nxp.com/t5/QorIQ/u-boot-configuration-changes-using-ls1021A-QORIQ-SDK/m-p/685351#M5332</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;OL&gt;&lt;LI&gt;&lt;SPAN style="font-size: 10.0pt;"&gt; Modification .h file in /&lt;SPAN style="background: white;"&gt; include/configs folder is needed for new peripherals on the LS1021a board.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; background: white;"&gt;Use the following command sequence for getting u-boot source:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; background: white;"&gt;bitbake -c cleansstate u-boot&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; background: white;"&gt;bitbake -c patch u-boot // source of the u-boot&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; background: white;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; background: white;"&gt;Use the following command sequence for u-boot compiling:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; background: white;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; background: white;"&gt;bitbake u-boot&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; background: white;"&gt;bitbake -c compile -f u-boot&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;OL start="2"&gt;&lt;LI&gt;&lt;SPAN style="font-size: 10.0pt;"&gt; Default configuration for the TWR-LS1021a board uses QSPI boot.&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jul 2017 06:11:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/u-boot-configuration-changes-using-ls1021A-QORIQ-SDK/m-p/685351#M5332</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2017-07-27T06:11:39Z</dc:date>
    </item>
    <item>
      <title>Re: u-boot configuration changes using ls1021A QORIQ SDK</title>
      <link>https://community.nxp.com/t5/QorIQ/u-boot-configuration-changes-using-ls1021A-QORIQ-SDK/m-p/685352#M5333</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the response Pavel, however; I think you did not understand&lt;/P&gt;&lt;P&gt;my questions, perhaps due to my articulation. So, I will break it down a&lt;/P&gt;&lt;P&gt;bit.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you look at the Document Number: QORIQSDK21703 Rev. 0, 03/2017&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;QorIQ SDK v2.0-1703 Documentation&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For QorIQ Processors&lt;/P&gt;&lt;P&gt;in section 3.3.1 Customize U-Boot, you will se the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How to Configure, Modify, or Rebuild U-Boot&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To Modify U-Boot Configuration:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Modify UBOOT_CONFIG. Values for UBOOT_CONFIG are listed in&lt;/P&gt;&lt;P&gt; conf/&lt;/P&gt;&lt;P&gt;local.conf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/****** end snip ********/&lt;/P&gt;&lt;P&gt;This statement is NOT included in the SDK documentation referenced. Does it&lt;/P&gt;&lt;P&gt;still apply since it is an NXP document?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question #3: Does this mean that the local.conf should be the ONLY place&lt;/P&gt;&lt;P&gt;the configuration should be made? If not where?&lt;/P&gt;&lt;P&gt;Question #4: Could you please indicate where changes should be made to: Use&lt;/P&gt;&lt;P&gt;a Micron spi Flash with qspi instead of the 2 options in the SDK?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jul 2017 19:50:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/u-boot-configuration-changes-using-ls1021A-QORIQ-SDK/m-p/685352#M5333</guid>
      <dc:creator>scottywimberley</dc:creator>
      <dc:date>2017-07-27T19:50:20Z</dc:date>
    </item>
    <item>
      <title>Re: u-boot configuration changes using ls1021A QORIQ SDK</title>
      <link>https://community.nxp.com/t5/QorIQ/u-boot-configuration-changes-using-ls1021A-QORIQ-SDK/m-p/685353#M5334</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Look at the Section 3.3.1 of SDK 2.0-1703 documentation:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fsupporting-information%2FQORIQ-SDK-2.0-IC-REV0.pdf" rel="nofollow" target="_blank"&gt;http://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;This Section shows the path to configuration files for all processors.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Attached file contains configuration file from this folder for the TWR-LS1021a board.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;There are the following in this file:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;UBOOT_CONFIG ??= "sdcard-ifc sdcard-qspi lpuart qspi secure-boot nor"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;UBOOT_CONFIG[nor] = "ls1021atwr_nor_config,,u-boot-dtb.bin"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;UBOOT_CONFIG[sdcard-ifc] = "ls1021atwr_sdcard_ifc_config,,u-boot-with-spl-pbl.bin"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;UBOOT_CONFIG[sdcard-qspi] = "ls1021atwr_sdcard_qspi_config,,u-boot-with-spl-pbl.bin"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;UBOOT_CONFIG[lpuart] = "ls1021atwr_nor_lpuart_config,,u-boot-dtb.bin"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;UBOOT_CONFIG[qspi] = "ls1021atwr_qspi_config,,u-boot-dtb.bin"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;UBOOT_CONFIG[secure-boot] = "ls1021atwr_nor_SECURE_BOOT_config"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;You can see that this SDK supports qspi boot.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Look at the attached file. It is screenshot /deploy folder from the SDK 2.0-1703 for the TWR-LS1021a.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Find u-boot for QSPI in this folder. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Jul 2017 03:16:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/u-boot-configuration-changes-using-ls1021A-QORIQ-SDK/m-p/685353#M5334</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2017-07-28T03:16:00Z</dc:date>
    </item>
  </channel>
</rss>