<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: bitbake fsl-image-full build error for t1040qds board in QorIQ</title>
    <link>https://community.nxp.com/t5/QorIQ/bitbake-fsl-image-full-build-error-for-t1040qds-board/m-p/313594#M533</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Thanks Yiping,&lt;/P&gt;&lt;P&gt;Yes, the above mentioned steps are working for me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Chandra&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Jul 2014 10:24:40 GMT</pubDate>
    <dc:creator>chandrashekhar</dc:creator>
    <dc:date>2014-07-02T10:24:40Z</dc:date>
    <item>
      <title>bitbake fsl-image-full build error for t1040qds board</title>
      <link>https://community.nxp.com/t5/QorIQ/bitbake-fsl-image-full-build-error-for-t1040qds-board/m-p/313592#M531</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;I am getting below error while building fsl-image-full for t1040qds board. But it works for fsl-image-core.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;ERROR: Function failed: do_configure (see /home/asr907/SDK/QorIQ-SDK-T1040-BSP0.2-20140310-yocto/build_t1040qds_release/tmp/work/ppce5500-fsl-linux/netcf/0.2.2+gitAUTOINC+2b0d9ca226c13d7150382367f62b256bdb2db5ef-r1/temp/log.do_configure.26819 for further information)&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;ERROR: Logfile of failure stored in: /home/asr907/SDK/QorIQ-SDK-T1040-BSP0.2-20140310-yocto/build_t1040qds_release/tmp/work/ppce5500-fsl-linux/netcf/0.2.2+gitAUTOINC+2b0d9ca226c13d7150382367f62b256bdb2db5ef-r1/temp/log.do_configure.26819&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Log data follows:&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;| DEBUG: Executing python function sysroot_cleansstate&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;| DEBUG: Python function sysroot_cleansstate finished&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;| DEBUG: SITE files ['endian-big', 'bit-32', 'powerpc-common', 'common-linux', 'common-glibc', 'powerpc32-linux', 'powerpc-linux', 'common']&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;| DEBUG: Executing shell function autotools_preconfigure&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;| DEBUG: Shell function autotools_preconfigure finished&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;| DEBUG: Executing shell function do_configure&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;| ./bootstrap: Bootstrapping from checked-out netcf sources...&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;| ./bootstrap: consider installing git-merge-changelog from gnulib&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;| ./bootstrap: getting gnulib files...&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;| fatal: unable to connect to git.sv.gnu.org:&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;| git.sv.gnu.org[0: 140.186.70.72]: errno=No route to host&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;| &lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;| Cloning into '.gnulib'...&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;| Clone of 'git://git.sv.gnu.org/gnulib.git' into submodule path '.gnulib' failed&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;| ERROR: Function failed: do_configure (see /home/asr907/SDK/QorIQ-SDK-T1040-BSP0.2-20140310-yocto/build_t1040qds_release/tmp/work/ppce5500-fsl-linux/netcf/0.2.2+gitAUTOINC+2b0d9ca226c13d7150382367f62b256bdb2db5ef-r1/temp/log.do_configure.26819 for further information)&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;ERROR: Task 5317 (/home/asr907/SDK/QorIQ-SDK-T1040-BSP0.2-20140310-yocto/meta-virtualization/recipes-networking/netcf/netcf_git.bb, do_configure) failed with exit code '1'&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;NOTE: Tasks Summary: Attempted 2637 tasks of which 2626 didn't need to be rerun and 1 failed.&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Waiting for 0 running tasks to finish:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Summary: 1 task failed:&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;&amp;nbsp; /home/asr907/SDK/QorIQ-SDK-T1040-BSP0.2-20140310-yocto/meta-virtualization/recipes-networking/netcf/netcf_git.bb, do_configure&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Summary: There was 1 ERROR message shown, returning a non-zero exit code.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Am I missing any configuration? How it can be resolved?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Chandra&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jun 2014 05:09:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/bitbake-fsl-image-full-build-error-for-t1040qds-board/m-p/313592#M531</guid>
      <dc:creator>chandrashekhar</dc:creator>
      <dc:date>2014-06-30T05:09:59Z</dc:date>
    </item>
    <item>
      <title>Re: bitbake fsl-image-full build error for t1040qds board</title>
      <link>https://community.nxp.com/t5/QorIQ/bitbake-fsl-image-full-build-error-for-t1040qds-board/m-p/313593#M532</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Chandra,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Previously a customer reported a similar problem in SDK 1.4, please check whether the following workaround could help you&lt;/P&gt;&lt;OL style="list-style-type: decimal;"&gt;&lt;LI&gt;$ bitbake netcf -c clean&lt;/LI&gt;&lt;LI&gt;$ bitbake netcf -c patch&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Go to netcf source in build_&amp;lt;machine&amp;gt;_release/tmp/work/ppce5500-fsl-linux/netcf/0.2.2+gitAUTOINC+2b0d9ca226c13d7150382367f62b256bdb2db5ef-r1/git/.&lt;/P&gt;&lt;P&gt;&amp;nbsp; 3. Modify the url in the file .gitmodules as " &lt;A href="http://repo.or.cz/r/gnulib.git"&gt;http://repo.or.cz/r/gnulib.git&lt;/A&gt;"&lt;/P&gt;&lt;P&gt;&amp;nbsp; 4. $ bitbake netcf -c configure -f&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping Wang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Jul 2014 08:49:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/bitbake-fsl-image-full-build-error-for-t1040qds-board/m-p/313593#M532</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2014-07-02T08:49:25Z</dc:date>
    </item>
    <item>
      <title>Re: bitbake fsl-image-full build error for t1040qds board</title>
      <link>https://community.nxp.com/t5/QorIQ/bitbake-fsl-image-full-build-error-for-t1040qds-board/m-p/313594#M533</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Thanks Yiping,&lt;/P&gt;&lt;P&gt;Yes, the above mentioned steps are working for me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Chandra&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Jul 2014 10:24:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/bitbake-fsl-image-full-build-error-for-t1040qds-board/m-p/313594#M533</guid>
      <dc:creator>chandrashekhar</dc:creator>
      <dc:date>2014-07-02T10:24:40Z</dc:date>
    </item>
  </channel>
</rss>