<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: We are using LS1043A, in that SerDes Lane A as configured as XFI and routed through a backplane to another Daughter card(same board works for Redundant purpose in our system) where the destination is also LS1043A. in QorIQ</title>
    <link>https://community.nxp.com/t5/QorIQ/We-are-using-LS1043A-in-that-SerDes-Lane-A-as-configured-as-XFI/m-p/642289#M4696</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In short, yes, direct connection is possible and the maximum speed can &lt;BR /&gt;be achieved. More detailed recommendations require making references&lt;BR /&gt;to NDA materials and cannot be placed here. Consider opening a&lt;BR /&gt;support case:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-wiki-small" data-containerid="2001" data-containertype="14" data-objectid="329745" data-objecttype="102" href="https://community.nxp.com/docs/DOC-329745"&gt;https://community.nxp.com/docs/DOC-329745&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Platon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 05 Dec 2016 16:17:30 GMT</pubDate>
    <dc:creator>bpe</dc:creator>
    <dc:date>2016-12-05T16:17:30Z</dc:date>
    <item>
      <title>We are using LS1043A, in that SerDes Lane A as configured as XFI and routed through a backplane to another Daughter card(same board works for Redundant purpose in our system) where the destination is also LS1043A.</title>
      <link>https://community.nxp.com/t5/QorIQ/We-are-using-LS1043A-in-that-SerDes-Lane-A-as-configured-as-XFI/m-p/642287#M4694</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If we route XFI of LS1043A in above senario will that work in 10Gb/s? Can the speed be achieved? Do we need to take any precautions while routing it?&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Dec 2016 12:04:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/We-are-using-LS1043A-in-that-SerDes-Lane-A-as-configured-as-XFI/m-p/642287#M4694</guid>
      <dc:creator>logeshs</dc:creator>
      <dc:date>2016-12-02T12:04:23Z</dc:date>
    </item>
    <item>
      <title>Re: We are using LS1043A, in that SerDes Lane A as configured as XFI and routed through a backplane to another Daughter card(same board works for Redundant purpose in our system) where the destination is also LS1043A.</title>
      <link>https://community.nxp.com/t5/QorIQ/We-are-using-LS1043A-in-that-SerDes-Lane-A-as-configured-as-XFI/m-p/642288#M4695</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have not connected any device in between. Interface will be like this XFI from LS1043A of Board A to XFI of LS1043A of Board B &amp;nbsp;connected through a Backplane. Kindly update me can we achieve 10Gb/s in this connection?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Dec 2016 06:04:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/We-are-using-LS1043A-in-that-SerDes-Lane-A-as-configured-as-XFI/m-p/642288#M4695</guid>
      <dc:creator>logeshs</dc:creator>
      <dc:date>2016-12-05T06:04:14Z</dc:date>
    </item>
    <item>
      <title>Re: We are using LS1043A, in that SerDes Lane A as configured as XFI and routed through a backplane to another Daughter card(same board works for Redundant purpose in our system) where the destination is also LS1043A.</title>
      <link>https://community.nxp.com/t5/QorIQ/We-are-using-LS1043A-in-that-SerDes-Lane-A-as-configured-as-XFI/m-p/642289#M4696</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In short, yes, direct connection is possible and the maximum speed can &lt;BR /&gt;be achieved. More detailed recommendations require making references&lt;BR /&gt;to NDA materials and cannot be placed here. Consider opening a&lt;BR /&gt;support case:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-wiki-small" data-containerid="2001" data-containertype="14" data-objectid="329745" data-objecttype="102" href="https://community.nxp.com/docs/DOC-329745"&gt;https://community.nxp.com/docs/DOC-329745&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Platon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Dec 2016 16:17:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/We-are-using-LS1043A-in-that-SerDes-Lane-A-as-configured-as-XFI/m-p/642289#M4696</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2016-12-05T16:17:30Z</dc:date>
    </item>
    <item>
      <title>Re: We are using LS1043A, in that SerDes Lane A as configured as XFI and routed through a backplane to another Daughter card(same board works for Redundant purpose in our system) where the destination is also LS1043A.</title>
      <link>https://community.nxp.com/t5/QorIQ/We-are-using-LS1043A-in-that-SerDes-Lane-A-as-configured-as-XFI/m-p/642290#M4697</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your clarification.&lt;/P&gt;&lt;P&gt;We do have existing NDA with NXP, can you tell me how can you share those documents?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Dec 2016 07:58:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/We-are-using-LS1043A-in-that-SerDes-Lane-A-as-configured-as-XFI/m-p/642290#M4697</guid>
      <dc:creator>logeshs</dc:creator>
      <dc:date>2016-12-06T07:58:06Z</dc:date>
    </item>
  </channel>
</rss>