<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic T1022 serdes configuration 0x81 in QorIQ</title>
    <link>https://community.nxp.com/t5/QorIQ/T1022-serdes-configuration-0x81/m-p/1832071#M11940</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are using T1022 processor. I am able to boot the pro&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="IMG20240319112341.jpg" style="width: 4000px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/269499i9D9AEB0FDBA9E99A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="IMG20240319112341.jpg" alt="IMG20240319112341.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;cessor. Board is working fine for serdes configuration 0x85/0x87 etc. but when I try to use 0x81 , it is showing as serdes configuration is not valid. I have enabled both the serdes pll. No pll is power down as was done for 85 and 87. Please see the log screenshot.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please suggest if we need to do any other changes to RCW for the same.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 20 Mar 2024 13:29:59 GMT</pubDate>
    <dc:creator>nikhiljain</dc:creator>
    <dc:date>2024-03-20T13:29:59Z</dc:date>
    <item>
      <title>T1022 serdes configuration 0x81</title>
      <link>https://community.nxp.com/t5/QorIQ/T1022-serdes-configuration-0x81/m-p/1832071#M11940</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are using T1022 processor. I am able to boot the pro&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="IMG20240319112341.jpg" style="width: 4000px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/269499i9D9AEB0FDBA9E99A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="IMG20240319112341.jpg" alt="IMG20240319112341.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;cessor. Board is working fine for serdes configuration 0x85/0x87 etc. but when I try to use 0x81 , it is showing as serdes configuration is not valid. I have enabled both the serdes pll. No pll is power down as was done for 85 and 87. Please see the log screenshot.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please suggest if we need to do any other changes to RCW for the same.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Mar 2024 13:29:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/T1022-serdes-configuration-0x81/m-p/1832071#M11940</guid>
      <dc:creator>nikhiljain</dc:creator>
      <dc:date>2024-03-20T13:29:59Z</dc:date>
    </item>
    <item>
      <title>Re: T1022 serdes configuration 0x81</title>
      <link>https://community.nxp.com/t5/QorIQ/T1022-serdes-configuration-0x81/m-p/1835668#M11947</link>
      <description>&lt;P&gt;Hello,&amp;nbsp;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Supported protocols are defined in the &lt;A href="https://elixir.bootlin.com/u-boot/latest/source/arch/powerpc/cpu/mpc85xx/t1040_serdes.c" target="_self"&gt;u-boot/arch/powerpc/cpu/mpc85xx/t1040_serdes.c&lt;/A&gt;:&lt;/P&gt;</description>
      <pubDate>Tue, 26 Mar 2024 19:11:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/T1022-serdes-configuration-0x81/m-p/1835668#M11947</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2024-03-26T19:11:47Z</dc:date>
    </item>
    <item>
      <title>Re: T1022 serdes configuration 0x81</title>
      <link>https://community.nxp.com/t5/QorIQ/T1022-serdes-configuration-0x81/m-p/1835863#M11949</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Serdes protocols defined in the file at the below link do not have all the supported configurations but mentioned in the RM. Like serdes configuration - 0x88 , 0x45 , 0x81 are not defined in the file. Do we need to add them manually in the code and check if that works ?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="0x81 is valid according to this." style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/270565i5058B83D4C0DEE7F/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capturen.JPG" alt="0x81 is valid according to this." /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;0x81 is valid according to this.&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="0x81 is not defined here." style="width: 930px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/270566iB4E6E8ED6B689DCC/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capturem.JPG" alt="0x81 is not defined here." /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;0x81 is not defined here.&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Mar 2024 02:42:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/T1022-serdes-configuration-0x81/m-p/1835863#M11949</guid>
      <dc:creator>nikhiljain</dc:creator>
      <dc:date>2024-03-27T02:42:44Z</dc:date>
    </item>
  </channel>
</rss>