<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Questions regarding GPIO2 EVDD power setting in QorIQ</title>
    <link>https://community.nxp.com/t5/QorIQ/Questions-regarding-GPIO2-EVDD-power-setting/m-p/1737388#M11723</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224115"&gt;@RT25&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;Yes, there is a possibility of malfunction. NXP recommends following the document for the guaranteed function of the device.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Mrudang&lt;/P&gt;</description>
    <pubDate>Wed, 11 Oct 2023 10:06:27 GMT</pubDate>
    <dc:creator>mrudangshelat-13</dc:creator>
    <dc:date>2023-10-11T10:06:27Z</dc:date>
    <item>
      <title>Questions regarding GPIO2 EVDD power setting</title>
      <link>https://community.nxp.com/t5/QorIQ/Questions-regarding-GPIO2-EVDD-power-setting/m-p/1736503#M11720</link>
      <description>&lt;P&gt;Hi All,&lt;SPAN&gt;We are developing the custom board using LS1046ASN8.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Then we are using the functionality of GPIO2.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Currently, 3.3V is input to the EVDD power supply terminal.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;In addition, in the prototype test, the 439th and 440th bit settings (EVDD_VSEL) of RCW were I set it to "00"=1.8V and it started up.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is there a possibility of a malfunction in this case?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 10 Oct 2023 10:27:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/Questions-regarding-GPIO2-EVDD-power-setting/m-p/1736503#M11720</guid>
      <dc:creator>RT25</dc:creator>
      <dc:date>2023-10-10T10:27:58Z</dc:date>
    </item>
    <item>
      <title>Re: Questions regarding GPIO2 EVDD power setting</title>
      <link>https://community.nxp.com/t5/QorIQ/Questions-regarding-GPIO2-EVDD-power-setting/m-p/1737388#M11723</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224115"&gt;@RT25&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;Yes, there is a possibility of malfunction. NXP recommends following the document for the guaranteed function of the device.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Mrudang&lt;/P&gt;</description>
      <pubDate>Wed, 11 Oct 2023 10:06:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/Questions-regarding-GPIO2-EVDD-power-setting/m-p/1737388#M11723</guid>
      <dc:creator>mrudangshelat-13</dc:creator>
      <dc:date>2023-10-11T10:06:27Z</dc:date>
    </item>
    <item>
      <title>Re: Questions regarding GPIO2 EVDD power setting</title>
      <link>https://community.nxp.com/t5/QorIQ/Questions-regarding-GPIO2-EVDD-power-setting/m-p/1737439#M11724</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203818"&gt;@mrudangshelat-13&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for teaching me.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;For example, if I set the RCW to 1.8V, does this mean that the GPIO output stage circuit (the MOSFET upper side of the push-pull circuit, etc.) will be damaged? Or will the internal circuit be damaged?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;(Actually, the terminal in question was not working properly, so I was wondering if it was possible to restore the CPU of the board I created. I wish things would go back to normal if I changed the settings to 3.3V correctly, but for now the problem remains.)&lt;/P&gt;</description>
      <pubDate>Wed, 11 Oct 2023 11:26:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/Questions-regarding-GPIO2-EVDD-power-setting/m-p/1737439#M11724</guid>
      <dc:creator>RT25</dc:creator>
      <dc:date>2023-10-11T11:26:52Z</dc:date>
    </item>
    <item>
      <title>Re: Questions regarding GPIO2 EVDD power setting</title>
      <link>https://community.nxp.com/t5/QorIQ/Questions-regarding-GPIO2-EVDD-power-setting/m-p/1738488#M11725</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/224115"&gt;@RT25&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;I suggest using the correct RCW configuration and testing the board again to confirm that the pin is okay. However, using the incorrect RCW might lead to malfunction. There is a rare chance of damage in this kind of situation.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Mrudang&lt;/P&gt;</description>
      <pubDate>Thu, 12 Oct 2023 09:27:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/Questions-regarding-GPIO2-EVDD-power-setting/m-p/1738488#M11725</guid>
      <dc:creator>mrudangshelat-13</dc:creator>
      <dc:date>2023-10-12T09:27:05Z</dc:date>
    </item>
  </channel>
</rss>