<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS1026 I2C JTAG in QorIQ</title>
    <link>https://community.nxp.com/t5/QorIQ/LS1026-I2C-JTAG/m-p/1420364#M10819</link>
    <description>&lt;P&gt;The test engineer found the solution:&lt;/P&gt;&lt;P&gt;Not like the LS1046, the LS1026 I2C/UART Power Bank need to be Configured before it can be used in JTAG Mode, so added extra command before each test that use this Power Bank.&lt;/P&gt;</description>
    <pubDate>Mon, 28 Feb 2022 08:01:51 GMT</pubDate>
    <dc:creator>itzik1</dc:creator>
    <dc:date>2022-02-28T08:01:51Z</dc:date>
    <item>
      <title>LS1026 I2C JTAG</title>
      <link>https://community.nxp.com/t5/QorIQ/LS1026-I2C-JTAG/m-p/1418114#M10810</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Could anybody toggle I2C pins on LS1026 during JTAG test?&lt;/P&gt;&lt;P&gt;These are not toggling in my board while in operational mode all is ok to all I2C devices.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Itzik&lt;/P&gt;</description>
      <pubDate>Wed, 23 Feb 2022 09:30:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/LS1026-I2C-JTAG/m-p/1418114#M10810</guid>
      <dc:creator>itzik1</dc:creator>
      <dc:date>2022-02-23T09:30:44Z</dc:date>
    </item>
    <item>
      <title>Re: LS1026 I2C JTAG</title>
      <link>https://community.nxp.com/t5/QorIQ/LS1026-I2C-JTAG/m-p/1419106#M10814</link>
      <description>&lt;P&gt;Test other pins on your LS1026a board. Perhaps there are a few similar pins on your board.&lt;/P&gt;
&lt;P&gt;If the LS1026a I2C correctly works in normal mode, your JTAG test setting should be checked.&lt;/P&gt;</description>
      <pubDate>Thu, 24 Feb 2022 13:13:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/LS1026-I2C-JTAG/m-p/1419106#M10814</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2022-02-24T13:13:34Z</dc:date>
    </item>
    <item>
      <title>Re: LS1026 I2C JTAG</title>
      <link>https://community.nxp.com/t5/QorIQ/LS1026-I2C-JTAG/m-p/1419138#M10815</link>
      <description>&lt;P&gt;Pins have been verified , we have checked with&amp;nbsp; a scope and found pins are not toggling at all in JTAG Mode while other pins are toggling.&lt;/P&gt;&lt;P&gt;I2C pins are working fine in normal mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 24 Feb 2022 14:07:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/LS1026-I2C-JTAG/m-p/1419138#M10815</guid>
      <dc:creator>itzik1</dc:creator>
      <dc:date>2022-02-24T14:07:30Z</dc:date>
    </item>
    <item>
      <title>Re: LS1026 I2C JTAG</title>
      <link>https://community.nxp.com/t5/QorIQ/LS1026-I2C-JTAG/m-p/1419159#M10816</link>
      <description>&lt;P&gt;Other bus like DDR, SPI are function OK in JTAG&lt;/P&gt;&lt;P&gt;Only problem with DVDD pins (I2C, UART)&lt;/P&gt;</description>
      <pubDate>Thu, 24 Feb 2022 14:32:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/LS1026-I2C-JTAG/m-p/1419159#M10816</guid>
      <dc:creator>itzik1</dc:creator>
      <dc:date>2022-02-24T14:32:47Z</dc:date>
    </item>
    <item>
      <title>Re: LS1026 I2C JTAG</title>
      <link>https://community.nxp.com/t5/QorIQ/LS1026-I2C-JTAG/m-p/1420364#M10819</link>
      <description>&lt;P&gt;The test engineer found the solution:&lt;/P&gt;&lt;P&gt;Not like the LS1046, the LS1026 I2C/UART Power Bank need to be Configured before it can be used in JTAG Mode, so added extra command before each test that use this Power Bank.&lt;/P&gt;</description>
      <pubDate>Mon, 28 Feb 2022 08:01:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/LS1026-I2C-JTAG/m-p/1420364#M10819</guid>
      <dc:creator>itzik1</dc:creator>
      <dc:date>2022-02-28T08:01:51Z</dc:date>
    </item>
  </channel>
</rss>