<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic sd card error in QorIQ</title>
    <link>https://community.nxp.com/t5/QorIQ/sd-card-error/m-p/1330076#M10476</link>
    <description>&lt;P&gt;I am working custom card with LS1046a processor. After generating SD card image for my custom card , when i try to boot with SD card with tiny linux, board comes up alright but its not detecting mmcblk0.&lt;/P&gt;&lt;P&gt;In log , it shows this error:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;mmc0: error -110 whilst initialising SD card&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Also at uboot , its able to detect the 4 partitions.&lt;/P&gt;&lt;P&gt;Scanning mmc 0:1...&lt;BR /&gt;Scanning mmc 0:2...&lt;BR /&gt;Scanning mmc 0:3...&lt;BR /&gt;Scanning mmc 0:4...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kindly help&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 26 Aug 2021 06:51:49 GMT</pubDate>
    <dc:creator>rashmikj</dc:creator>
    <dc:date>2021-08-26T06:51:49Z</dc:date>
    <item>
      <title>sd card error</title>
      <link>https://community.nxp.com/t5/QorIQ/sd-card-error/m-p/1330076#M10476</link>
      <description>&lt;P&gt;I am working custom card with LS1046a processor. After generating SD card image for my custom card , when i try to boot with SD card with tiny linux, board comes up alright but its not detecting mmcblk0.&lt;/P&gt;&lt;P&gt;In log , it shows this error:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;mmc0: error -110 whilst initialising SD card&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Also at uboot , its able to detect the 4 partitions.&lt;/P&gt;&lt;P&gt;Scanning mmc 0:1...&lt;BR /&gt;Scanning mmc 0:2...&lt;BR /&gt;Scanning mmc 0:3...&lt;BR /&gt;Scanning mmc 0:4...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kindly help&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 26 Aug 2021 06:51:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/sd-card-error/m-p/1330076#M10476</guid>
      <dc:creator>rashmikj</dc:creator>
      <dc:date>2021-08-26T06:51:49Z</dc:date>
    </item>
    <item>
      <title>Re: sd card error</title>
      <link>https://community.nxp.com/t5/QorIQ/sd-card-error/m-p/1331424#M10486</link>
      <description>&lt;P&gt;It looks like that image in not correctly installed on your SD card.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Is there problem for booting from this SD card on your board?&lt;/P&gt;
&lt;P&gt;Use "flex-installer" for preparing SD card.&lt;/P&gt;
&lt;P&gt;The following command also can be used for writing image file to SD card on your PC:&lt;/P&gt;
&lt;P&gt;sudo dd if=firmware_ls1046ardb_uboot_sdboot.img of=/dev/sdb bs=512 seek=8&lt;/P&gt;</description>
      <pubDate>Mon, 30 Aug 2021 04:28:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/sd-card-error/m-p/1331424#M10486</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2021-08-30T04:28:15Z</dc:date>
    </item>
    <item>
      <title>Re: sd card error</title>
      <link>https://community.nxp.com/t5/QorIQ/sd-card-error/m-p/1335018#M10521</link>
      <description>Booting with tiny linux with SD card is okay. But after that when i give the command fdisk -l to see the memory, am not able to see the mmcblk0.</description>
      <pubDate>Sat, 04 Sep 2021 10:09:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/sd-card-error/m-p/1335018#M10521</guid>
      <dc:creator>rashmikj</dc:creator>
      <dc:date>2021-09-04T10:09:41Z</dc:date>
    </item>
    <item>
      <title>Re: sd card error</title>
      <link>https://community.nxp.com/t5/QorIQ/sd-card-error/m-p/1337539#M10532</link>
      <description>&lt;P&gt;Attached file shows message log for LSDK 2004 and the "fdisk -l" command.&lt;/P&gt;
&lt;P&gt;It looks like that there is no similar problem for last version of LSDK.&lt;/P&gt;</description>
      <pubDate>Thu, 09 Sep 2021 08:00:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/sd-card-error/m-p/1337539#M10532</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2021-09-09T08:00:36Z</dc:date>
    </item>
  </channel>
</rss>