<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LSDK 20.12 u-boot debug print in QorIQ</title>
    <link>https://community.nxp.com/t5/QorIQ/LSDK-20-12-u-boot-debug-print/m-p/1329379#M10472</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using FRWY-LS1046A board with LSDK 20.12 release. I want to print out DDR related configurations to serial port. (teraterm or putty) So, I added below debug definitions at the top of&amp;nbsp;u-boot/drivers/ddr/fsl/ctrl_regs.c file. The flex-builder and flex-installer were used for bootable SD card according to the FRWY-LS1046A BSP user guide. The SD booting is still working but it doesn't show any expected log message from many debug() macros in the c-code. Could you help me for this?&lt;/P&gt;&lt;P&gt;#define DEBUG&lt;BR /&gt;#undef CONFIG_LOGLEVEL&lt;BR /&gt;#define CONFIG_LOGLEVEL 8&lt;BR /&gt;#include &amp;lt;common.h&amp;gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Jeff&lt;/P&gt;</description>
    <pubDate>Wed, 25 Aug 2021 10:10:48 GMT</pubDate>
    <dc:creator>jekim</dc:creator>
    <dc:date>2021-08-25T10:10:48Z</dc:date>
    <item>
      <title>LSDK 20.12 u-boot debug print</title>
      <link>https://community.nxp.com/t5/QorIQ/LSDK-20-12-u-boot-debug-print/m-p/1329379#M10472</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using FRWY-LS1046A board with LSDK 20.12 release. I want to print out DDR related configurations to serial port. (teraterm or putty) So, I added below debug definitions at the top of&amp;nbsp;u-boot/drivers/ddr/fsl/ctrl_regs.c file. The flex-builder and flex-installer were used for bootable SD card according to the FRWY-LS1046A BSP user guide. The SD booting is still working but it doesn't show any expected log message from many debug() macros in the c-code. Could you help me for this?&lt;/P&gt;&lt;P&gt;#define DEBUG&lt;BR /&gt;#undef CONFIG_LOGLEVEL&lt;BR /&gt;#define CONFIG_LOGLEVEL 8&lt;BR /&gt;#include &amp;lt;common.h&amp;gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Jeff&lt;/P&gt;</description>
      <pubDate>Wed, 25 Aug 2021 10:10:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/LSDK-20-12-u-boot-debug-print/m-p/1329379#M10472</guid>
      <dc:creator>jekim</dc:creator>
      <dc:date>2021-08-25T10:10:48Z</dc:date>
    </item>
    <item>
      <title>Re: LSDK 20.12 u-boot debug print</title>
      <link>https://community.nxp.com/t5/QorIQ/LSDK-20-12-u-boot-debug-print/m-p/1329445#M10473</link>
      <description>&lt;P&gt;LSDK 20.12 boot sequence in TF-A based. DDR memory initialization is performed&lt;BR /&gt;by TF-A code that executes before control is transferred to u-Boot. For this&lt;BR /&gt;reason, u-Boot DDR memory initialization routines are bypassed.&lt;/P&gt;
&lt;P&gt;Suggestions:&lt;BR /&gt;&lt;BR /&gt;1. Study LSDK User Guide Section 5.1.&lt;/P&gt;
&lt;P&gt;2. Use a JTAG based, source level debugger to debug your code.&lt;/P&gt;
&lt;P&gt;3. Refer to the right software package:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&amp;nbsp; &lt;A href="https://source.codeaurora.org/external/qoriq/qoriq-components/atf" target="_blank"&gt;https://source.codeaurora.org/external/qoriq/qoriq-components/atf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Platon&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 25 Aug 2021 12:19:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/LSDK-20-12-u-boot-debug-print/m-p/1329445#M10473</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2021-08-25T12:19:36Z</dc:date>
    </item>
    <item>
      <title>Re: LSDK 20.12 u-boot debug print</title>
      <link>https://community.nxp.com/t5/QorIQ/LSDK-20-12-u-boot-debug-print/m-p/1329847#M10474</link>
      <description>&lt;P&gt;Hi bpe,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for the answer. The debug print is working in TF-A code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Jeff&lt;/P&gt;</description>
      <pubDate>Thu, 02 Sep 2021 09:12:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/LSDK-20-12-u-boot-debug-print/m-p/1329847#M10474</guid>
      <dc:creator>jekim</dc:creator>
      <dc:date>2021-09-02T09:12:21Z</dc:date>
    </item>
  </channel>
</rss>