<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Layerscape PCIe Endpoint Development Boards in QorIQ</title>
    <link>https://community.nxp.com/t5/QorIQ/Layerscape-PCIe-Endpoint-Development-Boards/m-p/1262032#M10178</link>
    <description>&lt;P&gt;Are there any NXP or third-party development boards that feature a Layerscape processor such as the LS1021A as a PCIe Endpoint?&amp;nbsp; All of the NXP development boards focus on the LS processors as PCIe RC.&lt;/P&gt;&lt;P&gt;There is this note here on modifying the LS1046A-RDB board so that mPCIe Slot 2 can be converted from RC to EP mode:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/QorIQ-Knowledge-Base/LS1046A-RDB-in-PCIe-Endpoint-Mode/ta-p/1107415" target="_blank"&gt;https://community.nxp.com/t5/QorIQ-Knowledge-Base/LS1046A-RDB-in-PCIe-Endpoint-Mode/ta-p/1107415&lt;/A&gt;&lt;/P&gt;&lt;P&gt;But even with that change, you would be left with a female mPCIe Slot on the board.&amp;nbsp; I could not find an adapter that would allow you to connect that mPCIe Slot to a PCIe x1 connector on a desktop PC.&lt;/P&gt;&lt;P&gt;If we wanted to debug a PCIe driver to a Layerscape processor, it would be better to do so on a development board before performing a custom design.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 14 Apr 2021 13:05:21 GMT</pubDate>
    <dc:creator>mikedubya</dc:creator>
    <dc:date>2021-04-14T13:05:21Z</dc:date>
    <item>
      <title>Layerscape PCIe Endpoint Development Boards</title>
      <link>https://community.nxp.com/t5/QorIQ/Layerscape-PCIe-Endpoint-Development-Boards/m-p/1262032#M10178</link>
      <description>&lt;P&gt;Are there any NXP or third-party development boards that feature a Layerscape processor such as the LS1021A as a PCIe Endpoint?&amp;nbsp; All of the NXP development boards focus on the LS processors as PCIe RC.&lt;/P&gt;&lt;P&gt;There is this note here on modifying the LS1046A-RDB board so that mPCIe Slot 2 can be converted from RC to EP mode:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/t5/QorIQ-Knowledge-Base/LS1046A-RDB-in-PCIe-Endpoint-Mode/ta-p/1107415" target="_blank"&gt;https://community.nxp.com/t5/QorIQ-Knowledge-Base/LS1046A-RDB-in-PCIe-Endpoint-Mode/ta-p/1107415&lt;/A&gt;&lt;/P&gt;&lt;P&gt;But even with that change, you would be left with a female mPCIe Slot on the board.&amp;nbsp; I could not find an adapter that would allow you to connect that mPCIe Slot to a PCIe x1 connector on a desktop PC.&lt;/P&gt;&lt;P&gt;If we wanted to debug a PCIe driver to a Layerscape processor, it would be better to do so on a development board before performing a custom design.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Apr 2021 13:05:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/Layerscape-PCIe-Endpoint-Development-Boards/m-p/1262032#M10178</guid>
      <dc:creator>mikedubya</dc:creator>
      <dc:date>2021-04-14T13:05:21Z</dc:date>
    </item>
    <item>
      <title>Re: Layerscape PCIe Endpoint Development Boards</title>
      <link>https://community.nxp.com/t5/QorIQ/Layerscape-PCIe-Endpoint-Development-Boards/m-p/1262144#M10180</link>
      <description>&lt;P&gt;PCIe EP mode is not supported by LS1021A - refer to the QorIQ LS1021A Reference Manual, 28.2.2 Features:&lt;/P&gt;
&lt;P&gt;"Supports Root Complex (RC) mode"&lt;/P&gt;
&lt;P&gt;EP mode is not announced.&lt;/P&gt;</description>
      <pubDate>Wed, 14 Apr 2021 16:31:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/Layerscape-PCIe-Endpoint-Development-Boards/m-p/1262144#M10180</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-04-14T16:31:13Z</dc:date>
    </item>
    <item>
      <title>Re: Layerscape PCIe Endpoint Development Boards</title>
      <link>https://community.nxp.com/t5/QorIQ/Layerscape-PCIe-Endpoint-Development-Boards/m-p/1262195#M10181</link>
      <description>&lt;P&gt;Is PCIe EP mode supported on any of the Layerscape processors?&amp;nbsp; From the KnowledgeBase note, it looks like it is supported on the LS1046.&lt;/P&gt;&lt;P&gt;Related to that, are there any NXP or third-party boards that have a PCIe x1 or x4 interface to a Layerscape processor in PCIe EP mode?&lt;/P&gt;</description>
      <pubDate>Wed, 14 Apr 2021 17:15:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/Layerscape-PCIe-Endpoint-Development-Boards/m-p/1262195#M10181</guid>
      <dc:creator>mikedubya</dc:creator>
      <dc:date>2021-04-14T17:15:58Z</dc:date>
    </item>
    <item>
      <title>Re: Layerscape PCIe Endpoint Development Boards</title>
      <link>https://community.nxp.com/t5/QorIQ/Layerscape-PCIe-Endpoint-Development-Boards/m-p/1262216#M10182</link>
      <description>&lt;DIV class="lia-message-body lia-component-message-view-widget-body lia-component-body-signature-highlight-escalation lia-component-message-view-widget-body-signature-highlight-escalation"&gt;&lt;DIV class="lia-message-body-content"&gt;&lt;P&gt;Is PCIe EP mode supported on any of the Layerscape processors?&amp;nbsp; From the KnowledgeBase note, it looks like it is supported on the LS1046.&lt;/P&gt;&lt;P&gt;Related to that, are there any NXP or third-party boards that have a PCIe x1 or x4 interface to a Layerscape processor in PCIe EP mode?&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Wed, 14 Apr 2021 17:46:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/Layerscape-PCIe-Endpoint-Development-Boards/m-p/1262216#M10182</guid>
      <dc:creator>mikedubya</dc:creator>
      <dc:date>2021-04-14T17:46:08Z</dc:date>
    </item>
    <item>
      <title>Re: Layerscape PCIe Endpoint Development Boards</title>
      <link>https://community.nxp.com/t5/QorIQ/Layerscape-PCIe-Endpoint-Development-Boards/m-p/1262276#M10183</link>
      <description>&lt;P&gt;Based upon a couple of sources (Table 4 of the Layerscape SDK for Yocto and Linux v5.12-rc7 Documentation/devicetree/bindings/pci/layerscape-pci.txt) it looks like the Layerscape processors that support PCIe EP mode are:&lt;/P&gt;&lt;P&gt;LS1046A&lt;BR /&gt;LS1088A&lt;BR /&gt;LS2088A&lt;BR /&gt;LX2160A (r2)&lt;/P&gt;&lt;P&gt;But I still could not find an NXP or third-party PCIe x1 or x4 development board that exercises this interface.&lt;/P&gt;</description>
      <pubDate>Wed, 14 Apr 2021 19:16:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/Layerscape-PCIe-Endpoint-Development-Boards/m-p/1262276#M10183</guid>
      <dc:creator>mikedubya</dc:creator>
      <dc:date>2021-04-14T19:16:51Z</dc:date>
    </item>
    <item>
      <title>Re: Layerscape PCIe Endpoint Development Boards</title>
      <link>https://community.nxp.com/t5/QorIQ/Layerscape-PCIe-Endpoint-Development-Boards/m-p/1262404#M10184</link>
      <description>&lt;P&gt;I'm not aware about evaluation boards for LS1046A, LS1088A, LS2088A, LX2160A having PCIe EP.&lt;/P&gt;</description>
      <pubDate>Thu, 15 Apr 2021 02:20:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/QorIQ/Layerscape-PCIe-Endpoint-Development-Boards/m-p/1262404#M10184</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-04-15T02:20:45Z</dc:date>
    </item>
  </channel>
</rss>