<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>QonvergeのトピックThe differences between alternate functions and muliplex options</title>
    <link>https://community.nxp.com/t5/Qonverge/The-differences-between-alternate-functions-and-muliplex-options/m-p/372871#M97</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,everyone!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; In P1021RM,table3-10 (page 127) has listed the QUICC Engine Multiplex pins.For example, CE_PA0 has alternative functon of LAD8,but in table 3-7(page 119),CPPARAx[SELn] has no option for LAD8.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1. That mean that,i can use LAD8 and QUICC sub-function&amp;nbsp; simultaneously ?for e.g.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; for CE_PA0 ,&amp;nbsp; I set CPPARAx[SELn] to 11,then PA0 used for UPC1_S_TxADDR[4]. Following a utopia interface opration，the CPU can initial a eLBC access through LAD8 without any change of CPPARAx[SELn] value?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.What's the defferences of 'alternate function' and 'muliplex option'?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 03 Nov 2014 08:46:57 GMT</pubDate>
    <dc:creator>xiangwei</dc:creator>
    <dc:date>2014-11-03T08:46:57Z</dc:date>
    <item>
      <title>The differences between alternate functions and muliplex options</title>
      <link>https://community.nxp.com/t5/Qonverge/The-differences-between-alternate-functions-and-muliplex-options/m-p/372871#M97</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,everyone!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; In P1021RM,table3-10 (page 127) has listed the QUICC Engine Multiplex pins.For example, CE_PA0 has alternative functon of LAD8,but in table 3-7(page 119),CPPARAx[SELn] has no option for LAD8.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1. That mean that,i can use LAD8 and QUICC sub-function&amp;nbsp; simultaneously ?for e.g.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; for CE_PA0 ,&amp;nbsp; I set CPPARAx[SELn] to 11,then PA0 used for UPC1_S_TxADDR[4]. Following a utopia interface opration，the CPU can initial a eLBC access through LAD8 without any change of CPPARAx[SELn] value?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2.What's the defferences of 'alternate function' and 'muliplex option'?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Nov 2014 08:46:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Qonverge/The-differences-between-alternate-functions-and-muliplex-options/m-p/372871#M97</guid>
      <dc:creator>xiangwei</dc:creator>
      <dc:date>2014-11-03T08:46:57Z</dc:date>
    </item>
    <item>
      <title>Re: The differences between alternate functions and muliplex options</title>
      <link>https://community.nxp.com/t5/Qonverge/The-differences-between-alternate-functions-and-muliplex-options/m-p/372872#M98</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;P1021 QE pins are muxed with non-QE signals. The selection between QE and non-QE function is performed via PMUXCR bits.&lt;/P&gt;&lt;P&gt;Please, read description of QE1 field in RM Section 20.5.7&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;What's the defferences of 'alternate function' and 'muliplex option'&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PMUXCR selects between QE and non-QE alternate functions. &lt;/P&gt;&lt;P&gt;CPPARAx provides further selection between QE options.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do not not attach particular importance to the terms. They are interchangeable.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Nov 2014 07:31:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Qonverge/The-differences-between-alternate-functions-and-muliplex-options/m-p/372872#M98</guid>
      <dc:creator>LPP</dc:creator>
      <dc:date>2014-11-05T07:31:30Z</dc:date>
    </item>
  </channel>
</rss>