<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>QonvergeのトピックRe: ,b4860qds ethernet interface speed</title>
    <link>https://community.nxp.com/t5/Qonverge/b4860qds-ethernet-interface-speed/m-p/486579#M210</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1) Please provide U-Boot booting log, so it will be possible to check RCW.&lt;/P&gt;&lt;P&gt;2) Please address the request to the Wind RIver technical support.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Feb 2016 05:07:32 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2016-02-04T05:07:32Z</dc:date>
    <item>
      <title>,b4860qds ethernet interface speed</title>
      <link>https://community.nxp.com/t5/Qonverge/b4860qds-ethernet-interface-speed/m-p/486578#M209</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have one b4860qds board currently working. There are three Ethernet ports in it: J16 (100Mbps), J18 and J20 (both 1000Mbps). The only one working by default is J16, which is the 100Mbps, ergo the slower one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I enable J18 or J20 so that I can work with them as well? Does that depend on the BSP of the OS I am running? I am currently running VxWorks 653 2.5 and I wonder if this is something I need to tell to the BSP guys or something I can do directly in the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Feb 2016 02:36:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Qonverge/b4860qds-ethernet-interface-speed/m-p/486578#M209</guid>
      <dc:creator>victorgomez</dc:creator>
      <dc:date>2016-02-04T02:36:13Z</dc:date>
    </item>
    <item>
      <title>Re: ,b4860qds ethernet interface speed</title>
      <link>https://community.nxp.com/t5/Qonverge/b4860qds-ethernet-interface-speed/m-p/486579#M210</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1) Please provide U-Boot booting log, so it will be possible to check RCW.&lt;/P&gt;&lt;P&gt;2) Please address the request to the Wind RIver technical support.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Feb 2016 05:07:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Qonverge/b4860qds-ethernet-interface-speed/m-p/486579#M210</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2016-02-04T05:07:32Z</dc:date>
    </item>
    <item>
      <title>Re: ,b4860qds ethernet interface speed</title>
      <link>https://community.nxp.com/t5/Qonverge/b4860qds-ethernet-interface-speed/m-p/486580#M211</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ufedor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply. I can't get to the u-boot bootloader at the moment, but I will do that. I remember we flashed a new RCW. Are you saying that which interface is used depends on the RCW?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Feb 2016 19:31:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Qonverge/b4860qds-ethernet-interface-speed/m-p/486580#M211</guid>
      <dc:creator>victorgomez</dc:creator>
      <dc:date>2016-02-04T19:31:10Z</dc:date>
    </item>
    <item>
      <title>Re: ,b4860qds ethernet interface speed</title>
      <link>https://community.nxp.com/t5/Qonverge/b4860qds-ethernet-interface-speed/m-p/486581#M212</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The RCW controls SerDes protocols - please refer to the processor's RM for details.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Feb 2016 01:12:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Qonverge/b4860qds-ethernet-interface-speed/m-p/486581#M212</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2016-02-05T01:12:50Z</dc:date>
    </item>
  </channel>
</rss>