<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC Processors中的主题 Re: MPC860 power up problem</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC860-power-up-problem/m-p/352884#M876</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Although I solve the clcok problem, these still no any signals from the UART TXD pin. &lt;/P&gt;&lt;P&gt;The old design had been used for 5 years, the boot and software are the same, the hardware is just re-layout.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Oct 2014 11:11:55 GMT</pubDate>
    <dc:creator>billy_huan</dc:creator>
    <dc:date>2014-10-09T11:11:55Z</dc:date>
    <item>
      <title>MPC860 power up problem</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC860-power-up-problem/m-p/352882#M874</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When I power up the MPC860, the clkout pin will generate a clock switch from 40MHz to 13MHz over and over, which the extal clock source is 40MHz. The MODCK0 is "1" and MODCK1 is "0".&lt;/P&gt;&lt;P&gt;So why would such a case happen? The error hardware configration or the chip itself is bad.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;B.R.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Sep 2014 04:06:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC860-power-up-problem/m-p/352882#M874</guid>
      <dc:creator>billy_huan</dc:creator>
      <dc:date>2014-09-29T04:06:01Z</dc:date>
    </item>
    <item>
      <title>Re: MPC860 power up problem</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC860-power-up-problem/m-p/352883#M875</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could you please describe in more details what you mean by "generate a clock switch from 40MHz to 13MHz over and over" &lt;/P&gt;&lt;P&gt;Do you mean output clock switchs from 40MHz to 13MHz after the power on? Or the clock output remains stable, but the value switches from power-on to power-on cycles?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have scope picture illustrating the problem? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Sep 2014 11:44:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC860-power-up-problem/m-p/352883#M875</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2014-09-29T11:44:48Z</dc:date>
    </item>
    <item>
      <title>Re: MPC860 power up problem</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC860-power-up-problem/m-p/352884#M876</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Although I solve the clcok problem, these still no any signals from the UART TXD pin. &lt;/P&gt;&lt;P&gt;The old design had been used for 5 years, the boot and software are the same, the hardware is just re-layout.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Oct 2014 11:11:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC860-power-up-problem/m-p/352884#M876</guid>
      <dc:creator>billy_huan</dc:creator>
      <dc:date>2014-10-09T11:11:55Z</dc:date>
    </item>
    <item>
      <title>Re: MPC860 power up problem</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC860-power-up-problem/m-p/352885#M877</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could you please describe in more details, what was the exact root cause of the clkout problem?&lt;/P&gt;&lt;P&gt;If this root cause is somehow related to re-layout, than I'm quite sure the UART issue is also related to re-layout.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Oct 2014 12:15:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC860-power-up-problem/m-p/352885#M877</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2014-10-20T12:15:07Z</dc:date>
    </item>
  </channel>
</rss>