<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC ProcessorsのトピックRe: getting error while adding 'gpsd'</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/getting-error-while-adding-gpsd/m-p/349541#M833</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Rama Krishna Katta,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This problem is caused by chrpath native package problem, updating chrpath to 0.16 from 0.14 could solve this problem, please refer to the following.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I attached chrpath 0.16 package recipes for you.&lt;/P&gt;&lt;P&gt;1. Please execute the command "bitbake chrpath-native -c clean".&lt;/P&gt;&lt;P&gt;2. Remove the original recipe folder "meta/recipes-devtools/chrpath".&lt;/P&gt;&lt;P&gt;3. Use the attached recipes folder to replace the original one.&lt;/P&gt;&lt;P&gt;4. continue to build gpsd "bitbake gpsd", and the new chrpath native command will be used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have verified it on my host environment, if you have any problem, please feel free to let me know.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Sep 2014 06:41:12 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2014-09-10T06:41:12Z</dc:date>
    <item>
      <title>getting error while adding 'gpsd'</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/getting-error-while-adding-gpsd/m-p/349540#M832</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; chrpath -d "/home/asr907/SDK/QorIQ-SDK-T1040-BSP0.2-20140310-yocto/build_t1040rdb_release/tmp/work/ppce5500-fsl-linux/gpsd/3.7-r6/image/usr/sbin/gpsd"&lt;/P&gt;&lt;P&gt;| section size was read as 2097152, not 32!&lt;/P&gt;&lt;P&gt;| elf_open: Success&lt;/P&gt;&lt;P&gt;| scons: *** [/home/asr907/SDK/QorIQ-SDK-T1040-BSP0.2-20140310-yocto/build_t1040rdb_release/tmp/work/ppce5500-fsl-linux/gpsd/3.7-r6/image/usr/sbin/gpsd] Error 1&lt;/P&gt;&lt;P&gt;| scons: building terminated because of errors.&lt;/P&gt;&lt;P&gt;| ERROR: scons install execution failed.&lt;/P&gt;&lt;P&gt;| ERROR: Function failed: do_install (see /home/asr907/SDK/QorIQ-SDK-T1040-BSP0.2-20140310-yocto/build_t1040rdb_release/tmp/work/ppce5500-fsl-linux/gpsd/3.7-r6/temp/log.do_install.8035 for further information)&lt;/P&gt;&lt;P&gt;ERROR: Task 834 (/home/asr907/SDK/QorIQ-SDK-T1040-BSP0.2-20140310-yocto/meta-oe/meta-oe/recipes-navigation/gpsd/gpsd_3.7.bb, do_install) failed with exit code '1'&lt;/P&gt;&lt;P&gt;NOTE: Tasks Summary: Attempted 2329 tasks of which 2321 didn't need to be rerun and 1 failed.&lt;/P&gt;&lt;P&gt;Waiting for 0 running tasks to finish:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Sep 2014 07:47:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/getting-error-while-adding-gpsd/m-p/349540#M832</guid>
      <dc:creator>ramakrishnakatt</dc:creator>
      <dc:date>2014-09-09T07:47:36Z</dc:date>
    </item>
    <item>
      <title>Re: getting error while adding 'gpsd'</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/getting-error-while-adding-gpsd/m-p/349541#M833</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Rama Krishna Katta,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This problem is caused by chrpath native package problem, updating chrpath to 0.16 from 0.14 could solve this problem, please refer to the following.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I attached chrpath 0.16 package recipes for you.&lt;/P&gt;&lt;P&gt;1. Please execute the command "bitbake chrpath-native -c clean".&lt;/P&gt;&lt;P&gt;2. Remove the original recipe folder "meta/recipes-devtools/chrpath".&lt;/P&gt;&lt;P&gt;3. Use the attached recipes folder to replace the original one.&lt;/P&gt;&lt;P&gt;4. continue to build gpsd "bitbake gpsd", and the new chrpath native command will be used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have verified it on my host environment, if you have any problem, please feel free to let me know.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Sep 2014 06:41:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/getting-error-while-adding-gpsd/m-p/349541#M833</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2014-09-10T06:41:12Z</dc:date>
    </item>
  </channel>
</rss>