<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic getting error while adding  gpsd in  fsl-image-core.bb in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/getting-error-while-adding-gpsd-in-fsl-image-core-bb/m-p/349403#M830</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to add "gpsd" in the fsl-image-core.bb file, but while building with bitbake i am getting fallowing error&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERROR: QA Issue: non debug package contains .debug directory: kernel-dev path /work/t1042rdb-fsl-linux/linux-qoriq-sdk/3.8-r11.1/packages-split/kernel-dev/usr/src/kernel/.debug/mtdapp&lt;/P&gt;&lt;P&gt;ERROR: QA Issue: non debug package contains .debug directory: kernel-dev path /work/t1042rdb-fsl-linux/linux-qoriq-sdk/3.8-r11.1/packages-split/kernel-dev/usr/src/kernel/.debug/a.out&lt;/P&gt;&lt;P&gt;ERROR: QA run found fatal errors. Please consider fixing them.&lt;/P&gt;&lt;P&gt;ERROR: Function failed: do_package_qa&lt;/P&gt;&lt;P&gt;ERROR: Logfile of failure stored in: /home/asr907/SDK/QorIQ-SDK-T1040-BSP0.2-20140310-yocto/build_t1042rdb_release/tmp/work/t1042rdb-fsl-linux/linux-qoriq-sdk/3.8-r11.1/temp/log.do_package.2825&lt;/P&gt;&lt;P&gt;ERROR: Task 697 (/home/asr907/SDK/QorIQ-SDK-T1040-BSP0.2-20140310-yocto/meta-fsl-ppc/recipes-kernel/linux/linux-qoriq-sdk.bb, do_package) failed with exit code '1'&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Sep 2014 07:40:09 GMT</pubDate>
    <dc:creator>ramakrishnakatt</dc:creator>
    <dc:date>2014-09-09T07:40:09Z</dc:date>
    <item>
      <title>getting error while adding  gpsd in  fsl-image-core.bb</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/getting-error-while-adding-gpsd-in-fsl-image-core-bb/m-p/349403#M830</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to add "gpsd" in the fsl-image-core.bb file, but while building with bitbake i am getting fallowing error&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERROR: QA Issue: non debug package contains .debug directory: kernel-dev path /work/t1042rdb-fsl-linux/linux-qoriq-sdk/3.8-r11.1/packages-split/kernel-dev/usr/src/kernel/.debug/mtdapp&lt;/P&gt;&lt;P&gt;ERROR: QA Issue: non debug package contains .debug directory: kernel-dev path /work/t1042rdb-fsl-linux/linux-qoriq-sdk/3.8-r11.1/packages-split/kernel-dev/usr/src/kernel/.debug/a.out&lt;/P&gt;&lt;P&gt;ERROR: QA run found fatal errors. Please consider fixing them.&lt;/P&gt;&lt;P&gt;ERROR: Function failed: do_package_qa&lt;/P&gt;&lt;P&gt;ERROR: Logfile of failure stored in: /home/asr907/SDK/QorIQ-SDK-T1040-BSP0.2-20140310-yocto/build_t1042rdb_release/tmp/work/t1042rdb-fsl-linux/linux-qoriq-sdk/3.8-r11.1/temp/log.do_package.2825&lt;/P&gt;&lt;P&gt;ERROR: Task 697 (/home/asr907/SDK/QorIQ-SDK-T1040-BSP0.2-20140310-yocto/meta-fsl-ppc/recipes-kernel/linux/linux-qoriq-sdk.bb, do_package) failed with exit code '1'&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Sep 2014 07:40:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/getting-error-while-adding-gpsd-in-fsl-image-core-bb/m-p/349403#M830</guid>
      <dc:creator>ramakrishnakatt</dc:creator>
      <dc:date>2014-09-09T07:40:09Z</dc:date>
    </item>
    <item>
      <title>Re: getting error while adding  gpsd in  fsl-image-core.bb</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/getting-error-while-adding-gpsd-in-fsl-image-core-bb/m-p/349404#M831</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;SPAN class="replyToName"&gt;Rama Krishna Katta,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After updated native chrpath, and added "gpsd" in variable IMAGE_INSTALL of recipe meta-fsl-networking/images/fsl-image-core.bb, the rebuilt rootfs image with "bitbake fsl-image-core", I didn't find any problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that your above error is about Linux Kernel do package task.&lt;/P&gt;&lt;P&gt;Have you modified something about Linux Kernel?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Sep 2014 07:07:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/getting-error-while-adding-gpsd-in-fsl-image-core-bb/m-p/349404#M831</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2014-09-10T07:07:28Z</dc:date>
    </item>
  </channel>
</rss>