<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC8309 boot from SPI Flash in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8309-boot-from-SPI-Flash/m-p/149053#M53</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i am facing the same problem. My MPC8309 TWR board not booting .&lt;SPAN style="font-family: Arial,sans-serif; font-size: small;"&gt;i am using MPC TWR board. i am trying to boot the TWr board from SPI. i have interfaced an spi device to the connector and routed the spi signals.&amp;nbsp; ihave routed SPI _boot sel to CS of slave device.&lt;BR /&gt; i have done the following modification in the MPC8309 TWR board&lt;BR /&gt; &lt;BR /&gt; 1)&amp;nbsp; i have modified the reset conf words to '1111' to boot from SPI.&lt;BR /&gt; 2)&amp;nbsp; SPI signals&lt;BR /&gt; 3) SYS_CLK is 33MHz&lt;BR /&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i have followed AN3659 to create an SPI image and loaded in the SPI device through a third party tool.&lt;/P&gt;&lt;DIV class=""&gt; &lt;/DIV&gt;&lt;DIV class=""&gt;i have also read the flash locations. i read same values. is there anything to be changed in uboot? i am using the default uboot provided with twr board.&lt;/DIV&gt;&lt;DIV class=""&gt; &lt;/DIV&gt;&lt;DIV class=""&gt;I have monitored the DDR clock on the MPC8309 TWR board. i could see 131MHZ clock on those pins.&lt;BR /&gt; means that i am able to read the data from serial flash. if i modify the BOOT signature my DDR clock is not generated.&lt;BR /&gt; this is how i confirmed that SPI boot is ok. my u-boot is present @0x400 location in the serial flash. but still my system is not booting.&amp;nbsp; i could not use a debugger as JTAG is not working in my TWR board. following is my .dat file&lt;/DIV&gt;&lt;DIV class=""&gt; &lt;/DIV&gt;&lt;DIV class=""&gt;40:424f4f54&lt;BR /&gt;44:00000000&lt;BR /&gt;48:00077EE0&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;4c:00000000&lt;BR /&gt;50:00000400&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;54:00000000&lt;BR /&gt;58:01000000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;5c:00000000&lt;BR /&gt;60:01000100&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;64:00000000&lt;BR /&gt;68:00000013&lt;P&gt;&lt;/P&gt;&lt;BR /&gt;80:fff0211C&lt;BR /&gt;84:8000C000&lt;/DIV&gt;&lt;DIV class=""&gt; &lt;/DIV&gt;&lt;DIV class=""&gt;88:fff02000 &amp;nbsp;&lt;BR /&gt;8c:00000007 &amp;nbsp;&lt;P&gt;&lt;/P&gt;90:fff02080 &amp;nbsp;&lt;BR /&gt;94:80840102&lt;P&gt;&lt;/P&gt;98:fff02100 &amp;nbsp;&lt;BR /&gt;9c:00000000&lt;P&gt;&lt;/P&gt;a0:fff02104 &amp;nbsp;&lt;BR /&gt;a4:00220802&lt;P&gt;&lt;/P&gt;a8:fff02108 &amp;nbsp;&lt;BR /&gt;ac:26256222&lt;P&gt;&lt;/P&gt;b0:fff0210c &amp;nbsp;&lt;BR /&gt;b4:0f9028c7&lt;P&gt;&lt;/P&gt;b8:fff02114 &amp;nbsp;&lt;BR /&gt;bc:00401000&lt;P&gt;&lt;/P&gt;c0:fff02118 &amp;nbsp;&lt;BR /&gt;c4:44400232&lt;P&gt;&lt;/P&gt;c8:fff02124 &amp;nbsp;&lt;BR /&gt;cc:03200064&lt;P&gt;&lt;/P&gt;d0:fff02130 &amp;nbsp;&lt;BR /&gt;d4:02000000&lt;P&gt;&lt;/P&gt;d8:40000001 &amp;nbsp;&lt;BR /&gt;dc:00000100&lt;P&gt;&lt;/P&gt;e0:fff02128 &amp;nbsp;&lt;BR /&gt;e4:73000002&lt;P&gt;&lt;/P&gt;e8:fff02110 &amp;nbsp;&lt;BR /&gt;ec:C3080008&lt;P&gt;&lt;/P&gt;f0:fff000A0 &amp;nbsp;&lt;BR /&gt;f4:00000000&lt;P&gt;&lt;/P&gt;f8:fff000A4 &amp;nbsp;&lt;BR /&gt;fc:8000001b&lt;P&gt;&lt;/P&gt;100:20000001&lt;BR /&gt;104:21172210&lt;P&gt;&lt;/P&gt;108:40000001 &amp;nbsp;&lt;BR /&gt;10C:00000300&lt;P&gt;&lt;/P&gt;110:efefefef&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Feb 2018 04:53:21 GMT</pubDate>
    <dc:creator>usingbothmuxand</dc:creator>
    <dc:date>2018-02-22T04:53:21Z</dc:date>
    <item>
      <title>MPC8309 boot from SPI Flash</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8309-boot-from-SPI-Flash/m-p/149046#M46</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi:&lt;BR /&gt;There is a problem we met when the MPC8309 on our dev board trying to boot from a SPI Flash. We configure the MPC8309 to read reset configuration word from I2C EEPROM. The configuration word is: RCWLR=0x4405_0008 RCWHR=0xA430_0000. So MPC8309 is to boot from SPI Flash as described in the datasheet. The SPI CLK activates to read data. It goes well in reading all the data specific in Table5-5 until we try to configure the internal registers by using "Config Address/Data" pairs. That is, when we try to give a value to 0xFF40_nnnn, the SPI controller stop to read and the CPU is hanged!&lt;/P&gt;&lt;P&gt;If we don't configure any internal register and just end configuration with EC instruction(Described in Table5-7), The SPI start to read "User's Code". But after several bytes the process is down, too. In this case, we think the cause is that no local access window is enabled for DDR SDRAM controller. So, it seems that 0xFF40_nnnn is not a legal address, but the default value of IMMRBAR is indicated to be 0xFF40_0000 in the datasheet.&lt;BR /&gt;Any suggestion? Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jul 2011 09:51:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8309-boot-from-SPI-Flash/m-p/149046#M46</guid>
      <dc:creator>Huzhu1984</dc:creator>
      <dc:date>2011-07-13T09:51:02Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8309 boot from SPI Flash</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8309-boot-from-SPI-Flash/m-p/149047#M47</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Make sure the least significant bit (bit 31) of the configuration word address is CLEAR to signify addresses.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt; local access window is enabled for DDR SDRAM controller.﻿&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you initialise the DDR controller using this mechanism? I thought you'd need to do that from code loaded into SRAM.&lt;/P&gt;&lt;P&gt;It might be easier to load code into SRAM that configures the peripherals and DDR and then have it load the main code. Except this CPU doesn't have internal SRAM, does it?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does Freescale provide any working examples with the development board or elsewhere?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could this be relevant?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt; 4.3.3.2.3 EEPROM Data Format in Reset Configuration Mode﻿&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt; ﻿IMMRBAR value is prepended to the EEPROM address to generate the complete&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt; ﻿memory-mapped register’s address.&lt;BR /&gt;﻿&lt;/P&gt;&lt;P&gt;You shouldn't attach huge Reference Manuals or Data Sheets to your posts. That's a waste of space. We know where to get these from anyway. Just post LINKS to the documents on Freescale's web site instead.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jul 2011 15:05:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8309-boot-from-SPI-Flash/m-p/149047#M47</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2011-07-13T15:05:34Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8309 boot from SPI Flash</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8309-boot-from-SPI-Flash/m-p/149048#M48</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Tom:&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm sure I have cleared bit31 of configuration word address and&amp;nbsp;there is no&amp;nbsp;SRAM internal or external.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Freescale does provide an example on&amp;nbsp;some chips with similar implementation of boot. See &lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN3659.pdf" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN3659.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;I have checked the datasheet many time, I just don't understand why MPC8309 does not accept any of the Config Address/Data pair&amp;nbsp;burned in the SPI Flash.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;About the attachment, I am a rookie here and I will never do that again :smileyhappy:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jul 2011 15:47:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8309-boot-from-SPI-Flash/m-p/149048#M48</guid>
      <dc:creator>Huzhu1984</dc:creator>
      <dc:date>2011-07-13T15:47:54Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8309 boot from SPI Flash</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8309-boot-from-SPI-Flash/m-p/149049#M49</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm not sure if you managed to get your board working in the meantime, but here is a piece of data that isn't easily available:&lt;/P&gt;&lt;P&gt;For SD or SPI boot, IMMRBAR is modified from the reset default of 0xff400000 to 0xfff00000 by the 8309 ROM boot loader.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So you should appropriately change the addresses you are trying to write to, taking the new base address into account.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Mar 2012 20:25:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8309-boot-from-SPI-Flash/m-p/149049#M49</guid>
      <dc:creator>AlexP</dc:creator>
      <dc:date>2012-03-26T20:25:51Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8309 boot from SPI Flash</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8309-boot-from-SPI-Flash/m-p/149050#M50</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I want to boot from TF card, and the BOOT_CFG[0:3] is configured to 1101, I can watch the SD_CLK wave at the TF connector pin, but it seems to halted, didn't go further. In AN3659 and MPC8309RM, the configuration file need to define some addresses, I'm not very sure about how to set the address, and how to modify in U-Boot. Alexandru Popa said the IMMAR is modified to 0xfff00000 by 8309 ROM bootloader, I tried to modify in configursation data, but still no use.&lt;/P&gt;&lt;P&gt;My question is 8309 how to define the Target address and Execution address, and what is the difference between Execution address and RESET_VECTOR_ADDRESS?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 May 2013 08:38:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8309-boot-from-SPI-Flash/m-p/149050#M50</guid>
      <dc:creator>ruizhengxin</dc:creator>
      <dc:date>2013-05-09T08:38:15Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8309 boot from SPI Flash</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8309-boot-from-SPI-Flash/m-p/149051#M51</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm having excatly this same issue, booting from SPI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When i have only one config word, END OF CONFIG 0x8000_0001 it reads that and starts to copy data from SPI flash to somewhere,&lt;/P&gt;&lt;P&gt;but what ever other config word i have, the process is halted.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;(also the number of config words value seems to have no meaning)&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried to write to 0xff40_2000 (DDR controller) - halts&lt;/P&gt;&lt;P&gt;I have tried to write to 0xff40_0c00 (GPIO) - halts&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="text-decoration: line-through;"&gt;Did anyone found a solution for this?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="text-decoration: line-through;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Actually the IMMRBAR&amp;nbsp; 0xFFF0_0000 works for me. Writing to 0xFFF0_0c00 (GPIO) works,. i can toggle GPIO with config word.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using MPC8306 here btw.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 May 2014 12:09:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8309-boot-from-SPI-Flash/m-p/149051#M51</guid>
      <dc:creator>kimmoli</dc:creator>
      <dc:date>2014-05-16T12:09:44Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8309 boot from SPI Flash</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8309-boot-from-SPI-Flash/m-p/149052#M52</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello. Have you been able to boot u-boot from SPI Flash?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jun 2015 08:47:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8309-boot-from-SPI-Flash/m-p/149052#M52</guid>
      <dc:creator>evgeniytabakov</dc:creator>
      <dc:date>2015-06-03T08:47:59Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8309 boot from SPI Flash</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8309-boot-from-SPI-Flash/m-p/149053#M53</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;i am facing the same problem. My MPC8309 TWR board not booting .&lt;SPAN style="font-family: Arial,sans-serif; font-size: small;"&gt;i am using MPC TWR board. i am trying to boot the TWr board from SPI. i have interfaced an spi device to the connector and routed the spi signals.&amp;nbsp; ihave routed SPI _boot sel to CS of slave device.&lt;BR /&gt; i have done the following modification in the MPC8309 TWR board&lt;BR /&gt; &lt;BR /&gt; 1)&amp;nbsp; i have modified the reset conf words to '1111' to boot from SPI.&lt;BR /&gt; 2)&amp;nbsp; SPI signals&lt;BR /&gt; 3) SYS_CLK is 33MHz&lt;BR /&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i have followed AN3659 to create an SPI image and loaded in the SPI device through a third party tool.&lt;/P&gt;&lt;DIV class=""&gt; &lt;/DIV&gt;&lt;DIV class=""&gt;i have also read the flash locations. i read same values. is there anything to be changed in uboot? i am using the default uboot provided with twr board.&lt;/DIV&gt;&lt;DIV class=""&gt; &lt;/DIV&gt;&lt;DIV class=""&gt;I have monitored the DDR clock on the MPC8309 TWR board. i could see 131MHZ clock on those pins.&lt;BR /&gt; means that i am able to read the data from serial flash. if i modify the BOOT signature my DDR clock is not generated.&lt;BR /&gt; this is how i confirmed that SPI boot is ok. my u-boot is present @0x400 location in the serial flash. but still my system is not booting.&amp;nbsp; i could not use a debugger as JTAG is not working in my TWR board. following is my .dat file&lt;/DIV&gt;&lt;DIV class=""&gt; &lt;/DIV&gt;&lt;DIV class=""&gt;40:424f4f54&lt;BR /&gt;44:00000000&lt;BR /&gt;48:00077EE0&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;4c:00000000&lt;BR /&gt;50:00000400&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;54:00000000&lt;BR /&gt;58:01000000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;5c:00000000&lt;BR /&gt;60:01000100&amp;nbsp;&amp;nbsp; &amp;nbsp;&lt;BR /&gt;64:00000000&lt;BR /&gt;68:00000013&lt;P&gt;&lt;/P&gt;&lt;BR /&gt;80:fff0211C&lt;BR /&gt;84:8000C000&lt;/DIV&gt;&lt;DIV class=""&gt; &lt;/DIV&gt;&lt;DIV class=""&gt;88:fff02000 &amp;nbsp;&lt;BR /&gt;8c:00000007 &amp;nbsp;&lt;P&gt;&lt;/P&gt;90:fff02080 &amp;nbsp;&lt;BR /&gt;94:80840102&lt;P&gt;&lt;/P&gt;98:fff02100 &amp;nbsp;&lt;BR /&gt;9c:00000000&lt;P&gt;&lt;/P&gt;a0:fff02104 &amp;nbsp;&lt;BR /&gt;a4:00220802&lt;P&gt;&lt;/P&gt;a8:fff02108 &amp;nbsp;&lt;BR /&gt;ac:26256222&lt;P&gt;&lt;/P&gt;b0:fff0210c &amp;nbsp;&lt;BR /&gt;b4:0f9028c7&lt;P&gt;&lt;/P&gt;b8:fff02114 &amp;nbsp;&lt;BR /&gt;bc:00401000&lt;P&gt;&lt;/P&gt;c0:fff02118 &amp;nbsp;&lt;BR /&gt;c4:44400232&lt;P&gt;&lt;/P&gt;c8:fff02124 &amp;nbsp;&lt;BR /&gt;cc:03200064&lt;P&gt;&lt;/P&gt;d0:fff02130 &amp;nbsp;&lt;BR /&gt;d4:02000000&lt;P&gt;&lt;/P&gt;d8:40000001 &amp;nbsp;&lt;BR /&gt;dc:00000100&lt;P&gt;&lt;/P&gt;e0:fff02128 &amp;nbsp;&lt;BR /&gt;e4:73000002&lt;P&gt;&lt;/P&gt;e8:fff02110 &amp;nbsp;&lt;BR /&gt;ec:C3080008&lt;P&gt;&lt;/P&gt;f0:fff000A0 &amp;nbsp;&lt;BR /&gt;f4:00000000&lt;P&gt;&lt;/P&gt;f8:fff000A4 &amp;nbsp;&lt;BR /&gt;fc:8000001b&lt;P&gt;&lt;/P&gt;100:20000001&lt;BR /&gt;104:21172210&lt;P&gt;&lt;/P&gt;108:40000001 &amp;nbsp;&lt;BR /&gt;10C:00000300&lt;P&gt;&lt;/P&gt;110:efefefef&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Feb 2018 04:53:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8309-boot-from-SPI-Flash/m-p/149053#M53</guid>
      <dc:creator>usingbothmuxand</dc:creator>
      <dc:date>2018-02-22T04:53:21Z</dc:date>
    </item>
  </channel>
</rss>