<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC ProcessorsのトピックLS1028A GPIOs Reg</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/LS1028A-GPIOs-Reg/m-p/2020486#M4779</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;1. In LS0128A Reference Manual, Section "The GPIO module as implemented on the chip" was mentioned. Where is this section available?&lt;/P&gt;&lt;P&gt;2. I can see 3 sets of GPIOs GPIO 1 to 3. How are these different? It seems we can not use GPIO1_DAT0 and&amp;nbsp;GPIO2_DAT0 simultaneously. Is this correct?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
    <pubDate>Mon, 30 Dec 2024 10:50:07 GMT</pubDate>
    <dc:creator>mkraj</dc:creator>
    <dc:date>2024-12-30T10:50:07Z</dc:date>
    <item>
      <title>LS1028A GPIOs Reg</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/LS1028A-GPIOs-Reg/m-p/2020486#M4779</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;1. In LS0128A Reference Manual, Section "The GPIO module as implemented on the chip" was mentioned. Where is this section available?&lt;/P&gt;&lt;P&gt;2. I can see 3 sets of GPIOs GPIO 1 to 3. How are these different? It seems we can not use GPIO1_DAT0 and&amp;nbsp;GPIO2_DAT0 simultaneously. Is this correct?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Mon, 30 Dec 2024 10:50:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/LS1028A-GPIOs-Reg/m-p/2020486#M4779</guid>
      <dc:creator>mkraj</dc:creator>
      <dc:date>2024-12-30T10:50:07Z</dc:date>
    </item>
    <item>
      <title>Re: LS1028A GPIOs Reg</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/LS1028A-GPIOs-Reg/m-p/2026531#M4786</link>
      <description>&lt;P&gt;1. This is a mistake in LS1028ARM, there is no this section&amp;nbsp;&lt;SPAN&gt;"The GPIO module as implemented on the chip".&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;2. The base addresses of these 3 sets are different.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;GPIO1 base address: 230_0000h&lt;BR /&gt;GPIO2 base address: 231_0000h&lt;BR /&gt;GPIO3 base address: 232_0000h&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;You can use GPIO1_DAT0 and&amp;nbsp;GPIO2_DAT0 simultaneously.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 13 Jan 2025 08:03:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/LS1028A-GPIOs-Reg/m-p/2026531#M4786</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2025-01-13T08:03:05Z</dc:date>
    </item>
    <item>
      <title>Re: LS1028A GPIOs Reg</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/LS1028A-GPIOs-Reg/m-p/2026715#M4787</link>
      <description>&lt;P&gt;Dear yipingwang&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Mon, 13 Jan 2025 11:44:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/LS1028A-GPIOs-Reg/m-p/2026715#M4787</guid>
      <dc:creator>mkraj</dc:creator>
      <dc:date>2025-01-13T11:44:55Z</dc:date>
    </item>
  </channel>
</rss>