<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC ProcessorsのトピックEthernet not working properly</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/Ethernet-not-working-properly/m-p/1910561#M4680</link>
    <description>&lt;P&gt;i upgraded my device kernel 4.1 to 6.1 which use soc LS1020A. after upgrade device id booting properly and Ethernet poet is coming up but when i try to ping Ethernet server using Ethernet&amp;nbsp; port ping is not going even i am using the same Ethernet port which i use to boot device using tftp boot.&lt;/P&gt;&lt;P&gt;i added my device dts and dtsi file and kernel logs also.&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 17 Jul 2024 11:57:07 GMT</pubDate>
    <dc:creator>jagrati_chaudhary</dc:creator>
    <dc:date>2024-07-17T11:57:07Z</dc:date>
    <item>
      <title>Ethernet not working properly</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Ethernet-not-working-properly/m-p/1910561#M4680</link>
      <description>&lt;P&gt;i upgraded my device kernel 4.1 to 6.1 which use soc LS1020A. after upgrade device id booting properly and Ethernet poet is coming up but when i try to ping Ethernet server using Ethernet&amp;nbsp; port ping is not going even i am using the same Ethernet port which i use to boot device using tftp boot.&lt;/P&gt;&lt;P&gt;i added my device dts and dtsi file and kernel logs also.&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 17 Jul 2024 11:57:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Ethernet-not-working-properly/m-p/1910561#M4680</guid>
      <dc:creator>jagrati_chaudhary</dc:creator>
      <dc:date>2024-07-17T11:57:07Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet not working properly</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Ethernet-not-working-properly/m-p/1911632#M4684</link>
      <description>&lt;P&gt;Hello.&lt;/P&gt;
&lt;P&gt;You upgraded to 6.1 but in your log file I see the U-boot version as&amp;nbsp;&lt;/P&gt;
&lt;PRE class="bp-text bp-text-plain hljs bp-is-scrollable" tabindex="0"&gt;&lt;CODE class="bp-text-code txt"&gt;U-Boot 2016.09&lt;/CODE&gt;&lt;/PRE&gt;
&lt;P&gt;Please as a first step, upgrade your u-boot&amp;nbsp; version according to the LLDP version.&lt;/P&gt;</description>
      <pubDate>Thu, 18 Jul 2024 21:11:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Ethernet-not-working-properly/m-p/1911632#M4684</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2024-07-18T21:11:01Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet not working properly</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Ethernet-not-working-properly/m-p/1926456#M4707</link>
      <description>&lt;P&gt;Is there any way that i can upgrade my device Kernel without upgrade uboot?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 06 Aug 2024 14:18:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Ethernet-not-working-properly/m-p/1926456#M4707</guid>
      <dc:creator>jagrati_chaudhary</dc:creator>
      <dc:date>2024-08-06T14:18:13Z</dc:date>
    </item>
  </channel>
</rss>