<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC ProcessorsのトピックRe: Heat Spreader Implementation</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/Heat-Spreader-Implementation/m-p/1895786#M4647</link>
    <description>&lt;P&gt;Dear NXP Support Team.&lt;/P&gt;&lt;P&gt;Please help to share the download link for the following application note.&lt;/P&gt;&lt;P&gt;we cannot download AN4871 from the following link.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/external-link.jspa?url=http%3A%2F%2Fcache.nxp.com%2Ffiles%2F32bit%2Fdoc%2Fapp_note%2FAN4871.pdf" target="_blank" rel="nofollow noopener noreferrer"&gt;http://cache.nxp.com/files/32bit/doc/app_note/AN4871.pdf&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 28 Jun 2024 08:36:03 GMT</pubDate>
    <dc:creator>DanielDuJijun</dc:creator>
    <dc:date>2024-06-28T08:36:03Z</dc:date>
    <item>
      <title>Heat Spreader Implementation</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Heat-Spreader-Implementation/m-p/460146#M1304</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The Datasheet for MPC8640D says that "In any implementation of a heat sink solution, the force on the die should not exceed to pounds force".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. If say an additional 10% of force, or a total of 11lbs force, would the die be at a high risk of damage?&lt;/P&gt;&lt;P&gt;2. Is that limit a constant clamping force, or a one lime installation force limit?&lt;/P&gt;&lt;P&gt;3. What would the main failure mode be if excessive force was applied? (fail at High current, immediate failure, failure at temperature. etc.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Apr 2016 16:05:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Heat-Spreader-Implementation/m-p/460146#M1304</guid>
      <dc:creator>matthewware</dc:creator>
      <dc:date>2016-04-19T16:05:53Z</dc:date>
    </item>
    <item>
      <title>Re: Heat Spreader Implementation</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Heat-Spreader-Implementation/m-p/460147#M1305</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-family: Arial;"&gt;MPC8640D package has exposed silicon die (lidless). The main threats are cracking of the die because of package bending or non-parallel alignment of heat sink.&lt;BR /&gt;&lt;BR /&gt;Under no circumstances shall the total load exceed 80 N. Maximum short-term dynamic tensile force should not exceed 15 N (1.5 Kg equivalent). Maximum short-term dynamic compressive force shall not exceed 70 N (7.1 Kg equivalent).&lt;BR /&gt;Long-term static tensile forces are not allowed. Maximum long-term static compressive force on the package shall not exceed 45 N. &lt;BR /&gt;&lt;BR /&gt;Reference document:&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.freescale.com/external-link.jspa?url=http%3A%2F%2Fcache.nxp.com%2Ffiles%2F32bit%2Fdoc%2Fapp_note%2FAN4871.pdf" rel="nofollow" target="_blank"&gt;http://cache.nxp.com/files/32bit/doc/app_note/AN4871.pdf&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Note. Aplication note allows more force to be applied for this package. We provide conservative requirments in datasheet.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Apr 2016 07:20:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Heat-Spreader-Implementation/m-p/460147#M1305</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2016-04-26T07:20:57Z</dc:date>
    </item>
    <item>
      <title>Re: Heat Spreader Implementation</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Heat-Spreader-Implementation/m-p/1895786#M4647</link>
      <description>&lt;P&gt;Dear NXP Support Team.&lt;/P&gt;&lt;P&gt;Please help to share the download link for the following application note.&lt;/P&gt;&lt;P&gt;we cannot download AN4871 from the following link.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/external-link.jspa?url=http%3A%2F%2Fcache.nxp.com%2Ffiles%2F32bit%2Fdoc%2Fapp_note%2FAN4871.pdf" target="_blank" rel="nofollow noopener noreferrer"&gt;http://cache.nxp.com/files/32bit/doc/app_note/AN4871.pdf&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 28 Jun 2024 08:36:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Heat-Spreader-Implementation/m-p/1895786#M4647</guid>
      <dc:creator>DanielDuJijun</dc:creator>
      <dc:date>2024-06-28T08:36:03Z</dc:date>
    </item>
  </channel>
</rss>