<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: I need write MPC8306 interrupt function by c language in Uboot. But  I cann't find a handbook to describe it. in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/I-need-write-MPC8306-interrupt-function-by-c-language-in-Uboot/m-p/262150#M452</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In u-boot, code or variable addresses cannot be decided when compiling, GOT is used to solve this problem.&lt;/P&gt;&lt;P&gt;STARG_GOT is used to define the start of the table, END_GOT is used to define the end of the table, &lt;/P&gt;&lt;P&gt;GOT_ENTRY is used to write the offset into the table and "GOT" is used for reading the offset from the table.&lt;/P&gt;&lt;P&gt;Please refer to cpu/mpc83xx/u-boot.lds for _FIXUP_TABLE_ defination.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Jan 2014 06:05:19 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2014-01-02T06:05:19Z</dc:date>
    <item>
      <title>I need write MPC8306 interrupt function by c language in Uboot. But  I cann't find a handbook to describe it.</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/I-need-write-MPC8306-interrupt-function-by-c-language-in-Uboot/m-p/262148#M450</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My processor is Mpc8306. And my code must run in Uboot., not in linux. But I can not find any handbook to describe wirte interrupt function. I download gcc manual. The manual does not say about gramma about ppc interrupt. For example, gcc book describe the ARM interrupt:&amp;nbsp; "void f () __attribute__ ((interrupt ("IRQ")));" , it is a interrupt handle function to tell gcc compile.&amp;nbsp; Also, I don't know how to write assemble like start.s in uboot,&amp;nbsp; The start's file has something like "GOT_ENTRY(_FIXUP_TABLE_)",&amp;nbsp; I don't know what it mean.&lt;/P&gt;&lt;P&gt;Please help me?&lt;/P&gt;&lt;P&gt;.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 14 Dec 2013 09:15:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/I-need-write-MPC8306-interrupt-function-by-c-language-in-Uboot/m-p/262148#M450</guid>
      <dc:creator>leimao</dc:creator>
      <dc:date>2013-12-14T09:15:40Z</dc:date>
    </item>
    <item>
      <title>Re: I need write MPC8306 interrupt function by c language in Uboot. But  I cann't find a handbook to describe it.</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/I-need-write-MPC8306-interrupt-function-by-c-language-in-Uboot/m-p/262149#M451</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please refer to the section "Vector Table" in cpu/mpc83xx/start.S and the file cpu/mpc83xx/interrupts.c and cpu/mpc83xx/traps.c.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jan 2014 05:56:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/I-need-write-MPC8306-interrupt-function-by-c-language-in-Uboot/m-p/262149#M451</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2014-01-02T05:56:42Z</dc:date>
    </item>
    <item>
      <title>Re: I need write MPC8306 interrupt function by c language in Uboot. But  I cann't find a handbook to describe it.</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/I-need-write-MPC8306-interrupt-function-by-c-language-in-Uboot/m-p/262150#M452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In u-boot, code or variable addresses cannot be decided when compiling, GOT is used to solve this problem.&lt;/P&gt;&lt;P&gt;STARG_GOT is used to define the start of the table, END_GOT is used to define the end of the table, &lt;/P&gt;&lt;P&gt;GOT_ENTRY is used to write the offset into the table and "GOT" is used for reading the offset from the table.&lt;/P&gt;&lt;P&gt;Please refer to cpu/mpc83xx/u-boot.lds for _FIXUP_TABLE_ defination.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jan 2014 06:05:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/I-need-write-MPC8306-interrupt-function-by-c-language-in-Uboot/m-p/262150#M452</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2014-01-02T06:05:19Z</dc:date>
    </item>
  </channel>
</rss>