<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC ProcessorsのトピックRe: PRBS on MAC layer</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/PRBS-on-MAC-layer/m-p/1620467#M4380</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;1. Is there support for remote MAC loopback for dTSEC ?&lt;/P&gt;&lt;P&gt;2. In the DPAARM , it is mentioned that "&lt;EM&gt;Carrier extend symbols in full duplex mode are not supported&lt;/EM&gt;", does it mean that Carrier extend symbol is supported in half duplex mode?&lt;/P&gt;&lt;P&gt;3. No register could be found in RM as well as DPAARM for carrier extension. Do let us know the register configuration to enable/disable the carrier extend symbol.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ram&lt;/P&gt;</description>
    <pubDate>Thu, 23 Mar 2023 04:51:02 GMT</pubDate>
    <dc:creator>rammurmu</dc:creator>
    <dc:date>2023-03-23T04:51:02Z</dc:date>
    <item>
      <title>PRBS on MAC layer</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/PRBS-on-MAC-layer/m-p/1600932#M4353</link>
      <description>&lt;P&gt;I am having P5040ds processor and having a marvel switch on my board through MAC-MAC&amp;nbsp; SGMII connection. We are having some issue in communication between processor and switch.&lt;/P&gt;&lt;P&gt;The processor is configured on 1G fixed link SGMII mode and same setting is done on switch.&lt;/P&gt;&lt;P&gt;To debug the issue, we need to run PRBS on processor fm1-gb0 port, kindly provide related documentation / registers to do the same.&lt;/P&gt;&lt;P&gt;Also Is there any procedure to enable remote loopback on fm1-gb0 MAC?&lt;/P&gt;</description>
      <pubDate>Fri, 17 Feb 2023 07:10:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/PRBS-on-MAC-layer/m-p/1600932#M4353</guid>
      <dc:creator>hemwant</dc:creator>
      <dc:date>2023-02-17T07:10:47Z</dc:date>
    </item>
    <item>
      <title>Re: PRBS on MAC layer</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/PRBS-on-MAC-layer/m-p/1602503#M4354</link>
      <description>&lt;P&gt;&lt;SPAN&gt;P5040 does not have a built in PRBS generation and checking. but customer can use an external loop card/board (connecting the RX to TX) and generate any test sequence (including a test that would be similar/same as pseudorandom binary sequence) and check it in the test SW.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 21 Feb 2023 05:32:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/PRBS-on-MAC-layer/m-p/1602503#M4354</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2023-02-21T05:32:56Z</dc:date>
    </item>
    <item>
      <title>Re: PRBS on MAC layer</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/PRBS-on-MAC-layer/m-p/1620467#M4380</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;1. Is there support for remote MAC loopback for dTSEC ?&lt;/P&gt;&lt;P&gt;2. In the DPAARM , it is mentioned that "&lt;EM&gt;Carrier extend symbols in full duplex mode are not supported&lt;/EM&gt;", does it mean that Carrier extend symbol is supported in half duplex mode?&lt;/P&gt;&lt;P&gt;3. No register could be found in RM as well as DPAARM for carrier extension. Do let us know the register configuration to enable/disable the carrier extend symbol.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ram&lt;/P&gt;</description>
      <pubDate>Thu, 23 Mar 2023 04:51:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/PRBS-on-MAC-layer/m-p/1620467#M4380</guid>
      <dc:creator>rammurmu</dc:creator>
      <dc:date>2023-03-23T04:51:02Z</dc:date>
    </item>
    <item>
      <title>Re: PRBS on MAC layer</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/PRBS-on-MAC-layer/m-p/1624084#M4385</link>
      <description>&lt;P&gt;Any update on this query would be appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 29 Mar 2023 09:34:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/PRBS-on-MAC-layer/m-p/1624084#M4385</guid>
      <dc:creator>rammurmu</dc:creator>
      <dc:date>2023-03-29T09:34:02Z</dc:date>
    </item>
    <item>
      <title>Re: PRBS on MAC layer</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/PRBS-on-MAC-layer/m-p/1624666#M4386</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;SPAN&gt;rammurmu,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Would you please create a new thread to discuss your issues.&lt;/P&gt;
&lt;P&gt;Thanks,&lt;/P&gt;
&lt;P&gt;Yiping&lt;/P&gt;</description>
      <pubDate>Thu, 30 Mar 2023 00:45:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/PRBS-on-MAC-layer/m-p/1624666#M4386</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2023-03-30T00:45:42Z</dc:date>
    </item>
  </channel>
</rss>