<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC Processors中的主题 Re: MPC860 device compatibility</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC860-device-compatibility/m-p/1587379#M4349</link>
    <description>&lt;P&gt;Hello Hector,&lt;BR /&gt;Many thanks for looking into this.&lt;BR /&gt;The TDS3054B uses the&amp;nbsp;&lt;SPAN&gt;XPC860DEZP50D4. The board that this sits on has good power rails and good clock generation. The Power On Reset Circuitry is operating as expected.&lt;BR /&gt;&lt;BR /&gt;However, there is *no* CPU activity what so&amp;nbsp;ever. No Address line/bus activity, no Data bus activity. Nothing that would indicate that the processor was running.&lt;BR /&gt;&lt;BR /&gt;We did attempt to "Reflow" the BGA to see if it was just a solder ball issue. The reflow was a bit of a clumsy attempt and the processor was 'overheated' in the process and emitted a puff of smoke. So we definitely need to replace it.&lt;BR /&gt;&lt;BR /&gt;Best Regards&lt;BR /&gt;Paul.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 24 Jan 2023 23:14:18 GMT</pubDate>
    <dc:creator>pcarew</dc:creator>
    <dc:date>2023-01-24T23:14:18Z</dc:date>
    <item>
      <title>MPC860 device compatibility</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC860-device-compatibility/m-p/1585060#M4343</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We're trying to repair a Tektronix TDS3054B oscilloscope and it appears that the processor is dead.&lt;BR /&gt;This scope uses an NXP processor the XPC860DEZP50D4&lt;/P&gt;&lt;P&gt;It looks like we need to replace the processor on the main board, but these processors are hard to come by now.&lt;BR /&gt;We have found a source for another processor in the line and wanted to ask about their "Drop-In" compatibility.&lt;/P&gt;&lt;P&gt;The other processor is an &lt;SPAN&gt;MPC860ENVR66D4.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;My major question around the differences are:&lt;BR /&gt;a) Is the BGA pinout the same between the 2 devices (it looks like it might be from the orig. HW document)?&lt;BR /&gt;&lt;BR /&gt;b) Would the additional features in the EN version (2 extra 10T ethernet functions and 2 extra Serial Communications Controllers) cause any disruption if not used/initialized?&lt;BR /&gt;The existing firmware obviously would not know or expect these. If they are not initialized/configured, would they disrupt the operation of the processor?&lt;BR /&gt;&lt;BR /&gt;c) The ENC device supports a higher speed. Would this be ok being clocked at the lower DEZ speed?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many thanks.&lt;/P&gt;&lt;P&gt;Paul.&lt;/P&gt;</description>
      <pubDate>Wed, 18 Jan 2023 23:42:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC860-device-compatibility/m-p/1585060#M4343</guid>
      <dc:creator>pcarew</dc:creator>
      <dc:date>2023-01-18T23:42:35Z</dc:date>
    </item>
    <item>
      <title>Re: MPC860 device compatibility</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC860-device-compatibility/m-p/1587319#M4348</link>
      <description>&lt;P&gt;Hello pcarew,&lt;/P&gt;
&lt;P&gt;Hope this email finds you well&lt;/P&gt;
&lt;P&gt;I have been working on your case to find a solution for this situation, I'm currently waiting for an internal team validation.&lt;/P&gt;
&lt;P&gt;Meantime I want to ask you a&amp;nbsp; question:&lt;/P&gt;
&lt;P&gt;How did you know that the processor is dead?&lt;/P&gt;
&lt;P&gt;I will be back with you as soon as I get any update from the internal team,&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Hector Villarruel&lt;/P&gt;</description>
      <pubDate>Tue, 24 Jan 2023 19:33:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC860-device-compatibility/m-p/1587319#M4348</guid>
      <dc:creator>Hector_Villarruel</dc:creator>
      <dc:date>2023-01-24T19:33:02Z</dc:date>
    </item>
    <item>
      <title>Re: MPC860 device compatibility</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC860-device-compatibility/m-p/1587379#M4349</link>
      <description>&lt;P&gt;Hello Hector,&lt;BR /&gt;Many thanks for looking into this.&lt;BR /&gt;The TDS3054B uses the&amp;nbsp;&lt;SPAN&gt;XPC860DEZP50D4. The board that this sits on has good power rails and good clock generation. The Power On Reset Circuitry is operating as expected.&lt;BR /&gt;&lt;BR /&gt;However, there is *no* CPU activity what so&amp;nbsp;ever. No Address line/bus activity, no Data bus activity. Nothing that would indicate that the processor was running.&lt;BR /&gt;&lt;BR /&gt;We did attempt to "Reflow" the BGA to see if it was just a solder ball issue. The reflow was a bit of a clumsy attempt and the processor was 'overheated' in the process and emitted a puff of smoke. So we definitely need to replace it.&lt;BR /&gt;&lt;BR /&gt;Best Regards&lt;BR /&gt;Paul.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 24 Jan 2023 23:14:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC860-device-compatibility/m-p/1587379#M4349</guid>
      <dc:creator>pcarew</dc:creator>
      <dc:date>2023-01-24T23:14:18Z</dc:date>
    </item>
    <item>
      <title>Re: MPC860 device compatibility</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC860-device-compatibility/m-p/1589171#M4351</link>
      <description>&lt;P&gt;Hello pcarew,&lt;/P&gt;
&lt;P&gt;Hope this post finds you well,&lt;/P&gt;
&lt;P&gt;I have verified with the internal team and they inform me of the following statement:&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Yes, MPC860ENVR66D4 can used as a replacement for XPC860DEZP50D4.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Hector Villarruel&lt;/P&gt;</description>
      <pubDate>Sat, 28 Jan 2023 03:31:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC860-device-compatibility/m-p/1589171#M4351</guid>
      <dc:creator>Hector_Villarruel</dc:creator>
      <dc:date>2023-01-28T03:31:17Z</dc:date>
    </item>
  </channel>
</rss>