<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC Processors中的主题 Re: Flash configuration file needed for MPC870 processor</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/Flash-configuration-file-needed-for-MPC870-processor/m-p/1575389#M4336</link>
    <description>&lt;P&gt;Please refer to the application note&amp;nbsp;AN3630.CreatingFlashAlgorithm.pdf and&amp;nbsp;AddFlashDevs.pdf in&amp;nbsp;C:\Program Files (x86)\Freescale\CodeWarrior PA V8.8\PowerPC_EABI_Tools\FlashProgrammer\Documentation to create new flash algorithm and add a new flash device to CodeWarrior.&lt;/P&gt;</description>
    <pubDate>Thu, 29 Dec 2022 03:45:58 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2022-12-29T03:45:58Z</dc:date>
    <item>
      <title>Flash configuration file needed for MPC870 processor</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Flash-configuration-file-needed-for-MPC870-processor/m-p/1573207#M4334</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;we are using MPC870 processor and we have the micron flash MT28EW512ABA1LPC-0SIT connected to it. We are trying to program it from the Codewarrior USB tap over Code warrior v8.8 software, but we don't find our micron flash device listed in the code warrior software. Can anybody help us to get its flash algorithm (.elf file). or if there is any alternate way for this step, please suggest us.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Pradeep.S&lt;/P&gt;</description>
      <pubDate>Thu, 22 Dec 2022 05:33:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Flash-configuration-file-needed-for-MPC870-processor/m-p/1573207#M4334</guid>
      <dc:creator>Pradeepkumar_S</dc:creator>
      <dc:date>2022-12-22T05:33:25Z</dc:date>
    </item>
    <item>
      <title>Re: Flash configuration file needed for MPC870 processor</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Flash-configuration-file-needed-for-MPC870-processor/m-p/1575389#M4336</link>
      <description>&lt;P&gt;Please refer to the application note&amp;nbsp;AN3630.CreatingFlashAlgorithm.pdf and&amp;nbsp;AddFlashDevs.pdf in&amp;nbsp;C:\Program Files (x86)\Freescale\CodeWarrior PA V8.8\PowerPC_EABI_Tools\FlashProgrammer\Documentation to create new flash algorithm and add a new flash device to CodeWarrior.&lt;/P&gt;</description>
      <pubDate>Thu, 29 Dec 2022 03:45:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Flash-configuration-file-needed-for-MPC870-processor/m-p/1575389#M4336</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-12-29T03:45:58Z</dc:date>
    </item>
  </channel>
</rss>