<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC ProcessorsのトピックFlash Programming a MPC8xx with CodeWarrior Classic 8.8.6 and CodeWarrior TAP</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/Flash-Programming-a-MPC8xx-with-CodeWarrior-Classic-8-8-6-and/m-p/1542261#M4309</link>
    <description>&lt;P&gt;I installed CW 8.8 and the Patch 8.8.6 and I substituted the ccs folder for the one of CW Eclipse 11. I have added the "show com" command in the ccs config file: ccs.cfg located in ..\ccs\bin.&lt;/P&gt;&lt;P&gt;OS: Windows 11 64 bits.&lt;/P&gt;&lt;P&gt;I get a "CC communications fault" on the ccs console:&lt;/P&gt;&lt;P&gt;..&lt;/P&gt;&lt;P&gt;Received CMD_AVAILABLE_CONNECTIONS&lt;BR /&gt;command done - Ok&lt;BR /&gt;Received an unknown command 58&lt;BR /&gt;nhti command done - Ok&lt;BR /&gt;Received CMD_GET_CONFIG_CHAIN&lt;BR /&gt;nhti command done - Ok&lt;BR /&gt;Received CMD_CONFIG_CHAIN. count = 1&lt;BR /&gt;core 0: MPC8xx&lt;BR /&gt;nhti command done - CC communications fault&lt;BR /&gt;Received CMD_CONFIG_CHAIN. count = 0&lt;BR /&gt;Received CMD_CC_VERSION&lt;BR /&gt;Available USB TAPs:&lt;BR /&gt;&amp;lt;none&amp;gt;&lt;BR /&gt;VERSION: BL 1.0.1&lt;BR /&gt;VERSION: OS 1.0.4&lt;BR /&gt;CodeWarrior TAP Boot Loader version 1.0.1&lt;BR /&gt;CodeWarrior TAP OS version 1.0.4&lt;BR /&gt;Sending code to CodeWarrior TAP.........done&lt;BR /&gt;runme.sh&lt;BR /&gt;ccs/&lt;BR /&gt;ccs/bin/&lt;BR /&gt;ccs/bin/libtmsc8144.so&lt;BR /&gt;ccs/bin/cwtap_jtag.xsvf.gz&lt;BR /&gt;ccs/bin/libtmsc815x.so&lt;/P&gt;&lt;P&gt;..&lt;/P&gt;&lt;P&gt;When I perform the same test with target power at off, I get a "cable disconnected" error, which is normal.&lt;/P&gt;&lt;P&gt;I suspect my custom made probe tip has not the right pinout. It meant to be a DPI 10 pins BDM interface for 8xx processors (PowerQUICC I). I made the schematics based on the CWH-CTP-COP-YE-SCH from NXP.&lt;/P&gt;&lt;P&gt;Can somebody point me to potential mistakes in my attached diagram (CWH-CTP-DPI-YE.pdf) ?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;</description>
    <pubDate>Sat, 22 Oct 2022 20:25:14 GMT</pubDate>
    <dc:creator>mbedardh</dc:creator>
    <dc:date>2022-10-22T20:25:14Z</dc:date>
    <item>
      <title>Flash Programming a MPC8xx with CodeWarrior Classic 8.8.6 and CodeWarrior TAP</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Flash-Programming-a-MPC8xx-with-CodeWarrior-Classic-8-8-6-and/m-p/1542261#M4309</link>
      <description>&lt;P&gt;I installed CW 8.8 and the Patch 8.8.6 and I substituted the ccs folder for the one of CW Eclipse 11. I have added the "show com" command in the ccs config file: ccs.cfg located in ..\ccs\bin.&lt;/P&gt;&lt;P&gt;OS: Windows 11 64 bits.&lt;/P&gt;&lt;P&gt;I get a "CC communications fault" on the ccs console:&lt;/P&gt;&lt;P&gt;..&lt;/P&gt;&lt;P&gt;Received CMD_AVAILABLE_CONNECTIONS&lt;BR /&gt;command done - Ok&lt;BR /&gt;Received an unknown command 58&lt;BR /&gt;nhti command done - Ok&lt;BR /&gt;Received CMD_GET_CONFIG_CHAIN&lt;BR /&gt;nhti command done - Ok&lt;BR /&gt;Received CMD_CONFIG_CHAIN. count = 1&lt;BR /&gt;core 0: MPC8xx&lt;BR /&gt;nhti command done - CC communications fault&lt;BR /&gt;Received CMD_CONFIG_CHAIN. count = 0&lt;BR /&gt;Received CMD_CC_VERSION&lt;BR /&gt;Available USB TAPs:&lt;BR /&gt;&amp;lt;none&amp;gt;&lt;BR /&gt;VERSION: BL 1.0.1&lt;BR /&gt;VERSION: OS 1.0.4&lt;BR /&gt;CodeWarrior TAP Boot Loader version 1.0.1&lt;BR /&gt;CodeWarrior TAP OS version 1.0.4&lt;BR /&gt;Sending code to CodeWarrior TAP.........done&lt;BR /&gt;runme.sh&lt;BR /&gt;ccs/&lt;BR /&gt;ccs/bin/&lt;BR /&gt;ccs/bin/libtmsc8144.so&lt;BR /&gt;ccs/bin/cwtap_jtag.xsvf.gz&lt;BR /&gt;ccs/bin/libtmsc815x.so&lt;/P&gt;&lt;P&gt;..&lt;/P&gt;&lt;P&gt;When I perform the same test with target power at off, I get a "cable disconnected" error, which is normal.&lt;/P&gt;&lt;P&gt;I suspect my custom made probe tip has not the right pinout. It meant to be a DPI 10 pins BDM interface for 8xx processors (PowerQUICC I). I made the schematics based on the CWH-CTP-COP-YE-SCH from NXP.&lt;/P&gt;&lt;P&gt;Can somebody point me to potential mistakes in my attached diagram (CWH-CTP-DPI-YE.pdf) ?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Michael&lt;/P&gt;</description>
      <pubDate>Sat, 22 Oct 2022 20:25:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Flash-Programming-a-MPC8xx-with-CodeWarrior-Classic-8-8-6-and/m-p/1542261#M4309</guid>
      <dc:creator>mbedardh</dc:creator>
      <dc:date>2022-10-22T20:25:14Z</dc:date>
    </item>
    <item>
      <title>Re: Flash Programming a MPC8xx with CodeWarrior Classic 8.8.6 and CodeWarrior TAP</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Flash-Programming-a-MPC8xx-with-CodeWarrior-Classic-8-8-6-and/m-p/1543331#M4310</link>
      <description>&lt;P&gt;Please refer to section "DPI Connector Information" in the attached document.&lt;/P&gt;
&lt;P&gt;Please open CCS console&amp;nbsp;C:\Program Files (x86)\Freescale\CodeWarrior PA V8.8\ccs\bin\ccs.exe, type command "source IDcode.tcl" to check whether the processor ID information can be read.&lt;/P&gt;</description>
      <pubDate>Tue, 25 Oct 2022 09:34:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Flash-Programming-a-MPC8xx-with-CodeWarrior-Classic-8-8-6-and/m-p/1543331#M4310</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-10-25T09:34:43Z</dc:date>
    </item>
    <item>
      <title>Re: Flash Programming a MPC8xx with CodeWarrior Classic 8.8.6 and CodeWarrior TAP</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Flash-Programming-a-MPC8xx-with-CodeWarrior-Classic-8-8-6-and/m-p/1543518#M4312</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;It is a CodeWarrier TAP (latest model) that I have, so the connector info that I need is for it's 30 pins connector (and not only the 10 pin DPI).&lt;/P&gt;&lt;P&gt;The new TAP works with different cable tips and the particular one for DPI is not available. A schematics would solve the problem.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 25 Oct 2022 17:14:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Flash-Programming-a-MPC8xx-with-CodeWarrior-Classic-8-8-6-and/m-p/1543518#M4312</guid>
      <dc:creator>mbedardh</dc:creator>
      <dc:date>2022-10-25T17:14:34Z</dc:date>
    </item>
    <item>
      <title>Re: Flash Programming a MPC8xx with CodeWarrior Classic 8.8.6 and CodeWarrior TAP</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Flash-Programming-a-MPC8xx-with-CodeWarrior-Classic-8-8-6-and/m-p/1547446#M4314</link>
      <description>&lt;P&gt;Please refer to the following.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://www.nxp.com.cn/docs/en/application-note/AN2387.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/application-note/AN2387.pdf&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Nov 2022 06:23:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Flash-Programming-a-MPC8xx-with-CodeWarrior-Classic-8-8-6-and/m-p/1547446#M4314</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-11-02T06:23:26Z</dc:date>
    </item>
  </channel>
</rss>