<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MPC8308: RGMII (eTSEC1) at 3.3V? or only 2.5V? in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8308-RGMII-eTSEC1-at-3-3V-or-only-2-5V/m-p/259542#M427</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to the MPC8308 Datasheet:&lt;/P&gt;&lt;P&gt;"The RGMII interface is defined for 2.5 V, while the MII interface can be operated at 3.3 V"&lt;/P&gt;&lt;P&gt;If you use eTSEC1 in RGMII mode you should connect LVDD1 (NVDDC) to 2,5V.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Dec 2013 05:35:12 GMT</pubDate>
    <dc:creator>andrei_skok</dc:creator>
    <dc:date>2013-12-13T05:35:12Z</dc:date>
    <item>
      <title>MPC8308: RGMII (eTSEC1) at 3.3V? or only 2.5V?</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8308-RGMII-eTSEC1-at-3-3V-or-only-2-5V/m-p/259541#M426</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We're using the MPC8308. There is a confusion between the datasheet and some schematic about the supply for the eTSEC1 in RGMII mode. Can we connect the eTSEC1 at 3.3V in RGMII mode? or it's only 2.5V? &lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;LV&lt;SUB&gt;DD1&lt;/SUB&gt; = NV&lt;SUB&gt;DDC&lt;/SUB&gt; = TSEC1 = ? in RGMII mode&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;JMAccedian&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Dec 2013 22:38:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8308-RGMII-eTSEC1-at-3-3V-or-only-2-5V/m-p/259541#M426</guid>
      <dc:creator>jmaccedian</dc:creator>
      <dc:date>2013-12-12T22:38:25Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8308: RGMII (eTSEC1) at 3.3V? or only 2.5V?</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8308-RGMII-eTSEC1-at-3-3V-or-only-2-5V/m-p/259542#M427</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to the MPC8308 Datasheet:&lt;/P&gt;&lt;P&gt;"The RGMII interface is defined for 2.5 V, while the MII interface can be operated at 3.3 V"&lt;/P&gt;&lt;P&gt;If you use eTSEC1 in RGMII mode you should connect LVDD1 (NVDDC) to 2,5V.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Dec 2013 05:35:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8308-RGMII-eTSEC1-at-3-3V-or-only-2-5V/m-p/259542#M427</guid>
      <dc:creator>andrei_skok</dc:creator>
      <dc:date>2013-12-13T05:35:12Z</dc:date>
    </item>
  </channel>
</rss>