<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC Processors中的主题 Re: [LS2088ARDB] SCTP protocol checksum offloading</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/LS2088ARDB-SCTP-protocol-checksum-offloading/m-p/1509103#M4226</link>
    <description>&lt;P&gt;&lt;SPAN&gt;According to ethtool command's resutls, tx-checksum-sctp is off[fixed] that can't be changed.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;According to DPAA2RM's section 9.2.3.5 as below, it doesn't explicitly mention that dpaa2 has SCTP checksum offloading feature.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Next we will double check it with R&amp;amp;D team.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;9.2.3.5 Checksum Generation&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Checksums can be generated for primary and tunnel IPv4 as well as TCP or UDP. The associated “don’t&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;calculate checksum” input signal must be set in order to activate this functionality. The parser will require&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;all normal inputs to be present and will generate the valid checksum for the associated header as the frame&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;is parsed. Where required additional information can be found in the related HXS section.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 22 Aug 2022 02:29:38 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2022-08-22T02:29:38Z</dc:date>
    <item>
      <title>[LS2088ARDB] SCTP protocol checksum offloading</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/LS2088ARDB-SCTP-protocol-checksum-offloading/m-p/1502953#M4219</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm trying to use ethernet device tx offloading function in DPDK.&lt;/P&gt;&lt;P&gt;I set the tx offlading feature of rte_eth_conf like this:&lt;/P&gt;&lt;P&gt;.offloads = (DEV_TX_OFFLOAD_IPV4_CKSUM |&lt;BR /&gt;DEV_TX_OFFLOAD_UDP_CKSUM |&lt;BR /&gt;DEV_TX_OFFLOAD_SCTP_CKSUM),&lt;/P&gt;&lt;P&gt;When I send the packet, checksum of IPv4 or UDP is calculated and inserted by offloading function.&lt;/P&gt;&lt;P&gt;But when I send the SCTP packet, the chechsum of SCTP is not touched.&lt;/P&gt;&lt;P&gt;Does SCTP tx checksum offloading is supported in LS2088 or LX2160?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;J.Hwan Kim&lt;/P&gt;</description>
      <pubDate>Tue, 09 Aug 2022 04:08:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/LS2088ARDB-SCTP-protocol-checksum-offloading/m-p/1502953#M4219</guid>
      <dc:creator>jhkim2</dc:creator>
      <dc:date>2022-08-09T04:08:20Z</dc:date>
    </item>
    <item>
      <title>Re: [LS2088ARDB] SCTP protocol checksum offloading</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/LS2088ARDB-SCTP-protocol-checksum-offloading/m-p/1509103#M4226</link>
      <description>&lt;P&gt;&lt;SPAN&gt;According to ethtool command's resutls, tx-checksum-sctp is off[fixed] that can't be changed.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;According to DPAA2RM's section 9.2.3.5 as below, it doesn't explicitly mention that dpaa2 has SCTP checksum offloading feature.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Next we will double check it with R&amp;amp;D team.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;9.2.3.5 Checksum Generation&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Checksums can be generated for primary and tunnel IPv4 as well as TCP or UDP. The associated “don’t&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;calculate checksum” input signal must be set in order to activate this functionality. The parser will require&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;all normal inputs to be present and will generate the valid checksum for the associated header as the frame&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;is parsed. Where required additional information can be found in the related HXS section.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Aug 2022 02:29:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/LS2088ARDB-SCTP-protocol-checksum-offloading/m-p/1509103#M4226</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-08-22T02:29:38Z</dc:date>
    </item>
  </channel>
</rss>