<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC Processors中的主题 T1024:SPI BOOT SPI-CS# access STOP</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/T1024-SPI-BOOT-SPI-CS-access-STOP/m-p/1473933#M4182</link>
    <description>&lt;P&gt;&lt;SPAN&gt;When the T1024 is SPI booted, after the power is turned on, the SPI-CS # pin does not read the SPI to the end. It becomes HIGH level and U-BOOT does not start. For example, if the SPI read data is incorrect, will the SPI-CS # pin become HIGH? thank you.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 15 Jun 2022 00:12:15 GMT</pubDate>
    <dc:creator>kojimiura</dc:creator>
    <dc:date>2022-06-15T00:12:15Z</dc:date>
    <item>
      <title>T1024:SPI BOOT SPI-CS# access STOP</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/T1024-SPI-BOOT-SPI-CS-access-STOP/m-p/1473933#M4182</link>
      <description>&lt;P&gt;&lt;SPAN&gt;When the T1024 is SPI booted, after the power is turned on, the SPI-CS # pin does not read the SPI to the end. It becomes HIGH level and U-BOOT does not start. For example, if the SPI read data is incorrect, will the SPI-CS # pin become HIGH? thank you.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Jun 2022 00:12:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/T1024-SPI-BOOT-SPI-CS-access-STOP/m-p/1473933#M4182</guid>
      <dc:creator>kojimiura</dc:creator>
      <dc:date>2022-06-15T00:12:15Z</dc:date>
    </item>
  </channel>
</rss>