<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC ProcessorsのトピックTWR-MPC8309 local bus</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/TWR-MPC8309-local-bus/m-p/257515#M418</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to determine if I can use the TWR-MPC8309 local bus to connect to a TWR-LCD module and to my custom peripherals. Looking at the schematic, they don't make sense to me:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Data bits 0-7 seem to be reversed. MPC_LBC_D0 is hooked to bus D7, MPC_LBC_D7 is connected to bus D0, etc.&lt;/P&gt;&lt;P&gt;- Address bits are likely strange MPC address bits 25 downto 6 are connected to bus address bits 0 to 19. The address bit numbers don't even match.&lt;/P&gt;&lt;P&gt;- Shouldn't the signals on the backplane be connected to the multiplexed bus (the MPC_LBC_LAD* signals) instead of the demultiplexed signals?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Am I just missing something? I'm not seeing much documentation on the MPC8309 module, so I'm having to make a lot of guesses based on what I'm seeing in the schematics.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 27 May 2013 00:48:13 GMT</pubDate>
    <dc:creator>bbutler</dc:creator>
    <dc:date>2013-05-27T00:48:13Z</dc:date>
    <item>
      <title>TWR-MPC8309 local bus</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/TWR-MPC8309-local-bus/m-p/257515#M418</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to determine if I can use the TWR-MPC8309 local bus to connect to a TWR-LCD module and to my custom peripherals. Looking at the schematic, they don't make sense to me:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Data bits 0-7 seem to be reversed. MPC_LBC_D0 is hooked to bus D7, MPC_LBC_D7 is connected to bus D0, etc.&lt;/P&gt;&lt;P&gt;- Address bits are likely strange MPC address bits 25 downto 6 are connected to bus address bits 0 to 19. The address bit numbers don't even match.&lt;/P&gt;&lt;P&gt;- Shouldn't the signals on the backplane be connected to the multiplexed bus (the MPC_LBC_LAD* signals) instead of the demultiplexed signals?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Am I just missing something? I'm not seeing much documentation on the MPC8309 module, so I'm having to make a lot of guesses based on what I'm seeing in the schematics.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 May 2013 00:48:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/TWR-MPC8309-local-bus/m-p/257515#M418</guid>
      <dc:creator>bbutler</dc:creator>
      <dc:date>2013-05-27T00:48:13Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-MPC8309 local bus</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/TWR-MPC8309-local-bus/m-p/257516#M419</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Why not using MPC830x-TLCD &lt;A href="http://www.freescale.com/zh-Hans/webapp/sps/site/prod_summary.jsp?code=MPC830X_TLCD" title="http://www.freescale.com/zh-Hans/webapp/sps/site/prod_summary.jsp?code=MPC830X_TLCD"&gt;MPC830x-TLCD LCD Display Module for the TWR-MPC830x Module 产品概述&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 May 2013 09:40:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/TWR-MPC8309-local-bus/m-p/257516#M419</guid>
      <dc:creator>lunminliang</dc:creator>
      <dc:date>2013-05-27T09:40:13Z</dc:date>
    </item>
  </channel>
</rss>