<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MPC8306 and MPC8306S interchangeability in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8306-and-MPC8306S-interchangeability/m-p/1450692#M4142</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;If special features of MPC8306 ( eSDHC, 4xCAN, IEEE 1588) are not used can these two processors be used interchangeably as drop-in replacements for each other subject to a common core speed? Note that our design requires the use of all 3x10/100 Mbps ethernet with MII interface. Note that our design has been tested with MPC8306 but want to consider using MPC8306S due to availability issues.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;</description>
    <pubDate>Thu, 28 Apr 2022 12:44:01 GMT</pubDate>
    <dc:creator>Ghayal</dc:creator>
    <dc:date>2022-04-28T12:44:01Z</dc:date>
    <item>
      <title>MPC8306 and MPC8306S interchangeability</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8306-and-MPC8306S-interchangeability/m-p/1450692#M4142</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;If special features of MPC8306 ( eSDHC, 4xCAN, IEEE 1588) are not used can these two processors be used interchangeably as drop-in replacements for each other subject to a common core speed? Note that our design requires the use of all 3x10/100 Mbps ethernet with MII interface. Note that our design has been tested with MPC8306 but want to consider using MPC8306S due to availability issues.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;</description>
      <pubDate>Thu, 28 Apr 2022 12:44:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8306-and-MPC8306S-interchangeability/m-p/1450692#M4142</guid>
      <dc:creator>Ghayal</dc:creator>
      <dc:date>2022-04-28T12:44:01Z</dc:date>
    </item>
  </channel>
</rss>