<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC ProcessorsのトピックPower and IO shorts spontaneously developing on P1021</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/Power-and-IO-shorts-spontaneously-developing-on-P1021/m-p/1440574#M4125</link>
    <description>&lt;P&gt;We have seen several field failures of a product containing the P1021 processor.&amp;nbsp; Apparently spontaneously, while the system is up and running, the system shuts down.&amp;nbsp; Board level analysis shows dead shorts to ground of the 1.0V and 3.3V rails.&amp;nbsp; Upon removal of the processor, dead shorts are found on the Vddc (Core 0 and platform supply), the OVdd (IO subset supply), and on 8 or so IO pins in a tight cluster in the vicinity of the OVdd pins.&lt;/P&gt;&lt;P&gt;This would appear to be the result of some kind of over-voltage stress, but we can not find an obvious cause.&amp;nbsp; Does this seem more likely from an event on the OVdd line or on one of the failing IOs?&amp;nbsp; Note OVdd, BVdd, and CVdd are all tied to the 3.3V rail, and only IO associated with OVdd are found with shorts.&amp;nbsp; No other parts on the board are found to be damaged - many others share the 3.3V rail.&amp;nbsp; No other devices share the 1.0V rail.&lt;/P&gt;&lt;P&gt;Any thoughts on possible causation given these symptoms?&lt;/P&gt;</description>
    <pubDate>Thu, 07 Apr 2022 12:25:34 GMT</pubDate>
    <dc:creator>gregbuchannan</dc:creator>
    <dc:date>2022-04-07T12:25:34Z</dc:date>
    <item>
      <title>Power and IO shorts spontaneously developing on P1021</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Power-and-IO-shorts-spontaneously-developing-on-P1021/m-p/1440574#M4125</link>
      <description>&lt;P&gt;We have seen several field failures of a product containing the P1021 processor.&amp;nbsp; Apparently spontaneously, while the system is up and running, the system shuts down.&amp;nbsp; Board level analysis shows dead shorts to ground of the 1.0V and 3.3V rails.&amp;nbsp; Upon removal of the processor, dead shorts are found on the Vddc (Core 0 and platform supply), the OVdd (IO subset supply), and on 8 or so IO pins in a tight cluster in the vicinity of the OVdd pins.&lt;/P&gt;&lt;P&gt;This would appear to be the result of some kind of over-voltage stress, but we can not find an obvious cause.&amp;nbsp; Does this seem more likely from an event on the OVdd line or on one of the failing IOs?&amp;nbsp; Note OVdd, BVdd, and CVdd are all tied to the 3.3V rail, and only IO associated with OVdd are found with shorts.&amp;nbsp; No other parts on the board are found to be damaged - many others share the 3.3V rail.&amp;nbsp; No other devices share the 1.0V rail.&lt;/P&gt;&lt;P&gt;Any thoughts on possible causation given these symptoms?&lt;/P&gt;</description>
      <pubDate>Thu, 07 Apr 2022 12:25:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Power-and-IO-shorts-spontaneously-developing-on-P1021/m-p/1440574#M4125</guid>
      <dc:creator>gregbuchannan</dc:creator>
      <dc:date>2022-04-07T12:25:34Z</dc:date>
    </item>
  </channel>
</rss>