<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic NAND boot without CPLD in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/NAND-boot-without-CPLD/m-p/1426585#M4101</link>
    <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;We are using T2080RDB board. As per the manual for NAND boot, the SW3[4] should be one for selecting NAND and SW3[4] should be zero for selecting NOR.&lt;/P&gt;&lt;P&gt;Based on the Documents this pin is BOOT_SEL pin wrt to FLASH_SRC register and controlled by CPLD.&lt;/P&gt;&lt;P&gt;We are planning to remove CPLD in our custom board, so can we boot from NAND without using CPLD and sw3[4] which is used for boot media selection either by Hardware or software.&lt;/P&gt;&lt;P&gt;Can you please provide us valuable inputs to this query.&lt;/P&gt;&lt;P&gt;Thanks for your support.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Irfan&lt;/P&gt;</description>
    <pubDate>Fri, 11 Mar 2022 05:36:48 GMT</pubDate>
    <dc:creator>Irfan3</dc:creator>
    <dc:date>2022-03-11T05:36:48Z</dc:date>
    <item>
      <title>NAND boot without CPLD</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/NAND-boot-without-CPLD/m-p/1426585#M4101</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;We are using T2080RDB board. As per the manual for NAND boot, the SW3[4] should be one for selecting NAND and SW3[4] should be zero for selecting NOR.&lt;/P&gt;&lt;P&gt;Based on the Documents this pin is BOOT_SEL pin wrt to FLASH_SRC register and controlled by CPLD.&lt;/P&gt;&lt;P&gt;We are planning to remove CPLD in our custom board, so can we boot from NAND without using CPLD and sw3[4] which is used for boot media selection either by Hardware or software.&lt;/P&gt;&lt;P&gt;Can you please provide us valuable inputs to this query.&lt;/P&gt;&lt;P&gt;Thanks for your support.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Irfan&lt;/P&gt;</description>
      <pubDate>Fri, 11 Mar 2022 05:36:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/NAND-boot-without-CPLD/m-p/1426585#M4101</guid>
      <dc:creator>Irfan3</dc:creator>
      <dc:date>2022-03-11T05:36:48Z</dc:date>
    </item>
  </channel>
</rss>