<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC Processors中的主题 SSD problem on P4080</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/SSD-problem-on-P4080/m-p/1410955#M4080</link>
    <description>&lt;P&gt;I have a P4080DS card, when I plug the SSD to PCIe into the motherboard I cannot access the SSD. I also plugged the USB into the P4080DS but I can't access the USB also there is a power led on my USB but the power led does not flash when plugged in.&lt;/P&gt;</description>
    <pubDate>Wed, 09 Feb 2022 11:27:46 GMT</pubDate>
    <dc:creator>batalay06</dc:creator>
    <dc:date>2022-02-09T11:27:46Z</dc:date>
    <item>
      <title>SSD problem on P4080</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/SSD-problem-on-P4080/m-p/1410955#M4080</link>
      <description>&lt;P&gt;I have a P4080DS card, when I plug the SSD to PCIe into the motherboard I cannot access the SSD. I also plugged the USB into the P4080DS but I can't access the USB also there is a power led on my USB but the power led does not flash when plugged in.&lt;/P&gt;</description>
      <pubDate>Wed, 09 Feb 2022 11:27:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/SSD-problem-on-P4080/m-p/1410955#M4080</guid>
      <dc:creator>batalay06</dc:creator>
      <dc:date>2022-02-09T11:27:46Z</dc:date>
    </item>
  </channel>
</rss>