<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC Processors中的主题 Issue in NAND read operation</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/Issue-in-NAND-read-operation/m-p/1401691#M4061</link>
    <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;we are working on the NAND flash device for Custom T2081 board.&lt;/P&gt;&lt;P&gt;The Nand device which we are using is from Micron MT29F8G08ABDA-IFC.&lt;/P&gt;&lt;P&gt;The issue is as follows:&lt;/P&gt;&lt;P&gt;writing at ROW address= 0x10000000 or 0x00001000 IFC_NAND_EVTER_STAT shows NAND operation complete.&lt;/P&gt;&lt;P&gt;whereas while read operation at 0x10000000&amp;nbsp;IFC_NAND_EVTER_STAT shows NAND operation is not complete.&lt;/P&gt;&lt;P&gt;also while read operation at 0x00001000&amp;nbsp;IFC_NAND_EVTER_STAT shows NAND operation is complete but with Error as "uncorrectable ECC error due to page read operation".&lt;/P&gt;&lt;P&gt;For reference i am attaching the screenshots of the above mentioned issue.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please can you suggest me what could be the issue? Also how can we verify at what memory address of nand device it is getting programmed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; regards,&lt;/P&gt;&lt;P&gt;Irfan&lt;/P&gt;</description>
    <pubDate>Wed, 19 Jan 2022 11:46:04 GMT</pubDate>
    <dc:creator>Irfan3</dc:creator>
    <dc:date>2022-01-19T11:46:04Z</dc:date>
    <item>
      <title>Issue in NAND read operation</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Issue-in-NAND-read-operation/m-p/1401691#M4061</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;we are working on the NAND flash device for Custom T2081 board.&lt;/P&gt;&lt;P&gt;The Nand device which we are using is from Micron MT29F8G08ABDA-IFC.&lt;/P&gt;&lt;P&gt;The issue is as follows:&lt;/P&gt;&lt;P&gt;writing at ROW address= 0x10000000 or 0x00001000 IFC_NAND_EVTER_STAT shows NAND operation complete.&lt;/P&gt;&lt;P&gt;whereas while read operation at 0x10000000&amp;nbsp;IFC_NAND_EVTER_STAT shows NAND operation is not complete.&lt;/P&gt;&lt;P&gt;also while read operation at 0x00001000&amp;nbsp;IFC_NAND_EVTER_STAT shows NAND operation is complete but with Error as "uncorrectable ECC error due to page read operation".&lt;/P&gt;&lt;P&gt;For reference i am attaching the screenshots of the above mentioned issue.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please can you suggest me what could be the issue? Also how can we verify at what memory address of nand device it is getting programmed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; regards,&lt;/P&gt;&lt;P&gt;Irfan&lt;/P&gt;</description>
      <pubDate>Wed, 19 Jan 2022 11:46:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Issue-in-NAND-read-operation/m-p/1401691#M4061</guid>
      <dc:creator>Irfan3</dc:creator>
      <dc:date>2022-01-19T11:46:04Z</dc:date>
    </item>
    <item>
      <title>Re: Issue in NAND read operation</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Issue-in-NAND-read-operation/m-p/1408017#M4076</link>
      <description>&lt;P&gt;Attached file contains NAND Flash driver from SDK 2.0 u-boot. Compare your code and this driver.&lt;/P&gt;</description>
      <pubDate>Wed, 02 Feb 2022 12:52:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Issue-in-NAND-read-operation/m-p/1408017#M4076</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2022-02-02T12:52:34Z</dc:date>
    </item>
    <item>
      <title>Re: Issue in NAND read operation</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Issue-in-NAND-read-operation/m-p/1410249#M4079</link>
      <description>&lt;P&gt;Hi Pavel,&lt;/P&gt;&lt;P&gt;Thanks for your quick response.&lt;/P&gt;&lt;P&gt;We tried to follow your suggestions and based on that here are some of the observations.&lt;/P&gt;&lt;P&gt;1. We tried to write 10 locations of page 0 and the code-warrior shows NAND operation is complete. the IFC_NAND_EVTER_STAT register is loaded with value 0x80000000 which indicates the flash operation complete.&lt;/P&gt;&lt;P&gt;2. During the read operation of page 0 we are getting 00000000 as output on the memory window. so can you please suggest us what would be the issue.&lt;/P&gt;&lt;P&gt;For more details I am attaching the method (code) we have used for Reading/writing the NAND flash and the dump file obtained during the reading of NAND flash through code-warrior flash programmer along with the screenshots.&lt;/P&gt;&lt;P&gt;Please provide us the valuable input for solving this issue.&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; regards,&lt;/P&gt;&lt;P&gt;Irfan&lt;/P&gt;</description>
      <pubDate>Tue, 08 Feb 2022 11:41:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Issue-in-NAND-read-operation/m-p/1410249#M4079</guid>
      <dc:creator>Irfan3</dc:creator>
      <dc:date>2022-02-08T11:41:30Z</dc:date>
    </item>
  </channel>
</rss>