<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC ProcessorsのトピックDDR4 LS1046A</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/DDR4-LS1046A/m-p/1397875#M4059</link>
    <description>&lt;P&gt;Hello NXP,&lt;/P&gt;&lt;P&gt;Can I configure DDR controller in LS1046A to 2T and 3T. If configured, what are precautions shall I consider.&lt;/P&gt;&lt;P&gt;Also what is the minimum master clock speed configuration&amp;nbsp; allowed for DDR controller in LS1046A in DDR4 mode.&lt;/P&gt;</description>
    <pubDate>Wed, 12 Jan 2022 06:51:15 GMT</pubDate>
    <dc:creator>Nareshvarikuntla</dc:creator>
    <dc:date>2022-01-12T06:51:15Z</dc:date>
    <item>
      <title>DDR4 LS1046A</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/DDR4-LS1046A/m-p/1397875#M4059</link>
      <description>&lt;P&gt;Hello NXP,&lt;/P&gt;&lt;P&gt;Can I configure DDR controller in LS1046A to 2T and 3T. If configured, what are precautions shall I consider.&lt;/P&gt;&lt;P&gt;Also what is the minimum master clock speed configuration&amp;nbsp; allowed for DDR controller in LS1046A in DDR4 mode.&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jan 2022 06:51:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/DDR4-LS1046A/m-p/1397875#M4059</guid>
      <dc:creator>Nareshvarikuntla</dc:creator>
      <dc:date>2022-01-12T06:51:15Z</dc:date>
    </item>
    <item>
      <title>Re: DDR4 LS1046A</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/DDR4-LS1046A/m-p/1397899#M4060</link>
      <description>&lt;P&gt;2T or 3T can be configured - refer to the LS1046A Reference Manual, 15.4.8 DDR SDRAM control configuration (DDR_SDRAM_CFG).&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;2T (T2_EN) should not be set if DDR_SDRAM_CFG[T3_EN] is set.&lt;/P&gt;
&lt;P&gt;Note that RD_EN and T2_EN must not both be set at the same time.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;3T (T3_EN) cannot be set if DDR_SDRAM_CFG[T2_EN] is also set.&lt;/P&gt;
&lt;P&gt;3T timing may not be used with 4-beat bursts, unless DDR_SDRAM_CFG_2[OBC_CFG] is set.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Lowest supported Memory Bus Clock Frequency (DDR4) is 650 MHz - refer to the QorIQ LS1046A, LS1026A Data Sheet, Table 140. Processor, platform, and memory clocking specifications.&lt;/P&gt;</description>
      <pubDate>Wed, 12 Jan 2022 07:23:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/DDR4-LS1046A/m-p/1397899#M4060</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2022-01-12T07:23:49Z</dc:date>
    </item>
  </channel>
</rss>