<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC Processors中的主题 Error in Discrete DDR3L initialization</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/Error-in-Discrete-DDR3L-initialization/m-p/1381942#M4010</link>
    <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;We are using a discrete DDR3L on our custom board based on T2081 processor.&lt;/P&gt;&lt;P&gt;We tried it to test with QCVS tool, but it was failing in that with error message as&amp;nbsp;&lt;EM&gt;&lt;STRONG&gt;DDR initialization&amp;nbsp;fail: DINIT was not cleared by hardware&lt;/STRONG&gt;.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;To test it with u-boot driver, we configured the timing and configuration parameters of DDR from datasheet.&lt;/P&gt;&lt;P&gt;Now we are getting error as:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;SPI boot...&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Initializing....using Fixed DRAM&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;WARNING: Calling __hwconfig without a buffer and before environment is ready&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;WARNING: Calling __hwconfig without a buffer and before environment is ready&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;WARNING: Calling __hwconfig without a buffer and before environment is ready&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;WARNING: Calling __hwconfig without a buffer and before environment is ready&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Initializing....using fixed DDR: fsl_ddr_board_options&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Loading second stage boot loader .................................................................................................Bad trap at PC: 1000170, SR: 0, vector=e00&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;**bleep**: 01000170 XER: 00000000 LR: FFFD8B6C REGS: fffd7ed0 TRAP: 0e00 DAR: 00000000&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;MSR: 00000000 EE: 0 PR: 0 FP: 0 ME: 0 IR/DR: 00&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;GPR00: FFFE43B0 FFFD7FC0 FFFC8000 002BFFFF 000BFFFF FFFCB140 FFFCB140 FFFCB130&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;GPR08: 00000001 00200000 00200000 FFFD7FC0 FFFE3BE4 00000000 00000000 00000000&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;GPR16: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 01000170&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;GPR24: 00400000 00000000 00010000 00000000 00102000 FFFCB0F0 FFFE91C8 00102000&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Call backtrace:&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Exception in kernel pc 1000170 signal 0&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you please let me know the possible root cause of this.&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Awadhesh Singh&lt;/P&gt;</description>
    <pubDate>Mon, 06 Dec 2021 11:51:17 GMT</pubDate>
    <dc:creator>singhawadhesh</dc:creator>
    <dc:date>2021-12-06T11:51:17Z</dc:date>
    <item>
      <title>Error in Discrete DDR3L initialization</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Error-in-Discrete-DDR3L-initialization/m-p/1381942#M4010</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;We are using a discrete DDR3L on our custom board based on T2081 processor.&lt;/P&gt;&lt;P&gt;We tried it to test with QCVS tool, but it was failing in that with error message as&amp;nbsp;&lt;EM&gt;&lt;STRONG&gt;DDR initialization&amp;nbsp;fail: DINIT was not cleared by hardware&lt;/STRONG&gt;.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;To test it with u-boot driver, we configured the timing and configuration parameters of DDR from datasheet.&lt;/P&gt;&lt;P&gt;Now we are getting error as:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;SPI boot...&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Initializing....using Fixed DRAM&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;WARNING: Calling __hwconfig without a buffer and before environment is ready&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;WARNING: Calling __hwconfig without a buffer and before environment is ready&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;WARNING: Calling __hwconfig without a buffer and before environment is ready&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;WARNING: Calling __hwconfig without a buffer and before environment is ready&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Initializing....using fixed DDR: fsl_ddr_board_options&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Loading second stage boot loader .................................................................................................Bad trap at PC: 1000170, SR: 0, vector=e00&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;**bleep**: 01000170 XER: 00000000 LR: FFFD8B6C REGS: fffd7ed0 TRAP: 0e00 DAR: 00000000&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;MSR: 00000000 EE: 0 PR: 0 FP: 0 ME: 0 IR/DR: 00&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;GPR00: FFFE43B0 FFFD7FC0 FFFC8000 002BFFFF 000BFFFF FFFCB140 FFFCB140 FFFCB130&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;GPR08: 00000001 00200000 00200000 FFFD7FC0 FFFE3BE4 00000000 00000000 00000000&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;GPR16: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 01000170&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;GPR24: 00400000 00000000 00010000 00000000 00102000 FFFCB0F0 FFFE91C8 00102000&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Call backtrace:&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Exception in kernel pc 1000170 signal 0&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could you please let me know the possible root cause of this.&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Awadhesh Singh&lt;/P&gt;</description>
      <pubDate>Mon, 06 Dec 2021 11:51:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Error-in-Discrete-DDR3L-initialization/m-p/1381942#M4010</guid>
      <dc:creator>singhawadhesh</dc:creator>
      <dc:date>2021-12-06T11:51:17Z</dc:date>
    </item>
    <item>
      <title>Re: Error in Discrete DDR3L initialization</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Error-in-Discrete-DDR3L-initialization/m-p/1382993#M4014</link>
      <description>&lt;P&gt;Error message means that DDR controller was not able to go through the DDR initialization, as a result memory is not functional. Many reasons can cause it, mistakes in the schematics, mistakes in the RCW, board level issues, incorrect DDR sw setup, problems with power supplies, including MVREF.&lt;/P&gt;
&lt;P&gt;First I would recommend to check if the proper clock signal with expected frequency appears at the SDRAM clock pins after DDR initilalization. Use a scope for that.&lt;/P&gt;</description>
      <pubDate>Wed, 08 Dec 2021 02:15:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Error-in-Discrete-DDR3L-initialization/m-p/1382993#M4014</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2021-12-08T02:15:30Z</dc:date>
    </item>
  </channel>
</rss>