<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MPC885 GPCM and UPM in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC885-GPCM-and-UPM/m-p/1365483#M3946</link>
    <description>&lt;P&gt;I am using MPC885 (formerly FreeScale) with its GPCM used for controlling peripheral devices and its UPM used for operating an SDRAM.&lt;/P&gt;&lt;P&gt;My question is: How can I insert some delay between the GPCM end of cycle and UPM beginning of cycle?&lt;/P&gt;</description>
    <pubDate>Wed, 03 Nov 2021 06:08:27 GMT</pubDate>
    <dc:creator>KobyKluger</dc:creator>
    <dc:date>2021-11-03T06:08:27Z</dc:date>
    <item>
      <title>MPC885 GPCM and UPM</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC885-GPCM-and-UPM/m-p/1365483#M3946</link>
      <description>&lt;P&gt;I am using MPC885 (formerly FreeScale) with its GPCM used for controlling peripheral devices and its UPM used for operating an SDRAM.&lt;/P&gt;&lt;P&gt;My question is: How can I insert some delay between the GPCM end of cycle and UPM beginning of cycle?&lt;/P&gt;</description>
      <pubDate>Wed, 03 Nov 2021 06:08:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC885-GPCM-and-UPM/m-p/1365483#M3946</guid>
      <dc:creator>KobyKluger</dc:creator>
      <dc:date>2021-11-03T06:08:27Z</dc:date>
    </item>
    <item>
      <title>Re: MPC885 GPCM and UPM</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC885-GPCM-and-UPM/m-p/1366243#M3948</link>
      <description>&lt;P&gt;The processor allows to add one bus clock cycle between GPCM read cycle and subsequent bus transaction. ORx[EHTR] bit should be set for GPCM bank.&lt;/P&gt;
&lt;P&gt;If for some reason you need greater delay, you can program UPM read/write patterns with shifted/delayed CS assertion.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 04 Nov 2021 02:50:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC885-GPCM-and-UPM/m-p/1366243#M3948</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2021-11-04T02:50:25Z</dc:date>
    </item>
    <item>
      <title>Re: MPC885 GPCM and UPM</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC885-GPCM-and-UPM/m-p/1369846#M3961</link>
      <description>&lt;P&gt;I tried setting EHTR bit to "1" but it doesn't have any impact on the delay between GPCM and UPM.&lt;/P&gt;&lt;P&gt;The refrence manual states explicitley that EHTR bit refers to GPCM only, but it doesn't influence the delay when switching to UPM.&lt;/P&gt;&lt;P&gt;I wonder if anyway there is a way to insert more delay between the two machines without re-programming the UPM...&lt;/P&gt;</description>
      <pubDate>Thu, 11 Nov 2021 09:44:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC885-GPCM-and-UPM/m-p/1369846#M3961</guid>
      <dc:creator>KobyKluger</dc:creator>
      <dc:date>2021-11-11T09:44:00Z</dc:date>
    </item>
  </channel>
</rss>