<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC ProcessorsのトピックP1022 SDRAM test failed</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/P1022-SDRAM-test-failed/m-p/1361308#M3928</link>
    <description>&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;We are testing a custom board with processor P1022. The processor boots but is always stuck on the SDRAM test phases. This is observed in 2 of 15 boards so we do not consider it the problem of routing.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The power supplies, clocks to the DDR, and reset are checked and found to be ok.&lt;/P&gt;&lt;P&gt;Please help regarding this issue.&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Souvik&lt;/P&gt;</description>
    <pubDate>Tue, 26 Oct 2021 05:57:13 GMT</pubDate>
    <dc:creator>sarkarsouvik</dc:creator>
    <dc:date>2021-10-26T05:57:13Z</dc:date>
    <item>
      <title>P1022 SDRAM test failed</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/P1022-SDRAM-test-failed/m-p/1361308#M3928</link>
      <description>&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;We are testing a custom board with processor P1022. The processor boots but is always stuck on the SDRAM test phases. This is observed in 2 of 15 boards so we do not consider it the problem of routing.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The power supplies, clocks to the DDR, and reset are checked and found to be ok.&lt;/P&gt;&lt;P&gt;Please help regarding this issue.&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Souvik&lt;/P&gt;</description>
      <pubDate>Tue, 26 Oct 2021 05:57:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/P1022-SDRAM-test-failed/m-p/1361308#M3928</guid>
      <dc:creator>sarkarsouvik</dc:creator>
      <dc:date>2021-10-26T05:57:13Z</dc:date>
    </item>
    <item>
      <title>Re: P1022 SDRAM test failed</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/P1022-SDRAM-test-failed/m-p/1362084#M3931</link>
      <description>&lt;P&gt;You could use QCVS DDRv tool to connect to your custom board to do optimization and validation.&lt;/P&gt;
&lt;P&gt;You could use CodeWarrior to connect to your custom board to read DDR configuration register values, then modify the attached file according to these register values. Then create a QCVS DDR project with "Import from memory file" method, using the modified file.&lt;/P&gt;</description>
      <pubDate>Wed, 27 Oct 2021 05:29:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/P1022-SDRAM-test-failed/m-p/1362084#M3931</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2021-10-27T05:29:21Z</dc:date>
    </item>
  </channel>
</rss>