<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC Processors中的主题 Flash device in t2081</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/Flash-device-in-t2081/m-p/1348439#M3890</link>
    <description>&lt;P&gt;&lt;EM&gt;Hi Team,&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;I want to add NOR flash device on codewarrior or if possible use any other device which is already present in codewarrior.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Is any there any flash device which will readily support this device MT28FW02GBBA1HPC-0AAT.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;For reference i am sharing the datasheet of the device.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Thanks and Regards&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Irfan&lt;/EM&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 29 Sep 2021 13:55:05 GMT</pubDate>
    <dc:creator>Irfan3</dc:creator>
    <dc:date>2021-09-29T13:55:05Z</dc:date>
    <item>
      <title>Flash device in t2081</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/Flash-device-in-t2081/m-p/1348439#M3890</link>
      <description>&lt;P&gt;&lt;EM&gt;Hi Team,&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;I want to add NOR flash device on codewarrior or if possible use any other device which is already present in codewarrior.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Is any there any flash device which will readily support this device MT28FW02GBBA1HPC-0AAT.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;For reference i am sharing the datasheet of the device.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Thanks and Regards&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Irfan&lt;/EM&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 29 Sep 2021 13:55:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/Flash-device-in-t2081/m-p/1348439#M3890</guid>
      <dc:creator>Irfan3</dc:creator>
      <dc:date>2021-09-29T13:55:05Z</dc:date>
    </item>
  </channel>
</rss>