<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>PowerQUICC Processors中的主题 Re: MPC8548 PCI1 Agent Configuration</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8548-PCI1-Agent-Configuration/m-p/1302049#M3746</link>
    <description>&lt;P&gt;Please provide:&lt;/P&gt;
&lt;P&gt;1) the processor connection schematics as searchable PDF for inspection&lt;/P&gt;
&lt;P&gt;2) digital scope of the PCI bus activity (better if signals are probed at the processor's pins)&lt;/P&gt;
&lt;P&gt;3) how many boards were tested?&lt;/P&gt;</description>
    <pubDate>Sat, 03 Jul 2021 10:19:27 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2021-07-03T10:19:27Z</dc:date>
    <item>
      <title>MPC8548 PCI1 Agent Configuration</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8548-PCI1-Agent-Configuration/m-p/1301354#M3741</link>
      <description>&lt;P&gt;We have an MPC8548 configured (as far as we can tell) as a PCI1 Agent.&amp;nbsp; When we examine the internal registers, the 8548 appears to be correctly configured as an Agent.&amp;nbsp; However, when the PCI Host asserts IDSEL on the slot the 8548 is located, it does not respond... It does not assert DEVSEL or any other PCI signal.&lt;/P&gt;&lt;P&gt;It has been discussed to set the PCI1 arbiter to external, but we do not see how that could be an issue.&lt;/P&gt;&lt;P&gt;Deep dives into our data sheet have not revealed any reason for it to be non-responsive.&lt;/P&gt;</description>
      <pubDate>Thu, 01 Jul 2021 18:38:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8548-PCI1-Agent-Configuration/m-p/1301354#M3741</guid>
      <dc:creator>mepperly</dc:creator>
      <dc:date>2021-07-01T18:38:29Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8548 PCI1 Agent Configuration</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8548-PCI1-Agent-Configuration/m-p/1301472#M3742</link>
      <description>&lt;P&gt;You wrote:&lt;/P&gt;
&lt;P&gt;&amp;gt; the 8548 appears to be correctly configured as an Agent&lt;/P&gt;
&lt;P&gt;Please describe how you've checked this.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Additionally check whether the agent configuration lock has been disabled in the agent initialization code - refer to the MPC8548E PowerQUICC III Integrated Processor Family Reference Manual, 4.4.3.6 CPU Boot Configuration and 16.3.2.19 PCI Bus Function Register (PBFR).&lt;/P&gt;</description>
      <pubDate>Fri, 02 Jul 2021 03:14:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8548-PCI1-Agent-Configuration/m-p/1301472#M3742</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-07-02T03:14:04Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8548 PCI1 Agent Configuration</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8548-PCI1-Agent-Configuration/m-p/1301856#M3745</link>
      <description>&lt;P&gt;Per the PBFR, we are in agent mode, ACL is set on boot and then cleared.&amp;nbsp; We manually cleared the ACL and it still would not configure&lt;/P&gt;&lt;P&gt;We boot and clear the ACL, but the configuration cycles are not acknowledged by the agent (no DEVSEL when IDSEL goes high)&lt;/P&gt;&lt;P&gt;It appears we should clear the ACL early in our boot&lt;/P&gt;</description>
      <pubDate>Fri, 02 Jul 2021 12:51:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8548-PCI1-Agent-Configuration/m-p/1301856#M3745</guid>
      <dc:creator>mepperly</dc:creator>
      <dc:date>2021-07-02T12:51:33Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8548 PCI1 Agent Configuration</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8548-PCI1-Agent-Configuration/m-p/1302049#M3746</link>
      <description>&lt;P&gt;Please provide:&lt;/P&gt;
&lt;P&gt;1) the processor connection schematics as searchable PDF for inspection&lt;/P&gt;
&lt;P&gt;2) digital scope of the PCI bus activity (better if signals are probed at the processor's pins)&lt;/P&gt;
&lt;P&gt;3) how many boards were tested?&lt;/P&gt;</description>
      <pubDate>Sat, 03 Jul 2021 10:19:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/MPC8548-PCI1-Agent-Configuration/m-p/1302049#M3746</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-07-03T10:19:27Z</dc:date>
    </item>
  </channel>
</rss>