<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: [LS2088A] Codewarrior CCS command error in PowerQUICC Processors</title>
    <link>https://community.nxp.com/t5/PowerQUICC-Processors/LS2088A-Codewarrior-CCS-command-error/m-p/1261989#M3642</link>
    <description>&lt;P&gt;Without "ccs::config_chain {ls2088a sap2}",&amp;nbsp; I put the command "display ccs::get_config_chain".&lt;/P&gt;&lt;P&gt;The result was as follows :&lt;/P&gt;&lt;P&gt;(bin) 50 % display ccs::get_config_chain&lt;BR /&gt;Chain Position 0: LS2085A&lt;BR /&gt;Chain Position 1: CoreSight ATB Funnel&lt;BR /&gt;Chain Position 2: CoreSight TMC&lt;BR /&gt;Chain Position 3: CoreSight TMC&lt;BR /&gt;Chain Position 4: CoreSight ATB Funnel&lt;BR /&gt;Chain Position 5: CoreSight ATB Funnel&lt;BR /&gt;Chain Position 6: CoreSight ATB Funnel&lt;BR /&gt;Chain Position 7: CoreSight ATB Funnel&lt;/P&gt;&lt;P&gt;.......&lt;/P&gt;&lt;P&gt;Chain Position 322: CoreSight CTI&lt;BR /&gt;Chain Position 323: Cortex-A72 PMU&lt;BR /&gt;Chain Position 324: Cortex-A72 ETM&lt;BR /&gt;Chain Position 325: DAP&lt;BR /&gt;Chain Position 326: SAP2&lt;/P&gt;&lt;P&gt;Is this normal operation?&lt;/P&gt;&lt;P&gt;(1) In my LS2088ARDB board, there is no need to put the command "ccs::config_chain {ls2088a sap2}"?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In addition, I have another question.&lt;/P&gt;&lt;P&gt;When I command "ccs::write mem 2 0x7 0x001000D0 0x4 0x0 0x800", which is directed in LSDK User guide Rev.19 page.298 for secure boot test, "Unimplemented" message appears.&lt;/P&gt;&lt;P&gt;(2) Is that command not needed in secure boot test with CW in LS2088A?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
    <pubDate>Wed, 14 Apr 2021 11:36:50 GMT</pubDate>
    <dc:creator>jhkim2</dc:creator>
    <dc:date>2021-04-14T11:36:50Z</dc:date>
    <item>
      <title>[LS2088A] Codewarrior CCS command error</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/LS2088A-Codewarrior-CCS-command-error/m-p/1261020#M3633</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;When I put commands below in CCS console, I get error message.&lt;/P&gt;&lt;P&gt;config cc cwtap:10.11.238.176&lt;/P&gt;&lt;P&gt;ccs::config_chain {ls2088a sap2}&lt;/P&gt;&lt;P&gt;can't read "::ccs::core(ls2088a)": no such element in array&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How can I fix this problem?&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;JeongHwan Kim&lt;/P&gt;</description>
      <pubDate>Tue, 13 Apr 2021 06:28:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/LS2088A-Codewarrior-CCS-command-error/m-p/1261020#M3633</guid>
      <dc:creator>jhkim2</dc:creator>
      <dc:date>2021-04-13T06:28:06Z</dc:date>
    </item>
    <item>
      <title>Re: [LS2088A] Codewarrior CCS command error</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/LS2088A-Codewarrior-CCS-command-error/m-p/1261089#M3635</link>
      <description>&lt;P&gt;1) Which exactly board is in question?&lt;/P&gt;
&lt;P&gt;2) Is the processor capable to successfully complete its POR sequence? - i.e. all reset signals behave as shown in the QorIQ LS2088A Reference Manual, Figure 4-1. Power-On Reset Sequence.&lt;/P&gt;
&lt;P&gt;Pay special attention to the RESET_REQ_B and ASLEEP.&lt;/P&gt;
&lt;P&gt;3) How RCW is provided to the processor?&lt;/P&gt;
&lt;P&gt;4) Please execute in the CCS console "source IDcode.tcl" and provide the log.&lt;/P&gt;</description>
      <pubDate>Tue, 13 Apr 2021 07:57:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/LS2088A-Codewarrior-CCS-command-error/m-p/1261089#M3635</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-04-13T07:57:18Z</dc:date>
    </item>
    <item>
      <title>Re: [LS2088A] Codewarrior CCS command error</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/LS2088A-Codewarrior-CCS-command-error/m-p/1261594#M3637</link>
      <description>&lt;P&gt;1) My board is LS2088ARDB rev.F3.&lt;/P&gt;&lt;P&gt;2) I'm trying to test secure boot with Ls2088a, so I set the Switch 4.8 to 0 to put the core into RSP.&lt;/P&gt;&lt;P&gt;After that, I reboot the board and executed codewarrior software.&lt;/P&gt;&lt;P&gt;I started the CCS program with button "Connect" beside flash programming button.&lt;/P&gt;&lt;P&gt;3) I did not do anything but default CW setting.&lt;/P&gt;&lt;P&gt;4) I attach "source IDcode.tcl" result&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="idcode.tcl.png" style="width: 546px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/142178i7DAFA8136A16F216/image-size/large?v=v2&amp;amp;px=999" role="button" title="idcode.tcl.png" alt="idcode.tcl.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Apr 2021 02:10:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/LS2088A-Codewarrior-CCS-command-error/m-p/1261594#M3637</guid>
      <dc:creator>jhkim2</dc:creator>
      <dc:date>2021-04-14T02:10:54Z</dc:date>
    </item>
    <item>
      <title>Re: [LS2088A] Codewarrior CCS command error</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/LS2088A-Codewarrior-CCS-command-error/m-p/1261639#M3638</link>
      <description>&lt;P&gt;You wrote:&lt;/P&gt;
&lt;P&gt;&amp;gt; I started the CCS program with button "Connect" beside flash programming button.&lt;/P&gt;
&lt;P&gt;The CCS has to be started before resetting the board by running ccs.exe:&lt;/P&gt;
&lt;P&gt;c:\Freescale\CW4NET_v2020.06\Common\CCS\bin\ccs.exe&lt;/P&gt;</description>
      <pubDate>Wed, 14 Apr 2021 02:58:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/LS2088A-Codewarrior-CCS-command-error/m-p/1261639#M3638</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-04-14T02:58:47Z</dc:date>
    </item>
    <item>
      <title>Re: [LS2088A] Codewarrior CCS command error</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/LS2088A-Codewarrior-CCS-command-error/m-p/1261989#M3642</link>
      <description>&lt;P&gt;Without "ccs::config_chain {ls2088a sap2}",&amp;nbsp; I put the command "display ccs::get_config_chain".&lt;/P&gt;&lt;P&gt;The result was as follows :&lt;/P&gt;&lt;P&gt;(bin) 50 % display ccs::get_config_chain&lt;BR /&gt;Chain Position 0: LS2085A&lt;BR /&gt;Chain Position 1: CoreSight ATB Funnel&lt;BR /&gt;Chain Position 2: CoreSight TMC&lt;BR /&gt;Chain Position 3: CoreSight TMC&lt;BR /&gt;Chain Position 4: CoreSight ATB Funnel&lt;BR /&gt;Chain Position 5: CoreSight ATB Funnel&lt;BR /&gt;Chain Position 6: CoreSight ATB Funnel&lt;BR /&gt;Chain Position 7: CoreSight ATB Funnel&lt;/P&gt;&lt;P&gt;.......&lt;/P&gt;&lt;P&gt;Chain Position 322: CoreSight CTI&lt;BR /&gt;Chain Position 323: Cortex-A72 PMU&lt;BR /&gt;Chain Position 324: Cortex-A72 ETM&lt;BR /&gt;Chain Position 325: DAP&lt;BR /&gt;Chain Position 326: SAP2&lt;/P&gt;&lt;P&gt;Is this normal operation?&lt;/P&gt;&lt;P&gt;(1) In my LS2088ARDB board, there is no need to put the command "ccs::config_chain {ls2088a sap2}"?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In addition, I have another question.&lt;/P&gt;&lt;P&gt;When I command "ccs::write mem 2 0x7 0x001000D0 0x4 0x0 0x800", which is directed in LSDK User guide Rev.19 page.298 for secure boot test, "Unimplemented" message appears.&lt;/P&gt;&lt;P&gt;(2) Is that command not needed in secure boot test with CW in LS2088A?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;</description>
      <pubDate>Wed, 14 Apr 2021 11:36:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/LS2088A-Codewarrior-CCS-command-error/m-p/1261989#M3642</guid>
      <dc:creator>jhkim2</dc:creator>
      <dc:date>2021-04-14T11:36:50Z</dc:date>
    </item>
    <item>
      <title>Re: [LS2088A] Codewarrior CCS command error</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/LS2088A-Codewarrior-CCS-command-error/m-p/1262124#M3644</link>
      <description>&lt;P&gt;For the LS2088A it should be:&lt;/P&gt;
&lt;P&gt;ccs::config_chain {ls2085a sap2}&lt;/P&gt;</description>
      <pubDate>Wed, 14 Apr 2021 16:02:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/LS2088A-Codewarrior-CCS-command-error/m-p/1262124#M3644</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-04-14T16:02:53Z</dc:date>
    </item>
    <item>
      <title>Re: [LS2088A] Codewarrior CCS command error</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/LS2088A-Codewarrior-CCS-command-error/m-p/1263094#M3646</link>
      <description>&lt;P&gt;Thanks for reply.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I put the CW command "ccs::config_chain {ls2085a sap2}" and set "ccs::write_mem 2 0x7 0x001000D0 0x4 0x0 0x800" in order to set the board enter RSP for secure boot test.&lt;/P&gt;&lt;P&gt;But "unimplemented " message returned and I cannot go further.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="cw_error.jpg" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/142424i34F5A44E78412D02/image-size/large?v=v2&amp;amp;px=999" role="button" title="cw_error.jpg" alt="cw_error.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 16 Apr 2021 00:42:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/LS2088A-Codewarrior-CCS-command-error/m-p/1263094#M3646</guid>
      <dc:creator>jhkim2</dc:creator>
      <dc:date>2021-04-16T00:42:03Z</dc:date>
    </item>
    <item>
      <title>Re: [LS2088A] Codewarrior CCS command error</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/LS2088A-Codewarrior-CCS-command-error/m-p/1263157#M3649</link>
      <description>&lt;P&gt;Please provide complete ccs log as textual attachment - top a picture.&lt;/P&gt;</description>
      <pubDate>Fri, 16 Apr 2021 02:34:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/LS2088A-Codewarrior-CCS-command-error/m-p/1263157#M3649</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-04-16T02:34:10Z</dc:date>
    </item>
    <item>
      <title>Re: [LS2088A] Codewarrior CCS command error</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/LS2088A-Codewarrior-CCS-command-error/m-p/1263208#M3650</link>
      <description>&lt;P&gt;I attached the text file of CSS log&lt;/P&gt;</description>
      <pubDate>Fri, 16 Apr 2021 04:19:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/LS2088A-Codewarrior-CCS-command-error/m-p/1263208#M3650</guid>
      <dc:creator>jhkim2</dc:creator>
      <dc:date>2021-04-16T04:19:07Z</dc:date>
    </item>
    <item>
      <title>Re: [LS2088A] Codewarrior CCS command error</title>
      <link>https://community.nxp.com/t5/PowerQUICC-Processors/LS2088A-Codewarrior-CCS-command-error/m-p/1263247#M3651</link>
      <description>&lt;P&gt;The&lt;/P&gt;
&lt;P&gt;&lt;FONT face="courier new,courier"&gt;puts "Entry RSP: "&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;ccs::write_mem 2 0x7 0x001000D0 0x4 0x0 0x800&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;and&lt;/P&gt;
&lt;P&gt;&lt;FONT face="courier new,courier"&gt;puts "Exiting RSP: "&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="courier new,courier"&gt;ccs::write_mem 2 0x7 0x001000D0 0x4 0x0 0x400&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;are not needed for the LS2088A.&lt;/P&gt;</description>
      <pubDate>Fri, 16 Apr 2021 05:47:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/PowerQUICC-Processors/LS2088A-Codewarrior-CCS-command-error/m-p/1263247#M3651</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2021-04-16T05:47:04Z</dc:date>
    </item>
  </channel>
</rss>